Search:

Type: Posts; User: Adrenalynn; Keyword(s):

Page 1 of 13 1 2 3 4

Search: Search took 0.17 seconds.

  1. Replies
    131
    Views
    56,451

    Project Re: First ever project :)

    Congrats, Chris!
  2. Thread: HottieBot

    by Adrenalynn
    Replies
    20
    Views
    11,209

    Contest Entry Re: HottieBot

    Funny!

    Curious why you didn't go with a little 2 channel PWM-driven motor controller. Something like the Scorpion would have cut your part count and size (and programming) down infinitely much. ...
  3. Re: Looking for a better IP camera? - Cisco Wireless-N Internet Home Monitoring Camera WVC80N

    Yes. Let's see you get it running on an arduino - or even a SAM9...

    Again: Undocumented.

    And still undocumented.

    The module I posted is documented. With source.
  4. Re: Looking for a better IP camera? - Cisco Wireless-N Internet Home Monitoring Camera WVC80N

    http://www.sagrad.com/index.php?option=com_docman&task=doc_download&gid=47&Itemid=70 <-- 5Ghz

    The module in your linksys example is undocumented.
  5. Replies
    104
    Views
    38,158

    Re: ArbotiX ROS Package 0.2.0

    Sorry I laughed. Couldn't help it.
  6. Re: Looking for a better IP camera? - Cisco Wireless-N Internet Home Monitoring Camera WVC80N

    The SG901 modules are ~$30ea in moq: 1, have free drivers (cross platform) and they GPL the hardware abstraction layer.
    ...
  7. Re: Looking for a better IP camera? - Cisco Wireless-N Internet Home Monitoring Camera WVC80N

    802.11n is faaaar more frequency-agile and far less susceptible to interference regardless. That's a big part of what OFDM (Orthogonal Frequency Division Multiplexing) buys. And mimo doesn't hurt...
  8. Re: Looking for a better IP camera? - Cisco Wireless-N Internet Home Monitoring Camera WVC80N

    What 5.8 are they using?

    n is in the 5.4 to 5.75Ghz range.
  9. Re: Looking for a better IP camera? - Cisco Wireless-N Internet Home Monitoring Camera WVC80N

    >> until you start talking about the 40kbit 3-5fps 160x120 streams which are just painful to look at

    Even then it's latency that will kill you.

    >> so with a raw 2bpp palette you can contain a...
  10. Replies
    14
    Views
    7,032

    Question(s) Re: Where to go from here??

    http://tinyurl.com/bms4an
  11. Re: Looking for a better IP camera? - Cisco Wireless-N Internet Home Monitoring Camera WVC80N

    2.4ghz WiFi g can stream 60fps 720p HD without a hiccup.

    PNG isn't going to get you anywhere. You need to research motion prediction, sprites, and temporal compression.
  12. Re: Collaboration group for ROS+Arbotix-based robots

    I've got a couple HPs under the desk here that have 32gbit/sec fabric. But DLink makes some inexpensive managed stackable 32gbit/sec switches now that aren't have bad.
  13. Re: Recommended 24V Battery for laser scanner?

    Do you know what the current requirements are? Maybe you could use a boost regulator and step the power up from the Create?
  14. Replies
    4
    Views
    3,951

    Re: Off-Topic: Webcam recommendation request

    No worries. The occasional [enter] helps a lot between paragraphs.

    DSL is a doable solution. I had just seen you mentioning satellite in there. Latency is the killer over satellite.

    I have a...
  15. Replies
    4
    Views
    3,951

    Re: Off-Topic: Webcam recommendation request

    That was like a giant wall of text. But am I correct in reading you're looking to stream realtime video with PTZ over a satellite link?
  16. Re: Collaboration group for ROS+Arbotix-based robots

    In theory, if everyone played nice, ran identical [properly interpreted] network adapters feeding a carefully chosen access point(s), and followed an exact band-plan - there would be ~7gigabits, 20+...
  17. Replies
    3
    Views
    5,429

    Re: C# code for moving servos!

    What servo controller are you using? That's the important question - followed by what servos...
  18. Replies
    19
    Views
    10,790

    Question(s) Re: my own spin on the Phantom X

    dotNet will open a serial port just fine. So you can talk to the arbotiX all you like.
  19. Replies
    11
    Views
    16,683

    Re: Understanding a 3-XBEE network?

    If you're promiscuously broadcasting, anything that knows how to interpret a fully formed command will. If it doesn't, it'll just kick back an error, as you surmised.
  20. Replies
    19
    Views
    10,790

    Question(s) Re: my own spin on the Phantom X

    ROS is being worked on by one of the foremost teams in robotics on the planet right now. Fergs has an interface from ROS to the arbotiX - he's not writing ROS. That'd be Willow Garage's team.
    ...
  21. Replies
    278
    Views
    108,835

    Project Re: More Mule then Rover?

    That's hardly localization...
  22. Replies
    15
    Views
    11,054

    Re: Free stuff free stuff free stuff :p

    Given the cost of tags and the range of the scanner - I'd suggest you consider a web cam with fiducials (http://www.roborealm.com/help/Fiducial.php) or even the newest implementation of fiducials -...
  23. Re: Looking for a better IP camera? - Cisco Wireless-N Internet Home Monitoring Camera WVC80N

    We have a couple of those watching a client's datacenter. They're actually a pretty nice camera for cheap cmos and pseudo-lens. That said - they aren't so hot at holding up a connection unless...
  24. Thread: Gyroscopes

    by Adrenalynn
    Replies
    12
    Views
    7,246

    Re: Gyroscopes

    Although the Trimble GIS stuff I've used also integrates RF triangulation to help that along a bit. Averaging out the error, even with WAAS, is never going to get you down to mm accuracy without...
  25. Re: Collaboration group for ROS+Arbotix-based robots

    If everyone goes -n, then it could be constrained to 5.8Ghz and get out of the muck, right? Just lock it to a 5.8 channel space, n-only

    High rejection 2.4 antennas would help a bunch too.
  26. Question(s) Re: how to see through my webcam from some place else?

    You're looking for streaming software.

    VLC, ZoneMinder, Windows Media Encoder - three free examples.
  27. Re: Collaboration group for ROS+Arbotix-based robots

    I've been gone for awhile. Can you link me to the thread with your current walking via remote ax-12-based hexapod that has a fitPC and an arbotiX on it?
  28. Replies
    278
    Views
    108,835

    Project Re: More Mule then Rover?

    I'd be careful with the "all will ____". None of my large controllers will do any such thing if they lose either analog or PCM.

    But regardless - I don't really care what motor controller you...
  29. Replies
    278
    Views
    108,835

    Project Re: More Mule then Rover?

    >> the more I liked it(for safety reasons)

    I have to ask what those "safety reasons" versus a combat robot motor controller would be.

    >> also the $600 cost

    That's about double the cost of...
  30. Replies
    278
    Views
    108,835

    Project Re: More Mule then Rover?

    Have you torn the motor controllers apart and looked at the boards? A lot of these controllers are actually OEM Curtis. And documentation/pinouts are fairly easy to come by.
    ...
  31. Replies
    1
    Views
    3,244

    Question(s) Re: Low profile stepper motor

    Raiding junk printers is always my goto for small steppers.

    Welcome to the forum!
  32. Re: Any experience with Bumblebee2 stereo camera?

    Alas, you missed Ferg's point that the low-end gaming cameras are designed to be far sparser than we require. Raising the density actually hurts them.

    Of course, mass production always drives...
  33. Replies
    29
    Views
    23,714

    Question(s) Re: Newby Arbotix hassles

    I had to roll the JRE to the 32 bit version, and run the dev environment with administrative rights.
  34. Replies
    18
    Views
    9,038

    Question(s) Re: Arduino and SC16A Problem

    The UART is bidirectional. I was thinking the hardware serial was on 2/3, but I guess it's on 0/1. One of these clone boards is on 2/3... [shrug]

    You can run software serial or hardware...
  35. Replies
    18
    Views
    9,038

    Question(s) Re: Arduino and SC16A Problem

    I'm not even sure why it links...

    void setup()
    {
    Serial.begin(9600); // opens serial port, sets data rate to 9600 bps
    }

    void loop() {}

    Get rid of all references to software serial -...
  36. Replies
    19
    Views
    10,649

    Bioloid Re: something wrong with bioloid

    I don't use the CM-*, preferring real controllers like the arbotiX - but I'd wonder if yoinking the connection while it's programming might have gotten it into a bricked-state?
  37. Replies
    18
    Views
    9,038

    Question(s) Re: Arduino and SC16A Problem

    I lost interest when I saw we were using software serial on a hardware UART...
  38. Replies
    2
    Views
    4,716

    Question(s) Re: breath sensors

    Well, if you use a vacuum switch, it would need to make a good seal on their face so there wasn't any escaping gas.

    How about a hygrometer (humidity sensor)? As long as your humidity is under...
  39. Replies
    8
    Views
    5,718

    Question(s) Re: A Good Motor Controller

    Actually, I think it's pretty effective. If you can't figure out what the problem is, just create a new problem that is impossible to repair. Voila! Now you can stop trying to figure out the...
  40. Re: Looking for small, tabletop, autonomous robot

    Maybe a half dozen of them. If they're fast enough...

    Again, same problem. Wheels go flyin off before a single ping can see the edge.

    Never trust any single sensor regardless of what it is.
Results 1 to 40 of 500
Page 1 of 13 1 2 3 4