Search:

Type: Posts; User: Deimos; Keyword(s):

Page 1 of 6 1 2 3 4

Search: Search took 0.01 seconds.

  1. Replies
    3
    Views
    6,715

    Anyone want to collaborate on a project?

    I just stopped by and it's crazy to see everyone who is still around. Feels like it's been forever.

    I currently don't have time/money to put together a new mech project, but if somebody wants to...
  2. Replies
    70
    Views
    253,239

    Re: 2017 Robogames Ideas

    I'm hoping to bring my mech to this one. I've got significantly more resources at my disposal now thanks to my university; most importantly a machine shop and a couple comp-sci guys who volunteered...
  3. Replies
    48
    Views
    37,464

    Re: Robogames 2016 Mech Warfare Announcement.

    I won't be able to get my mech up and running by then unfortunately. I keep getting sidetracked trying to optimize my gait engine and I never got around to milling the other three Tibia's I need. Ah...
  4. Replies
    12
    Views
    14,713

    Re: Mini oscilloscope and function generator

    The analog discovery is pretty nice. Does what it's supposed to; super user friendly documentation. I got it and a decently sized kit of components for all of $150 because my college uses it for...
  5. Replies
    37
    Views
    57,593

    Re: RTEAM Robotics Club Mech Warfare 2015

    I think it could be interesting to remove the 1 hit/s cap on the panels and instead imposing a rate of fire limit on all mechs. My thinking being that getting in close and unloading in bursts would...
  6. Replies
    84
    Views
    69,736

    Re: 3DOF Quadrupedal AX-12A Mech :: Fang

    Experimenting with aluminum brackets:

    5952

    This was my first attempt, I used some leftover 0.050" T6. Bends were done with a break I made out of angle iron. The main issue looks like it's going...
  7. Replies
    10
    Views
    15,063

    Re: My robot accidentally my monitor!

    I second tician's response.
  8. Re: MWScore Initiative: a thread about the development of the MW scoring system

    My panels just have the velostat stuck down with double sided tape on the edges and rest on the traces. The sensitivity worked out just fine, there is plenty of difference between resting and a bb...
  9. Replies
    36
    Views
    71,042

    Re: Mech Warfare 2015

    What panels will you be distributing? I stopped working on mine because I liked tician's panels more and I was getting ready to see about getting my hands on some.
  10. Replies
    84
    Views
    69,736

    Re: 3DOF Quadrupedal AX-12A Mech :: Fang

    Oops I meant to take that out :). Definitely my brother's fault. Yeah, pretty smooth :).
  11. Replies
    84
    Views
    69,736

    Re: 3DOF Quadrupedal AX-12A Mech :: Fang

    Sure! Github. Good luck understanding that :p. It is the result of two incredibly lazy programmers at 2:00 in the morning. It's going to be reorganized, cleaned up and commented soonish (probably).
    ...
  12. Replies
    84
    Views
    69,736

    Re: 3DOF Quadrupedal AX-12A Mech :: Fang

    Well, took a little longer than expected, but with some help from my brother it's walking. Using an Arbotix-M for now. Beaglebone Black was looking like it was more work than I wanted to do at the...
  13. Re: MWScore Initiative: a thread about the development of the MW scoring system

    These are looking great! Do you expect to have them ready for March or should I finalize my panels for competitors at the WV event?
  14. Replies
    36
    Views
    71,042

    Re: Mech Warfare 2015

    I'm in if Chicago isn't happening this year (if it is then maybe). I'll be able to show up on Friday to help out as well.
  15. Replies
    36
    Views
    71,042

    Re: Mech Warfare 2015

    My panels will likely be ready by then, I can send some to you, sthmck, if you would like to review them in lieu of official approval from Andrew. I've just been swamped with school/work, but I'll be...
  16. Replies
    6
    Views
    8,051

    Re: Mounting a turret on the Quadruped

    There are mounting holes for an AX-12 on the top of the PhantomX quad, and like Jwatte said you don't need two Arbotix's. I'd recommend just mounting an AX-12 to top, and purchasing a couple brackets...
  17. Replies
    10
    Views
    12,363

    Re: Problem with Arbotix ADC

    From the AnalogInOutSerial example:

    The circuit:
    * potentiometer connected to analog pin 0.
    Center pin of the potentiometer goes to the analog pin.
    side pins of the potentiometer go to...
  18. Replies
    8
    Views
    13,054

    Question(s) Re: Dynamixel comm_rxtimeout error for linux

    Ah, I did not mean to say that the modification of dxl_hal.c was causing the issue, simply that if one were to make the modifications required to use the USB2AX (which I assumed was what arman had...
  19. Replies
    8
    Views
    13,054

    Question(s) Re: Dynamixel comm_rxtimeout error for linux

    The linked thread is mine, and discusses modifying dxl_hal.c so it works with the USB2AX, what am I missing?
  20. Replies
    8
    Views
    13,054

    Question(s) Re: Dynamixel comm_rxtimeout error for linux

    True, however I do believe that there are other modifications in Xevel's version (such as changing the serial port name to ttyACM instead of ttyUSB or whatever) that would need to be left out if you...
  21. Replies
    8
    Views
    13,054

    Question(s) Re: Dynamixel comm_rxtimeout error for linux

    Also, you should not change dxl_hal.c if you are using the USB2Dynamixel. You only need to modify that if you are using Xevel's USB2AX.
  22. Replies
    22
    Views
    79,756

    Sticky: Re: Mech Warfare Weapons Guide

    Updated to include Onyx Fire II board. I'll add a bit about R-Team's setup soon. Though, if you wanted to write up a quick guide about your setup I'm sure you'd do a better job of it than I could....
  23. Replies
    26
    Views
    160,682

    Sticky: Re: Mech Warfare 2014 Update

    How is the mech warfare committee coming along? I think it would be very beneficial to get that going as soon as possible. Having some leadership to coordinate community efforts on MW related...
  24. Replies
    13
    Views
    15,427

    Re: Onyx Fire II DXL-bus actuator board

    Looks very thorough, nice job!

    One thing you may wish to clarify: On page 4 (in the table) minimum input voltage is specified as 7V, but on page 6 (paragraph 1) it says:

    Since I intend to power...
  25. Replies
    84
    Views
    69,736

    Re: 3DOF Quadrupedal AX-12A Mech :: Fang

    The retaining screw did the trick, thanks!
  26. Replies
    84
    Views
    69,736

    Re: 3DOF Quadrupedal AX-12A Mech :: Fang

    Progress:

    5450

    Everything went together fairly smoothly so far! Just one thing i'm having trouble with: I can't figure out how to get the horn onto my MX-28 :p, it's really, really difficult to...
  27. Replies
    38
    Views
    31,835

    Re: New Mech: The Kevin

    I'd go with interpolation, it seems to be the preferred method. The Bioloid library has interpolation functions that are really easy to use, so you probably wouldn't have to write too much code.
  28. Replies
    45
    Views
    39,328

    Re: Another AEG design thread

    You may have mentioned this already, but is it possible to power the guns with a separate power source (2s lipo) instead of the dynamixel bus?

    If so, I'll get one too!
  29. Re: Feedback on Phantom Quad MKII and Arbotix Commander kits.

    It's mentioned in the Arbotix manual under "I2C and Serial Headers", the getting setup page under "Upload Pypose Sketch", and the Arbotix hardware overview under "FTDI Serial Port / Programming...
  30. Replies
    45
    Views
    39,328

    Re: Another AEG design thread

    I believe they are micro metal gearmotors from Pololu.

    Edit: Also says so in the agitator description on shapeways.
  31. Replies
    105
    Views
    94,820

    Re: Let's talk 5.8ghz FPV camera setups

    I did a quick latency test with the following system:
    FatShark "CCD Killer" 600 TVL CMOS camera
    FatShark 250mW TX
    ImmersionRC Uno5800v2 RX
    Rubber Duck Antennas (Circularly polarized antennas...
  32. Replies
    105
    Views
    94,820

    Re: Let's talk 5.8ghz FPV camera setups

    Those are the frequencies that Tybs said he will be using. So probably a good choice. (See here, and here)
  33. Replies
    105
    Views
    94,820

    Re: Let's talk 5.8ghz FPV camera setups

    I just did a quick test of my camera system, (details here) and I'm really happy with it. The only thing that's missing is the circularly polarized antennas, which have yet to arrive.

    The video is...
  34. Question(s) Re: How can avoid the jerking of 6-DOF arm made up of AX-12

    I heard that someone else seemed to remember claims that the servos tend to overheat if you use the speed control instead of interpolation (see here). I haven't actually tried it, just something I...
  35. Replies
    8
    Views
    15,976

    Question(s) Re: newbie: AX12 continuous rotation with Arbotix

    Two byte registers will have a low and a high byte, indicated by _L and _H respectively in the preprocessor directives (in the bioloid library) or by (L) and (H) in the ax-12 manual. You should see...
  36. Re: Line Follower with one sensor - Help to improve the code

    First of all, you should use code tags when posting code so that we can read it.

    void loop() //Main program - infinite loop
    {
    LineFinder = digitalRead (52); // voltage measurement of sensor...
  37. Replies
    80
    Views
    86,681

    Re: New Mech Warfare competitor, Pics and Stuff

    Very impressive!

    The only thing I might be worried about is the angle of the hopper. If you have to aim too high (at giger for example) gravity will no longer be your friend ;).

    Looking forward...
  38. Replies
    17
    Views
    22,297

    Re: Serial communication between Arduino and Arbotix

    For the pins, a little google powers or just looking at a breakout board should get you what you need:
    5332
    Just match GRN on the breakout to GRN on the arbotix. Keep in mind that the breakout's tx...
  39. Replies
    105
    Views
    94,820

    Re: Let's talk 5.8ghz FPV camera setups

    That TX/RX kit uses a different channel group than the one Tybs said he would use at the event. I don't know if that will be a problem but at the very least you won't be able to use any RX that Tybs...
  40. Replies
    22
    Views
    79,756

    Sticky: Re: Mech Warfare Weapons Guide

    I might wait until the guide is a little more complete and refined. It's no fun to update and edit things in two separate locations :).


    I believe you can attach files to a post using the paper...
Results 1 to 40 of 214
Page 1 of 6 1 2 3 4