Search:

Type: Posts; User: jwatte; Keyword(s):

Page 1 of 13 1 2 3 4

Search: Search took 0.04 seconds.

  1. Replies
    247
    Views
    80,930

    Project Re: More Mule then Rover?

    It's a robot controlled lift! Stylish!
  2. Re: How to use nrf24l01 wireless module with Arbotix-M Robocontroller & Arduino Mega 2560 r3 to communicate between each other?

    You need to make the appropriate connections to the NRF chip, which includes the SPI bus and the chip-enable signal.
    Any available digital pin "ought" to work for Chip Enable -- it's a low-bandwidth...
  3. Question(s) Re: AX-12A - When Reading Present Position Getting Inaccurate Reading

    A status packet is a response with zero data. They're pretty much the same thing.
    A command packet and an instruction packet are names for the same thing, too.

    It can't possibly be the case that...
  4. Question(s) Re: AX-12A - When Reading Present Position Getting Inaccurate Reading

    I would not expect ser.readline() to return a proper response. The response packet has a very similar format as the command packet, and needs to be appropriately decoded.
  5. Replies
    3
    Views
    301

    Re: Sync_write to multiple servos

    Is the problem in the servos, or with the board/sketch?
    Is this a buffer overflow problem in the "serial tosser" code?
    If you hook up a scope/logic analyzer to the servo TTL bus, does the 10+...
  6. Replies
    8
    Views
    1,160

    Re: PhatomX with XL430-W250 servos

    The receiver outputs this protocol:
    https://github.com/jwatte/donkey_racing/blob/master/teensy_hat_firmware/FlySkyIBus.h
    It's ten 16-bit integers with some surrounding framing information.
  7. Replies
    34
    Views
    13,509

    Re: Numa V2 - Quad Mech

    Peanuts incoming:

    For Onyx (RIP) I defined a "standard leg" where the coordinate system is "forward/back," "out/in," and "up/down."

    The IK solution then runs in terms of this standard leg, and...
  8. Replies
    1
    Views
    213

    Re: Cobot Research and Development

    Looks awesome!

    Make it bus away the table once it's empty, perhaps?

    Sing and dance for birthdays? (and serve/cut cake?)
  9. Replies
    16
    Views
    1,952

    Re: Mech Warfare at Bay Area Maker Faire 2019

    I would love STL files!
    Do these mount to the Double Eagle AEGs, or some other kind?
  10. Replies
    247
    Views
    80,930

    Project Re: More Mule then Rover?

    That sounds exciting!

    Curiousity killing cats:
    How is the "L" part attached? Welded?
    How thick is the plate that the bolts go through?
  11. Replies
    16
    Views
    1,952

    Re: Mech Warfare at Bay Area Maker Faire 2019

    Yeah, some kind of light preload on the feed seems needed. The design I've been using seemed to have a 10-15% dry fire / false load rate.
    The twisty 1/4" spring feed seemed alright, although I don't...
  12. Replies
    8
    Views
    1,160

    Re: PhatomX with XL430-W250 servos

    The U2D2 (and, to be fair, the USB2AX,) both are kind-of expensive for what they are: A $2 chip on a board with some connectors.
    Sure, the market might be only a few hundred, so you'd need a fair...
  13. Replies
    8
    Views
    1,160

    Re: PhatomX with XL430-W250 servos

    I've had great luck with the FS-i6S controller/receiver: https://amzn.to/2T7pP5J The receiver actually spits out a simple protocol of reveived data over serial port, so you don't need to decode the...
  14. Replies
    1
    Views
    630

    Question(s) Re: How can I connect ROS with Unreal engine?

    I've only created Unreal plugins in Visual Studio. There, the integration is actually very nice.

    I imagine if you have an exposed function in your plugin and you can call it from Blueprint, then...
  15. Replies
    247
    Views
    80,930

    Project Re: More Mule then Rover?

    Interesting!

    How do you figure out where the main flex is coming from? Do you have video from the sides while it's doing it?
  16. Replies
    247
    Views
    80,930

    Project Re: More Mule then Rover?

    Only one way to settle this: Build TWO snow plowing mules, one with an aluminum bracket, and one with steel, and measure what the relevant bracket lifetimes are under equivalent workloads!
    ...
  17. Replies
    247
    Views
    80,930

    Project Re: More Mule then Rover?

    Sure, aluminum will fatigue and break, but, you know, they make airplanes out of it. With enough safety margin, you'll be fine :-)

    Anyway, if he wants to make another bracket because he enjoys...
  18. Replies
    247
    Views
    80,930

    Project Re: More Mule then Rover?

    It's the torque, more than the power, that matters for your bracket. Think of it this way: A motor that is stalled develops zero power (at the shaft) but develops a lot of force at the mount!
    You...
  19. Re: How to change the speed of the AX12a and Read its current speed ?

    The value range is documented in the manual for the servo. I don't remember the exactly values, but because it's a 2-byte register, the value range is higher than 0-255.
    The "_L" and "_H" are the...
  20. Replies
    4
    Views
    664

    Question(s) Re: torque control for ax 12a

    Yes, almost all motors of this kind have a continuous duty rating of 20-25% of the maximum instantaneous rating. It's a fact of physics.

    There is another thread on this board about adding external...
  21. Replies
    16
    Views
    1,952

    Re: Mech Warfare at Bay Area Maker Faire 2019

    That's 10 minutes from where I live and 5 minutes from where I work, so ... yeah, I'll have to be there. I'll borrow my daughter's AX-12 based 'mech. (Onyx has donated too many pieces to be...
  22. Replies
    3
    Views
    593

    Re: C program for AX

    Yes, a zero bit is sent as wire-to-ground on the TTL UART bus. It works fine to wire a microcontroller UART straight to the servo, EXCEPT when the servo tries to send a response back, the...
  23. Replies
    6
    Views
    1,032

    Re: XL430-W250 Stop moving randomly

    Are you sure it's the motor? If so, is it signaling an error? (Not reading status back is in general a bad habit, because it makes debugging harder.)

    If you hook up a scope or logic analyzer on...
  24. Re: Dynamixel MX-64T Torque control with Arbotix

    Have you enabled torque with register 24?
  25. Replies
    4
    Views
    664

    Question(s) Re: torque control for ax 12a

    If the servo cannot get to the desired goal, it will generate an error to tell you this. The practice of "set a goal position that is not achievable" is not generally useful for controlling these...
  26. Replies
    6
    Views
    1,032

    Re: XL430-W250 Stop moving randomly

    Not really. The main question is if you have command response turned on; if so, you may have to wait for a timeout if the servo didn't get the packet (because sometimes it's slighlty slow to...
  27. Replies
    4
    Views
    911

    Re: Puppet Master/ Slave setup

    Is the theory that you have two robots, one to capture the pose, and one to play it back?
    That would require software.
    The user "tician" on this board used to support a graduate art program that...
  28. Replies
    3
    Views
    696

    Project Re: Sinusoidal Servo control using MATLAB

    I don't know how fast Matlab can run -- can it run at 100 Hz itself? If not, then you're going to have to live with whatever it can do ...
  29. Replies
    3
    Views
    696

    Project Re: Sinusoidal Servo control using MATLAB

    The best you can do is to send a very high speed stream of updates -- say, 100 Hz -- for where you want the position to be.

    Let the control algorithm and damping inherent in the servo then drive...
  30. Replies
    4
    Views
    911

    Re: Puppet Master/ Slave setup

    The RoboPlus software that comes with the Dynamixel series of servos can do some of those things without programming.
    You have to read the instructions, which are sometimes hard to just FIND, and...
  31. Question(s) Re: Dynamixels AX-12A on OpenCM 9.04 + OpenCM 485: how to send instruction packets

    Here's my setup code for OpenCM 9.04:


    void DxlIO::begin() { afio_remap(AFIO_REMAP_USART1);
    afio_cfg_debug_ports(AFIO_DEBUG_FULL_SWJ_NO_NJRST);
    gpio_set_mode(PORT_TXRX_DIRECTION,...
  32. Replies
    4
    Views
    581

    Question(s) Re: Dynamixel Robotis AX12A - half duplex

    1. Yes, if you set the register to 1, then there will only be an acknowledgement from the servo for a READ command.

    2. You can tie the TX and RX lines together. That will make the RX line receive...
  33. Replies
    4
    Views
    581

    Question(s) Re: Dynamixel Robotis AX12A - half duplex

    Yes, you can set the response level to make it quiet. Check the documentation for register 16 (Status Return Level)...
  34. Replies
    247
    Views
    80,930

    Project Re: More Mule then Rover?

    Btw, the CC/CV lead/acid cycle that works for me is:

    - Set constant voltage to 14.5 V
    - Set constant current to something less than the Ah rating of your battery, but in A (i e, <= 1C rate)
    -...
  35. Replies
    247
    Views
    80,930

    Project Re: More Mule then Rover?

    Looks cold. Better the robot than me :-)

    Lead-Acid are slow-charging batteries; there's really no (safe) way around that. You can charge them with a benchtop power supply set at constant-voltage...
  36. Replies
    247
    Views
    80,930

    Project Re: More Mule then Rover?

    Such an awesome remote drone :-)
  37. Replies
    247
    Views
    80,930

    Project Re: More Mule then Rover?

    I imagine the WiFi and cameras use wall warts plugged into the 110V inverter?

    I then imagine you could use a wide-input-range buck regulator (or two) to output the appropriate voltage for each of...
  38. Replies
    1
    Views
    572

    Discussion Re: controlling dynamixel mx-64at

    If you want to use multiple batteries, then you need to create custom Dynamixel hub boards.
    The board would pass the serial signal/s and the ground signal through, but would disconnect the 12V...
  39. Replies
    7
    Views
    2,361

    Re: RoboGames cancelled?

    I hate Maker Faire because it's so crowded and noisy, but if there's a dedicated spot for Mech Warfare, it's a very convenient drive or train ride for me, so I could totally do that. Assuming I could...
  40. Replies
    1
    Views
    508

    Question(s) Re: controlling dynamixel mx-64at

    A pretty easy way to control these servos is to use the OpenCM 9.04 board, and the Robotis library that has built-in functions for sending commands to the servos.

    A single 11.1V LiPo battery will...
Results 1 to 40 of 500
Page 1 of 13 1 2 3 4