At this point, I expect this is unlikely to happen? But maybe late May is far enough out (I have my doubts).
Type: Posts; User: Gertlex; Keyword(s):
At this point, I expect this is unlikely to happen? But maybe late May is far enough out (I have my doubts).
I could probably make it, though no guarantees. Good incentive to get more work done in the next ~3 months :D
Make sure they'll refund you if they decided to cancel due to covid-19 :D
Quick question for helpful context: which Xbees are you using?
I don't actually have experience with Interbotix, or with writing my own MoveIt code, but here's one library for python use of MoveIt: https://github.com/mikeferguson/moveit_python. That might help...
Like jwatte, I live in the terminal and use vim, so can't help regarding IDEs, but I feel like what I describe below is fairly close to "the right way" when workign with ROS.
From my own...
I'd be interested (I'm in San Jose). The best bet for an arena is if the guys from Tucson want to make the trip to Rocklin with their arena. Otherwise, the work needed to get a working arena and...
My writeup of Numa2 over at hackaday.io is finally up!: https://hackaday.io/project/166096-numa-2-14-dof-mech-warfare-robot
At Bay Area MakerFaire 2019, I believe Numa 2's record was L-W-W-L, and...
Certainly allowed to discuss other communities! If anything, this community and others used to be more active. These days, apparently, kids just want to be youtube/twitch stars.
Those of us here...
Some comments on the Numa v Mech99 match:
- This was a really fun match!
- I didn't find out until after that 99 had a busted leg servo, thus I had no idea about its immobilization right around the...
It's bidirectional via xbee. My data rate from the robot is to send one row of data (12 bytes) every 4s or so. I'm actually doing a single read of a single servo's temperature once per second, and...
At Maker Faire 2019, I had Numa 2 sending temperature information back over the Xbee. I had my added-on Wixel in turn relaying that to my computer. The goal here was to be able to monitor...
That's impressive! Nice work. Diving right into the fun stuff next, or doing more refinement first?
Similarly, here's a Hack-A-Day feature from earlier today about BAMF!
https://hackaday.com/2019/06/07/mech-warfare-like-driving-a-building-sized-robot-through-a-busy-city/
Try some different wires, too, to rule that out.
A while ago I was looking at my original Numa thread and wondering why I had so few updates leading up to Robogames. Well now I'm reminded. The list of things to do is never ending (well, I wrote it...
Now that's a tease! (There's nothing to see there other than a grey restricted icon thing, it seems)
20 lbs is insane sounding :D
I should also document the 3d-print encapsulated switch wired to one of the push buttons, giving me the ability to set a mode. E.g. TwitchMX's turret mode + laser was toggled in this manner :)
It sounds like at most locations, same aisle as the elbow grease. :-D
I realized that with the Wixel on my Arbotix commander, if instead of forwarding the bytes generated by the commander, I instead forwarded the bytes received by the commander's xbee (i.e. from the...
Awesome, thanks for the pics!
Thanks for the pictures! Am I correct in understanding that the back panel will have 3 (or 4?) connectors, plus an integrated 1S battery (I don't recall where I read that).
Assuming we're using this same setup next month, can we get dimensions of where the 4pin connector is located on each score panel? I want to make sure I have clearance for the cable that will plug...
I recently did 3 more servos, so I have four on Numa2. My own finding was that a dremel is slower and not needed with the AX12 case. Instead, I used a trapezoidal razor blade. Scored lines for the...
Still gotta weigh it. I'm worried it weighs more than I intended, but I can't find my numbers for the original Numa's total weight.
The positioning of servos 2 and 3 is pretty much just what I decided looked good, and enabled a good range of motion of the ankle.
What's your take on that choice? It sounds like you have opinions...
Lot's left to do. But looking really goood.
7488
Great to see you still have the itch! For the sake of your servos, I would suggest you do some torque calculations to see the loads on your servos with that leg design.
The key number is going to...
I'm continuing to progress nicely, especially recently. But for the moment, I have a question for the peanut gallery:
Problem: For a given leg geometry, AX-12s can be mounted in two ways,...
There's a real chance Numa2 will be ready...!
7460
Do we know registration, etc. deadlines for this yet?
Sadly I haven't and don't forsee finishing my mech in time for December. :(
looks at calendar
So, in the last ten months, I've been very slowly progressing... Hasn't helped that (1) I'm always busy with work and (2) work is very similar, cognitively to the stuff I am...
Hmmmm looks like I missed the registration deadline. Oh well, I'll shoot for joining you guys for a weekend in Arizona this winter :). Twitter suggests the registration deadline was March 16; I...
I bet it will survive the few years before his next iteration! :D
Looking marvelous as always, Tommy!
While I've played with a RPiA, I've never used the zero. I certainly wouldn't want to be running raspbian, and I don't have any desire to experiment with more minimal OSes... so the pyboard is...
More slow progress, mostly yesterday. Got the pyboard properly communicating with the motor drivers. It was a series of mistakes that I had to find along the way to getting that working. It seems...
Switched to a pyboard instead of the hydrabus. It's only disadvantage is fewer mounting holes. And maybe that I like blue more than green :P
Correspondingly made a perf-board shield for the...
Awesome work, and great documentation so far! :) The bot is very clean looking!
Looking forward to more.
That is a good point, heh. Not 100% sure I'll use the minification always, either, as you can live-debug with the python interpreter running on the board. I may need that for debugging frequently :|
Still working on this! Slowly. Satisfying things I've accomplished sporadically:
- Desoldered the ARM chip off my Hydrabus and procured replacement (from china, hopefully not fake); haven't...
The wires going to the board are all non-moving. The runtime of the robot is measured in tens of hours at most, and so I won't be worrying about these wires. The ones between the servos on the...