Search:

Type: Posts; User: MikeG; Keyword(s):

Page 1 of 7 1 2 3 4

Search: Search took 4.82 seconds.

  1. Replies
    8
    Views
    10,753

    Project Re: IK Video of a Planar 2R AX-12 Arm

    You can start by reading the openly published source code from the link on post #1? Who's we? Is this a school project?
  2. Replies
    1
    Views
    2,831

    Re: "Dynamixel AX-12+ Actuator Latencies"

    Does anyone else find this paper a little weird?

    Edit: I should explain myself and define weird. First processing the serial signal. That takes some time. The result is a PWM signal.

    At...
  3. Replies
    1
    Views
    2,049

    Internet controlled LED

    Have you ever wanted to turn an LED off and on over the internet? Well guess what, your search is over.

    http://www.agaverobotics.com/spinneret/controlpanel.htm

    I know... silly... but a lot of...
  4. Replies
    11
    Views
    7,139

    Re: N00b Question About WiFi Controlled Humanoids

    You could look for someone in the animatronics field to give you a hand. As stated, the Internet connectivity part is fairly straight forward.
  5. Replies
    11
    Views
    7,139

    Re: N00b Question About WiFi Controlled Humanoids

    Internet control can be accomplished with an internet connected laptop running a custom program. Laptop on wheels?

    You need a robot facade and motor control which is most likely a custom build. ...
  6. Thread: Servo mirroring

    by MikeG
    Replies
    4
    Views
    3,174

    Question(s) Re: Servo mirroring

    Billy absolutely right.

    I use trig functions so position calculations are not coupled to the AX-12 hardware values. Then simply convert angles to AX-12 goal position. Also the center value of 150...
  7. Replies
    10
    Views
    10,082

    Question(s) Re: Multiple USB2Dynamixels?

    Or you could create a dynamic array of FT_HANDLE pointers. There's several ways to handle the situation all involve code updates but nothing major.
  8. Replies
    10
    Views
    10,082

    Question(s) Re: Multiple USB2Dynamixels?

    If you want to use the API with 2 FTDI chips then you need to identify the FTDI device. You can do accomplish that with an index (FT_Open) or name using FT_OpenEX. The USB2Dynamixel API is just an...
  9. Replies
    10
    Views
    10,082

    Question(s) Re: Multiple USB2Dynamixels?

    Since you mentioned dxl_read_word and dxl_write_word, I'm assuming you're using the USB2Dynamixel API. The API uses the FTDI's FTD2XX DLL not a virtual com port. You have to modify the...
  10. Replies
    1
    Views
    8,784

    Re: Access Denied to Port??!!

    The port is probably already open or the context that your code is is running under does not have access to the resource. Probably an open port from a downstream error. Just a guess because I don't...
  11. Replies
    62
    Views
    26,693

    Re: An robot programming idea in Python

    I absolutely agree Jes1510
  12. Replies
    4
    Views
    5,415

    Question(s) Re: Electronic Brick to axon!

    I'm sure someone will correct me but it looks like the Electronic Brick Chassis (v1.1) is designed from an ardunio? The brick exposes the Ardunio's pins through 10 and 3 pin connectors. The Brick...
  13. Re: Robot goals. What are you trying to achieve with your robot?

    ROS looks very nice. What do you think of the decision to use XML-RPC over SOAP?
  14. Re: Robot goals. What are you trying to achieve with your robot?

    What about a distributed architecture? Several months ago, I built a small IK web service that takes D-H parameters and end points as arguments. The web service crunches the math and replies with a...
  15. Project Re: Non-Tech needs help with a project and willing to pay

    Mathew;

    The ball is in your court. I just need to verify your requirements. Then I'll create a requirements document which will also outline our responsibilities for this project. If we both...
  16. Project Re: Non-Tech needs help with a project and willing to pay

    @Al1970 and zoomkat, you're right the requirements a little thin.

    The ballpark cost (and time) I provided is called a ROM (rough order of magnitude). This is the 40,000 foot view of a project and...
  17. Project Re: Non-Tech needs help with a project and willing to pay

    @darkback2 the pressure sensors mentioned are variable resistors. They start off at a very high resistance and go around 1M depending on the force applied. Off the top of my head, the response...
  18. Project Re: Non-Tech needs help with a project and willing to pay

    It pretty easy to drop electronics is a standard plastic enclosure with cutouts for the LCD , buttons, and connections. Plastic enclosures are pretty common and can be found in most electronic...
  19. Project Re: Non-Tech needs help with a project and willing to pay

    What's described is a pretty a simple project. It should take someone a weekend to put it together.

    Items
    LCD
    Force Sensing Resistor
    Microcontroller
    Plastic pad

    So what are you willing...
  20. Replies
    3
    Views
    5,694

    Question(s) Re: Servos causing Ardweeny Resets/Hangs

    Glenn, it's easier for people to help you if you post a schematic (or description) and your source code.
  21. Replies
    4
    Views
    6,431

    Project Re: Using USB-I2C adapter

    You provided the manual for the USB-I2C and the manual states…

    Reading 3 bytes from slave device 0x50 starting internal address 0x00 would be,
    0x55 0x51 0x00 0x03

    I understand...
  22. Replies
    4
    Views
    6,431

    Project Re: Using USB-I2C adapter

    The "Reading from I2C devices with a 1 byte internal address register" sections states

    "This is similar to writing, except that you should add 1 to the device address to make it an odd number....
  23. Replies
    3
    Views
    6,009

    Re: Dynamixel position accuracy, calibration

    I ran in to a similar situation, where the AX-12s were overshooting the mark a bit. Slowing the motors down helped.
  24. Replies
    9
    Views
    15,378

    Project Re: Handmade 5DOF Manipulator with tactile feedback

    Cool... My son and I visited the local hardware store this weekend to pick up materials to build the links.

    Do you have the Supermodified v2 boards? I pre-order them a month or two ago and I'm...
  25. Replies
    9
    Views
    15,378

    Project Re: Handmade 5DOF Manipulator with tactile feedback

    That a very nice arm and control system. I really like the rotary gripper.

    I per-ordered supermodified v2 a while back with the plan is to build a 6 axis robotic arm.
  26. Re: Timeout problem with Forest Moon Dynamixel library

    Sounds good, let me know if you have any question about the source code.
  27. Re: Timeout problem with Forest Moon Dynamixel library

    Like I said, you simply send t<cr> while in manage mode. I followed this method because that's how the Robot Terminal works. If you want to start with the manage LED blinking (selection mode) then...
  28. Re: Timeout problem with Forest Moon Dynamixel library

    The display you posted is exactly what happens when the manage LED is blinking when you send the "t". The order is

    1) Open the port
    2) Place the CM-5 in manage mode - The manage LED is solid
    3)...
  29. Re: Timeout problem with Forest Moon Dynamixel library

    As I explained, you have to place the CM-5 in manage mode first!
  30. Re: Timeout problem with Forest Moon Dynamixel library

    Sorry, gave you the wrong dll. That should not have stopped you from controlling a servo though. Anyway, this one will display everything going through the serial port....
  31. Re: Timeout problem with Forest Moon Dynamixel library

    Right just enter a "t" and click the button to enter toss mode. I modified the exe to give give you a response that you're in toss mode. No need to enter a 0x0D, I'm doing that in the code which is...
  32. Re: Timeout problem with Forest Moon Dynamixel library

    To enter toss mode, send a "t" and a CR (0x0D) after entering manage mode on the CM-5.

    Download the binaries on http://www.agaverobotics.com/services/dotnet/Dynamixel/default.aspx, setup the...
  33. Replies
    7
    Views
    5,226

    Re: Starting with robotica

    You can add as many standard hobby servos as you have IO pins - well kinda' but that's for another time.

    A dedicated RC servo controller can be used to off load main processor resources. The...
  34. Re: Timeout problem with Forest Moon Dynamixel library

    I guess I don't understand. Why can't you connect the USB2Dyanmxel to an ITX USB port then to the AX-12 bus?
  35. Re: Timeout problem with Forest Moon Dynamixel library

    Amazon.com: Medialink - Wireless G USB Adapter - 802.11g - 54Mbps - Windows 2000 / XP / Vista 32-Bit / Vista 64-Bit / Windows 7 Compatible: Electronics
  36. Re: Timeout problem with Forest Moon Dynamixel library

    USB wifi?
  37. Re: Timeout problem with Forest Moon Dynamixel library

    Here's the problem... the AX-12 network is a 1/2 duplex 1Mbps (default) serial bus. The Bluesmirf is a full duplex 9600 to 115200 bps serial bus.

    A full duplex bus uses one wire for transmit and...
  38. Re: Timeout problem with Forest Moon Dynamixel library

    The CM-5 is a great controller and designed to be used with the Bioloid software. That constraint might limit your project - might not.
  39. Re: Timeout problem with Forest Moon Dynamixel library

    I have other code... still has a bug in the response parser... but you're welcome to it. It uses listeners to update memory resident Dynamixel control table objects.
  40. Re: Timeout problem with Forest Moon Dynamixel library

    Yes it does.

    The Forest Moon stuff is very well written.

    I'm not the brightest bulb on the strip so I wrote USB2Dynamixel code that worked for my brain. Each instruction is a class....
Results 1 to 40 of 277
Page 1 of 7 1 2 3 4