Search:

Type: Posts; User: LloydF; Keyword(s):

Page 1 of 7 1 2 3 4

Search: Search took 0.03 seconds.

  1. Replies
    124
    Views
    40,084

    News/Announcement Re: The Robotis TurtleBot3

    LOL and unfortunately there is no RTC (Real Time Clock) on this model.:tongue:
  2. Replies
    14
    Views
    4,141

    News/Announcement Re: Turtlebot3 with Openmanipulator

    Sweet! Got the pick and place example to work. It would seem there was a typo, on there web page.
    On section 9.1.3.3, after launching the arm initialization routine, they use this command line to...
  3. Replies
    124
    Views
    40,084

    News/Announcement Re: The Robotis TurtleBot3

    75187519

    The fan was overkill as I have never been able to get it hot enough to turn on:sad:
    Once booted onto the USB this is a full on speed demon with V2 camera and as far as I can tell a...
  4. Replies
    124
    Views
    40,084

    News/Announcement Re: The Robotis TurtleBot3

    I noticed that most, if not all the TB3 files are now on ROS Melodic Ubuntu 18.04 :happy:
    Has anyone tried running the TB3 on Ubuntu 18.04 yet?
    I have this new SBC the Jetson NANO. I configured...
  5. Replies
    14
    Views
    4,141

    News/Announcement Re: Turtlebot3 with Openmanipulator

    God knows what happened, but I rebuilt Ubuntu and the ROS packages and everything is Okay now :o
    This was easier than running all them bug reports. (Note. Found if you are playing with the End...
  6. Replies
    14
    Views
    4,141

    News/Announcement Re: Turtlebot3 with Openmanipulator

    Hum, that last link may be useful, thank you.
  7. Replies
    14
    Views
    4,141

    News/Announcement Re: Turtlebot3 with Openmanipulator

    I am so unhappy. The dynamixel-workbench will no longer compile, which make the arm :confused: dead. I hope they fix it, not sure how to get
    one of there programmers to look at what the hell he is...
  8. Replies
    49
    Views
    34,946

    Sticky: News/Announcement Re: HR-OS1 Documentation

    I updated everything an ran it on Ubuntu Mate, installed ROS, because i have plans :cool:, and everything seems to be working, with a little work on the ps3.
  9. Replies
    124
    Views
    40,084

    News/Announcement Re: The Robotis TurtleBot3

    I have had issues with rubber products and the dry hot air of Arizona ( just nasty to most plastic's). Anyhow when I printed
    out these wheels they have three groves in them that are exactly the size...
  10. Replies
    14
    Views
    4,141

    News/Announcement Re: Turtlebot3 with Openmanipulator

    I am happy to report that I have been able to get everything working, with the exception of the RC100 joystick with the OpenManipuiator. It should work but hum:confused: I am still working on that...
  11. Replies
    14
    Views
    4,141

    News/Announcement Re: Turtlebot3 with Openmanipulator

    7453
    The default configuration for the manipulator is on the u2d2 or a USB serial connection, and it works really well.
    They have a direct link to some STL files for 3-D printers, so I printed some...
  12. Replies
    124
    Views
    40,084

    News/Announcement Re: The Robotis TurtleBot3

    I printed out and put the tire and caster configuration from the turtlebot3 friends Carrier, onto my tb3 to see if it would help with getting up onto carpets. It worked and works, giving me just...
  13. Replies
    14
    Views
    4,141

    News/Announcement Re: Turtlebot3 with Openmanipulator

    744374447445
    Here it is. I downloaded the build instructions, as this one comes with no instructions, but useful links :wink:
    There Disclaimer really needs to be more visible. i.e Base plate is...
  14. Replies
    14
    Views
    4,141

    News/Announcement Re: Turtlebot3 with Openmanipulator

    Well with that out of the way it's back to waiting for a package :tongue:.
    Look at the http://www.robotis.us/ site they have a frame set and a heavy base plate for the manipulator.
  15. Replies
    14
    Views
    4,141

    News/Announcement Re: Turtlebot3 with Openmanipulator

    :o Thank you. I found page 248 in the book were you press the reset and switch 2 which forces the boot-loader to run, yea!
    That really had me thinking I bricked my boards when I noticed, I was not...
  16. Replies
    14
    Views
    4,141

    News/Announcement Re: Turtlebot3 with Openmanipulator

    LOL. It is not even here yet and I am having issues.
    I tried to update a OpenCR board and now I have two OPenCR bricks.:confused:
    Sigh looks like hours of entertainment, starts now.
  17. Replies
    14
    Views
    4,141

    News/Announcement Turtlebot3 with Openmanipulator

    It seem it is being renamed the Openmanipulator-x now.
    http://emanual.robotis.com/docs/en/platform/openmanipulator_x/overview/
  18. Replies
    124
    Views
    40,084

    News/Announcement Re: The Robotis TurtleBot3

    This is my Burger now with voice and vision ;)
    7426
    I found this: RASPIAUDIO.COM Stereo onboard speaker with Sound Card (AUDIO+SPEAKER) for Raspberry Pi Zero/Pi3/PI3B/PI3B+/Pi2/ with Better quality...
  19. Replies
    124
    Views
    40,084

    News/Announcement Re: The Robotis TurtleBot3

    Looks like ROBOTIS has a new disk image for the TB3 out and, a firmware update to (v1.2.1) :wink:
  20. Replies
    124
    Views
    40,084

    News/Announcement Re: The Robotis TurtleBot3

    Just a thought but, getting ROS and a turtlebot up and running with a book that covers you're platform, and written very well, is a
    amazing deal. It's the documentation that I like to read over and...
  21. Replies
    124
    Views
    40,084

    News/Announcement Re: The Robotis TurtleBot3

    Odd, while building a new TB3 I could not get the motors ID#one and two to work.:sad:
    I only had to program them on the U2D2 and set the ID's before.
    This time I had to use the Arduino Example...
  22. Replies
    124
    Views
    40,084

    News/Announcement Re: The Robotis TurtleBot3

    Yea! Thank you for the heads up.:wink:
    I order a few sensors to play with, now that i am all updated, seems you had a lot to do with making this happen, thank you.
  23. Replies
    124
    Views
    40,084

    News/Announcement Re: The Robotis TurtleBot3

    Wow! Sweet thank you for sharing:veryhappy:.
  24. Replies
    124
    Views
    40,084

    News/Announcement Re: The Robotis TurtleBot3

    Woot! Woot! I am happy to say everything seems to be working on the Up board with a dual band A/C wifi dongle, and did not have to add on thing more to swap out the intel joule on the waffle with the...
  25. Replies
    124
    Views
    40,084

    News/Announcement Re: The Robotis TurtleBot3

    Sweet, I missed the manipulator, this should be fun.:wink:
    (dude you do way more programing than most so, rock on)!!
    I mean with spring here and all.:o
    I will have to head on over there and...
  26. Replies
    124
    Views
    40,084

    News/Announcement Re: The Robotis TurtleBot3

    I did a direct swap out of the intel joule and the new up board, I did have to add a edimax AC wifi dongle, it uses the rtl8812au which is easy to find drivers for, so I got Dual AC WiFi up and...
  27. Thread: UP Board

    by LloydF
    Replies
    35
    Views
    21,634

    Discussion Re: UP Board

    Hum, I got my new UP Board today with the robot development kit from Intel. I got a account with Intel and downloaded there latest ISO and was able to boot up to Ubuntu 14.04 and then Upgraded to...
  28. Replies
    124
    Views
    40,084

    News/Announcement Re: The Robotis TurtleBot3

    Yikes hum, it looks like July before a new Ubuntu-Mate or one can go through acrobatic connotations for Ubuntu-Mate now, hum:rolleyes:.
    Nope I'll wait on that one. Thanks for the heads up. This...
  29. Replies
    124
    Views
    40,084

    News/Announcement Re: The Robotis TurtleBot3

    The Raspian desktop image from Robotis works with the RPI3B running it first, I'll give the Mate version a test today.
    (Note Tested it out and the Ubuntu Mate version will not boot at all on...
  30. Replies
    124
    Views
    40,084

    News/Announcement Re: The Robotis TurtleBot3

    That is annoying. I had to set up the SD card for the RPI3 before it would boot on the new RPI3B+. Hum?:confused:
  31. Replies
    124
    Views
    40,084

    News/Announcement Re: The Robotis TurtleBot3

    Movidius Neural Compute Stick

    The Neural Compute Stick (NCS) is a tiny computer meant to accelerate the execution of neural networks. The entire hardware is packed into a USB-stick which is...
  32. Replies
    124
    Views
    40,084

    News/Announcement Re: The Robotis TurtleBot3

    Oh, yea the new RPI3B+ needs a fast sd card or it will not boot, I only had 2 out of 5 that were fast enough class 10's to boot lol.:o
    (NOTE. I was totally wrong here read on)
  33. Replies
    124
    Views
    40,084

    News/Announcement Re: The Robotis TurtleBot3

    Got the Intel Movidius neural Compute sticks running on the Raspberry PI3 B+ :rolleyes: using the ROBOTIS image. It just needed it's
    source files updated. Will move it into my turtlebot3 now. I am...
  34. Replies
    124
    Views
    40,084

    News/Announcement Re: The Robotis TurtleBot3

    Grats! The Book is worth it's weight in gold.:tongue:
  35. Replies
    124
    Views
    40,084

    News/Announcement Re: The Robotis TurtleBot3

    When the power gets to 11.0v on the battery you will hear the buzzer go off on the OpenCR board, it is a UPS system so just plug the 12v power supply with adapter into the OpenCR board and you can...
  36. Replies
    124
    Views
    40,084

    News/Announcement Re: The Robotis TurtleBot3

    It looks like ROBOTIS USA has released there TBS Waffle PI, Yea!:cool:
    I love my TB3 Burger but there is little to no room to add more sensor improvements,
    like the Movidius neural Compute...
  37. Replies
    124
    Views
    40,084

    News/Announcement Re: The Robotis TurtleBot3

    Look at step 7 http://emanual.robotis.com/docs/en/platform/turtlebot3/overview/ there is a second RPI3 image were, they have pre-installed ROS and the ROS-packages related to the TurtleBot3. It ...
  38. Replies
    124
    Views
    40,084

    News/Announcement Re: The Robotis TurtleBot3

    How about that! The Remote controller for the TB3 from ROBOTIS the (RC-100B) has its code built into the tb3 OpenCR board so you can remotely control it pretty much anyplace, like a remote...
  39. Replies
    124
    Views
    40,084

    News/Announcement Re: The Robotis TurtleBot3

    Nice, The only problem that Robotis seems to have is that the web-page people don't appear to be actual TB3 programmers and are not communicating with the programmers well. The Examples, are a good...
  40. Replies
    124
    Views
    40,084

    News/Announcement Re: The Robotis TurtleBot3

    LOL and now the waiting begins. :happy:
    Other than no heat sinks for you PI, I believe you will be happy .
Results 1 to 40 of 277
Page 1 of 7 1 2 3 4