Search:

Type: Posts; User: Chench; Keyword(s):

Page 1 of 2 1 2

Search: Search took 0.00 seconds.

  1. Replies
    111
    Views
    155,309

    Contest Entry Re: MorpHex, a sphere formed morphing hexapod

    Great stuff as always Zenta! PS you're on the front page of engadget :-) .
  2. Replies
    53
    Views
    49,428

    Re: The Ultimate Arbotix Thread

    Hey guys, just a quick question out of interest: -
    There is an "ArbotiX+" defined in the arduino environment after installing the ArbotiX stuff. It is defined in boards.txt as using the Atmega1280....
  3. Replies
    10
    Views
    123,741

    Project Re: Prospero: Robotic Farmer

    Very impressive! I like how it is designed to do something out in the real (and messy!) world. Have you set in loose in a garden or field yet? Also the systems for marking the ground and planting the...
  4. Replies
    13
    Views
    58,399

    Project Code

    Spent several hours this weekend on re-organising the code. This has added absolutely no functionality at all but it will make it a lot easier to do interesting things in future (: . I have had a...
  5. Replies
    7
    Views
    15,819

    Re: Cire's Simple Biped

    Hey, looks promising! I think there is a potential to save a lot of weight by using this mechanism as it eliminates the need for as many DOF. I saw this video a few months ago which impressed me with...
  6. Replies
    13
    Views
    58,399

    Project Update

    Hi guys,
    Finally got back to this project and did a bit of work. I started using the Maestro speed commands to control the rate at which the servos move to their new position. This helped a lot with...
  7. Replies
    13
    Views
    58,399

    Project Re: Low Cost Hexapod

    Well the weather has been too nice to do much robotics recently. Perfect for r/c helicopter flying though :) . Anyway I have made some progress since my last update.

    - Altered the code for the...
  8. Thread: Bioloid LiPo's

    by Chench
    Replies
    16
    Views
    17,682

    Question(s) Re: Bioloid LiPo's

    Hmm, I'm getting confused now. . . I find it a lot easier thinking in terms of coulombs rather than volts. A coulomb is the amount of charge that moves when an amp flows for a second, so it's...
  9. Replies
    6
    Views
    6,686

    Discussion Re: Nokia N900 and Bioloid

    Sounds pretty cool. Does the phone have a hardware serial port available? If it does, you should be able to convert to half-duplex and talk directly to the Ax-12 servos. If not, you'll need to use a...
  10. Thread: Bioloid LiPo's

    by Chench
    Replies
    16
    Views
    17,682

    Question(s) Re: Bioloid LiPo's

    Tyberius,
    I think that should be "A discharge", "42 A" and "84 A", rather than Ah.
    A = amps, unit of current
    Ah = amps x time, unit of charge, or a stand-in for energy (i.e capacity)when voltage...
  11. Thread: Arduino & AX-12

    by Chench
    Replies
    16
    Views
    19,144

    Question(s) Re: Arduino & AX-12

    It might well do . . . Sounds like your project and Fergs' comms code would pretty much cover it. I'd like to be able to customise it to use the particular sensors / outputs I needed, but with it...
  12. Replies
    5
    Views
    9,580

    Re: Board to PDA adapter??

    Actually it could work - some PDA's do support USB host - but I'd definately have a look on the internet to see if your model has host functionality before doing any spending.
  13. Replies
    2
    Views
    30,236

    Re: Roborealm vision software for Roboard

    Roborealm also has a pretty comprehensive API for running it on a remote PC using t'Internet/LAN if 15 fps wont do the business. Just to be clear altwolf - is that the issue with the Nao humanoid on...
  14. Thread: Arduino & AX-12

    by Chench
    Replies
    16
    Views
    19,144

    Question(s) Re: Arduino & AX-12

    Sounds good!
  15. Thread: Arduino & AX-12

    by Chench
    Replies
    16
    Views
    19,144

    Question(s) Re: Arduino & AX-12

    Yes, I know, but you are limited to reading analog and digital pins. You couldn't, for example, read pulse widths, read/write serial communications or i2c, control r/c servos etc. I'm sure it'd be...
  16. Thread: Arduino & AX-12

    by Chench
    Replies
    16
    Views
    19,144

    Question(s) Re: Arduino & AX-12

    Ah I see. I haven't played with an Arduino so I'm not completely clued up on it. Just out of interest, do you think an Arduino would make a decent sensor server on the AX-12 bus? I.e. read a few...
  17. Thread: Arduino & AX-12

    by Chench
    Replies
    16
    Views
    19,144

    Question(s) Re: Arduino & AX-12

    I'm pretty sure the Arduino can do software serial on any pin though, up to 9600 baud or something. But the ArbotiX seems to be a pretty much ready made controller for all the Robotis servos, in that...
  18. Replies
    126
    Views
    91,291

    Re: The Ultimate Phoenix Thread

    I'm finding it a bit hard to follow the notation you're using, but I think I can see how you're going about it.
    If you assume the corner legs are always offset by 60 degrees, will you be able to do...
  19. Replies
    42
    Views
    57,777

    Contest Entry Re: Zenta's first biped

    A fine brood of robots you have Zenta. I've always wondered how you managed to do so many simultaneous movements eg. in your A-pod videos. Now I know, that controller is ingenious. I'm looking...
  20. Replies
    13
    Views
    58,399

    Project Re: Low Cost Hexapod

    Quick update:
    The Pololu Maestro 24 turned up in the post today (or yesterday; had to pay VAT on it though :( ). It's a lot more compact than the SD21!

    ...
  21. Replies
    9
    Views
    13,796

    Re: 2.4 Ghz FPV cameras

    I've read a few stories of FPV planes using 2.4GHz video cameras getting shot down by WiFi. I think 900 MHz video transmitters are also pretty popular as they tend to suffer less from this sort of...
  22. Replies
    126
    Views
    91,291

    Re: The Ultimate Phoenix Thread

    Sounds good! So you work out the local rotation the global rotation produces, then do the rotation equations/matrices to local coordinates, and then convert the rotated coordinates back to global?
  23. Replies
    13
    Views
    58,399

    Project Re: Low Cost Hexapod

    Ok, I got it walking today. I still need to get the wiring sorted out as it barely fits in the body and I need to extend another three servo cables. I also haven't thought about where the battery is...
  24. Replies
    13
    Views
    58,399

    Project Re: Low Cost Hexapod

    All in good time :). For now here's some more pics. The legs are mounted up so you can see roughly how it's going to look. I still have to centre all the servos though. I've got a graphical (Windows...
  25. Replies
    13
    Views
    58,399

    Project Re: Low Cost Hexapod

    I've actually got the basics pretty much nailed down on the IK side of things. Most of the work was in getting the gait and rotation equations equations worked out, but they appear to be working now....
  26. Replies
    13
    Views
    58,399

    Project Low Cost Hexapod

    I became interested in hexapods after seeing Matt Denton's MSR-01 and Zenta's A-pod and Phoenix. I'm studying engineering so I decided to put some of the maths to use and write my own hexapod control...
  27. Replies
    289
    Views
    329,816

    Re: EX-106+/RX-64 Humanoid Robot: Giger

    Cool, looking forward to that!
  28. Replies
    289
    Views
    329,816

    Re: EX-106+/RX-64 Humanoid Robot: Giger

    Is that the same hex that was carrying a video camera in the botjunkie video? i'd love to see some robot's eye footage of the action.
  29. Replies
    5
    Views
    6,286

    Question(s) Re: Bluesmirf to AX-12 bus

    iBot, that was the conclusion I had come to, I'm going to look into the using the flow control lines.
    I think maybe your transistorbcircuit would be the easier route to go down, Mike, as it avoids...
  30. Replies
    5
    Views
    6,286

    Question(s) Re: Bluesmirf to AX-12 bus

    Thanks for your advice.
    The Bluesmirf acts as a serial 'pipe' so hopefully I won't need a micro in between. Shorting the Rx/Tx lines is the method I use to test the Bluesmirf but I'm not sure if...
  31. Replies
    5
    Views
    6,286

    Question(s) Bluesmirf to AX-12 bus

    Hi guys,
    I wondered if anyone had experience connecting a Bluesmirf bluetooth serial module directly to the AX-12 bus. I know that the CM5 controller is able to take commands over serial but I would...
  32. Replies
    125
    Views
    601,233

    Project Re: A-pod, an ant inspired hexapod

    Great work. The movements are really refined, like the mechanics. Roughly how long does it to process the IK, rotation functions etc. for each cycle?
  33. Replies
    97
    Views
    101,505

    Just For Fun Re: The ultimate robot video collection

    Haha, never gets old for me. I'm trying to get hexapod code working just now, and A-pod is very inspiring.
    Awesome, can't wait to see it.
  34. Replies
    97
    Views
    101,505

    Just For Fun Re: The ultimate robot video collection

    Zenta is very modest, but this definately belongs here.

    http://www.youtube.com/watch?v=0jyBiECoS3Q
  35. Replies
    4
    Views
    5,760

    Discussion Re: Link Cell Phone to Microcontroller

    I've had success using a phone to talk to a Picaxe microcontroller via a Bluesmirf. Its on my blog here. I've seen a few other projects doing this too - Miss Alignment, for example.
    Are you planning...
  36. Replies
    6
    Views
    9,005

    Re: Hello. I'm new to building robots...

    +1 on Lets Make Robots. Have you seen their start here robot? http://letsmakerobots.com/start . That's what really got me interested in robotics last year. You can get into altering the robot's...
  37. Replies
    4
    Views
    7,379

    Re: New Mac User, with CNC Dreams...

    If you have an Intel Mac (one of the newer models) you can install Windows along with Mac OS via Bootcamp. Thats what I use for Roborealm, Visual Studio etc.
  38. Replies
    4
    Views
    11,766

    Project Re: iHexi - The iPhone controlled Hexapod

    Sweet. How do does the iphone talk to the robot?
  39. Replies
    33
    Views
    51,062

    Re: A BRAT based Mech, "Miss Alignment"

    Haha I have my moments. Credit goes to Wimo's creator though, he gave me the idea. I'm actually working on a somewhat similar project myself and I'm just trying to get the bluetooth working now. I...
  40. Replies
    33
    Views
    51,062

    Re: A BRAT based Mech, "Miss Alignment"

    Hi there, I think your project is amazing and you guys obviously have a great deal of knowledge and experience to be able to modify the phone to such an extent. I'm attempting a somewhat similar...
Results 1 to 40 of 42
Page 1 of 2 1 2