I guess it does jingel around a bit, don't really know why lol
Type: Posts; User: rebel; Keyword(s):
I guess it does jingel around a bit, don't really know why lol
I guess it would be me, not getting the sequences right lol? :p
Thanks KevinO, took me long enough just to get this guy together. As far as flex there is a little bit in the servo mounts in the hips and ankle, but it is barely noticeable. I do not see any...
http://youtu.be/URamEYxAf6A First steps, not using hip twist servos or the battery side to side tray.
Construction of the battery tray and showing side to side movement for better balance and walking
48314831483248334834483548364837483848394840
I modified my first robots feet for now
48164817
Standing on own power but all servos not centered, BLAH.
Any one got some cool ideas for feet, can start preping a mold for CF if it is not to crazy??
And any info that might help with MW would be nice as well
4815Forgot I had to make feet, always forget something lol
481148124813
Almost there :p
Ya, not sure how the height will turn out, but it will be just a little heavier then the last one, and be able to carry a heavier load.
Would have the legs done, but I forgot how to count, lol....
Got half the legs together
4802480348044805
:p
479247934794
Updates
Finally got my House hold goods477847794780
Looks like good deals, but not for carbon fiber :(
Use the design from Wall-E, would not be overly complicated to make, or get to fold into its self
Asking for some help or constructive crits here. Looking to use the Fio v3 - ATmega32U4, but a little stand-of-ish, because I have mainly stuck with the SSC-32 and LYXN stuff. Building a laptop right...
Looks like a fun project :p
Even I, ya me :p, do not mess with anything below 400 oz/in of torque for robotics.
Pretty much everyone uses Xbees to control the robot, and WIFI for camera, directly to computer. From what everyone has been saying do not use blue tooth at all, I could be wrong though. My PS2...
My next robot, keep in mind it is a Biped, has already gone over $4K. One thing I will tell you, going cheap does not work for these robots
Can someone change this to project please, didn't see I messed that up
Yes my friend, maybe 2 more weeks before I get my house hold goods, so not much else for me to do till then :p
I only do have been Bipeds, Mainly :p
Looks and moves very nicely
That's cool, good job with that
And the back, same as last bot.
But one change that I hope makes a big difference, with balancing.
4469
This is the front, chest and hips.
Similar to my last bots design.
4468
Using Chapstick as a size reference
There will be 8 of these, 4 in each leg
4467
That thing is cool :P
That looks really cool
Yes, people in the US have no clue what a beer is LOL :tongue:
I do not believe I never saw this guy before, on here. Very good work. Now I want one lol :P
I just got to Germany. My father has the parts and will send them to me this week. Half the robot is in my house hole goods, they will get here beginning of next month. So I am guessing my first...
I put a thin layer of plastic over it all to protect the CF when it is cut
yes flanges bearings, makes it easy to assemble and disassemble the legs.
I am using some acetyl parts this time, the black piece is ABS.
Because of the moving parts, in the chest, I wanted...
44274428443044314432
Some pics of parts as they come in. 4417
Got my Raspberry PI, and just loaded Lucid Puppy on it. Sorry I have not been on more, after my getting to RG2012 late, and not being able to qual for Mech Warfare, I have had a bad attitude about...
Unfinished HS-7980TH servo mounts
40194020
Wiil look better after they are refinished. Need a little work done till they are perfect.
Sorta having that issue now. I used the PLD from Ingis, but i am having issues with how long to make the "levers" going betwen the legs. Is there a safe formula to figure out how long to make em?