Search:

Type: Posts; User: Croc; Keyword(s):

Search: Search took 0.01 seconds.

  1. Thread: W.A.S.P.

    by Croc
    Replies
    9
    Views
    9,667

    Contest Entry Re: W.A.S.P.

    Awesome, thanks for that mate.
    I guess the 8/15A UBEC I have already ordered will be a bit overkill, but im fine with that, I was actually worried it might not be enough. Can always order a 3A one...
  2. Thread: W.A.S.P.

    by Croc
    Replies
    9
    Views
    9,667

    Contest Entry Re: W.A.S.P.

    This robot looks amazing. Very helpful to me as im also working on a HXT900 based hexapod.
    Just wondering, how much does it weigh all up?
    Also, have you ever had any power problems with the 3A...
  3. Replies
    3
    Views
    7,868

    Question(s) Re: Just another hexapod servo controller thread

    Cool, thanks guys. SSC-32 it is.
    Ill post the hex when its finished, however im sure ill be asking for more help/advice before im done.

    I cant believe the shipping prices though, the $67 its...
  4. Replies
    3
    Views
    7,868

    Question(s) Just another hexapod servo controller thread

    Hi all

    I have decided to build a small, cheap, hobby servo hexapod, which if I can get working in time, I may use for a Uni project.
    Ive got the design and fabrication side of the project pretty...
Results 1 to 4 of 4