Search:

Type: Posts; User: HakBot; Keyword(s):

Search: Search took 0.00 seconds.

  1. Replies
    34
    Views
    26,587

    News/Announcement Re: Skynet Research wants YOU!

    http://www.firstshowing.net/2009/02/02/skynet-research-viral-marketing-for-terminator-salvation/
  2. Replies
    125
    Views
    643,540

    Project Re: A-pod, an ant inspired hexapod

    Zenta,

    Once again you have gone over the top! Keep up the good work. Cant wait to see what you do next.
  3. Replies
    14
    Views
    18,616

    Re: C++ Serial Communication

    Was this solved? Would the OP mind using C++ .NET? If so creating a serial port connection is cake. Its a standard item listed in the tool box such as a button is. You can manipulate the variables in...
  4. Replies
    30
    Views
    18,967

    Re: Discussion of Servors

    Firestorm,

    This is just my opinion but Im guessing you dont want to spend thousands on whatever it is you are doing so if this is the case I would recommend the 645MG from Hitec. I think you can...
  5. Replies
    5
    Views
    6,417

    Re: cheap multimeter

    I also purchased the Harbor Freight meter and I can say it does work but you will probably spend more time fiddling with the leads trying to get a connection than you will actually using the meter....
  6. Replies
    22
    Views
    27,668

    Project Re: Custom joystick to control robot arm

    No idea, must be something up with the forum because the link is still in the post when i click edit. It is still posted on my youtube page and my site: YouTube - Controlling a robot arm naturally
  7. Replies
    22
    Views
    27,668

    Project Re: Custom joystick to control robot arm

    4mem8,

    Can you post a picture of your first place prize? I have searched the site and followed all links but I cant locate any info on the arm.

    Edit: Ah its a crust crawler arm. Very cool I...
  8. Replies
    22
    Views
    27,668

    Project Re: Custom joystick to control robot arm

    I need some modifications done to my site before I am able to post this write up so I have created a PDF for now. If there is anything you want to know about that I didn't explain or need to explain...
  9. Replies
    22
    Views
    27,668

    Project Re: Custom joystick to control robot arm

    Thanks for the kind words everyone. I will definitely be posting more in this forum!
  10. Replies
    22
    Views
    27,668

    Project Custom joystick to control robot arm

    Hello,

    I just wanted to share my latest project with the forum. I have created a custom input device to control movements on a robotic arm. I believe this kind of system is most commonly called a...
Results 1 to 10 of 10