Search:

Type: Posts; User: Pocar19; Keyword(s):

Search: Search took 0.00 seconds.

  1. Replies
    9
    Views
    5,264

    Re: MX 28 Servo Questions

    Thanks for your feedback!
    In my case I put 500uF capacitors into 12V line and for the time being I haven't got anymore communication issue... I'll keep my fingers crossed!
  2. Replies
    9
    Views
    5,264

    Re: MX 28 Servo Questions

    I did have experience few communication issue with MX-series. For my project I don't use heavy load and I powered my daisy chain of servos at 12V using a power supply.
    Do you know if there is a way...
  3. Replies
    9
    Views
    5,264

    Re: MX 28 Servo Questions

    Indeed you can read the absolute position of the encoder ( I tested only MX28) while the servo is spinning in wheel mode.
  4. Replies
    0
    Views
    5,072

    Question(s) FTDI FT232R - impossible to open port

    Hello,
    I am using FTDI FT232R to comunicate via RS485 with Dynamixel Robotis servo (in particular EX106).
    My program is written in C++ using visual C++ 2010 and I am using the last driver from FTDI...
  5. Replies
    5
    Views
    9,616

    Question(s) Dynamixel SDK (Robotis)

    Hello,
    I have a question... does anyone know if it is possible to control in parallel two Dynamixel motors, one connected via RS485 and one connected via TTL ?
    I will make my question clearer......
Results 1 to 5 of 5