Wow didn't see this until just now when looking around for photos for a presentation. A very late thank you. It's alright; we got other photos.
Type: Posts; User: byi; Keyword(s):
Wow didn't see this until just now when looking around for photos for a presentation. A very late thank you. It's alright; we got other photos.
So, how did these end up going? Are either of these active? Also, could you post a new discord link if that is still running?
The site being unreachable the other day makes this seem slightly more relevant.
July sounds significantly more plausible for us. Will keep you posted.
Thanks RTeam for putting in the time to make this happen.
I would not be opposed to switching. Bit sad to see the end of something I've been on for a decade, especially since so much is documented here, but yea this is not the best option anymore.
...
I would love to be able to say that the Princeton group is in, but honestly I don't think we'll be ready in time. Maybe. I'll see what the others think.
With all of us working from home due to...
Put me down as interested in attending but unable to assist from all the way on the east coast.
Best of luck!
In case that one does eventually stop being available, another viable gearbox is usually sold as the Well R2 VZ61 Scorpion gearbox, or some permutation of those names. It's a bit heavier but less...
There have been a couple viable three servo entries similar to the above. Mine for Shep Robo 2015 specifically did it for cost reasons. We managed with two AX and one MX, and here is a project that...
Dang. Well, keep us posted! Thanks for plugging along with this despite setbacks.
Assuming the Princeton groups stays on task this summer, we'll be there with one mech.
That's great to hear! That will certainly put some pressure on the team here to stay on schedule this summer. :)
Looking forward to hearing how it went :)
That all aluminum gun assembly is a thing of beauty.
Props on a nice build in two weeks.
At least it sounds really cool?
Seriously though, very cool to see a different approach working well.
Wow! That is on a new level. Nicely done.
I would very much like this as well. No idea how this is done or who does it though.
Holy cow that thing is speedy!
I will have to take my next gait iteration up a notch or start putting serious thought into that jump jet idea if I plan to keep up with the mobility improvements...
True. I've seen some transmitters that look a bit like console game controllers. The buttons on those might make better triggers, but I do not know if any are sufficiently configurable to make that...
Good to know. I thought there might be an unofficial consensus not to use them, given that they don't seem to be used and that I specifically remember the interference headaches in the 2.4ghz band we...
Are RC controllers allowed? I noticed no one seems to use them, so I assumed that was to avoid interfering with the signals from smaller digital transmitters (as per robogames 2011 when all the...
If I understand correctly, most transmitters take a composite video signal, so a normal VGA -> RCA adapter would work. I've also seen some transmitters that take HDMI input. I've been looking into it...
Thanks for passing all of this along, guys. It's a huge help. :)
Wow. Thanks for all the details. Those are good things to know ahead of time rather than finding out along the way.
Awesome. Thanks!
I really also should look into springs. It makes a lot of sense.
If I understand correctly, the AX-12 mosfets are awkwardly located under a folded over capacitor, and the clearance space inside the servo is pretty minimal. I guess if you have R-Team style heat...
If I recall correctly, Immortal had this design feature fairly well developed. I look forward to seeing want innovations can be made in that area.
Glad to hear I'm not crazy, or at least no crazier than my opponents. :)
Did you mention it in the forums before? I was scrolling around earlier since I could have sworn someone proposed this...
Yea... I'm pretty bummed, but one guy had to drop out this spring, exams are killing me right now, and then we all have issues travelling. Just wasn't going to happen this time. We'll be ready for...
The group in Princeton recently had a couple people join, and as usual they had a bunch of "new" ideas to solve the various design constraints of building a mech before getting a sense of why such...
It looks like we can't make it. Rather disappointing to all of us, but we plan to use the extra time before the next event to implement new features. Best of luck!
Sorry for the delay. We're having some nontechnical issues and likely cannot make it. Hoping to figure that out shortly.
The Princeton group will probably be bringing a mech. It's a new group, so we'll have to see if we can finish in time, but things are looking good. Looking forward to it!
Looking at it now. Very intriguing... Thanks for the advice!
Dang. I was just starting to prep for this. Well, I'll try for ShepRobo (if that is running) and whenever the next Tucson event is on.
Separately, with Columbia and Harvard having currently active...
I was just about to start working on my next design with Robogames in mind (nevermind that, I guess), so I also hope to have something ready in the spring. If not, I'll keep next December in mind.
Currently planning a new mech, also on limited time and money, with the additional constraint of limited tools. Alas, my current university has much fewer tools available to students than my previous...
I think the video for Joshua is the first attempt. That was before I figured out the bug in my code that led to my back legs shutting down. Got it on the second go.
edit: third go apparently XP
Thank you. Much of that credit should go to various members of R-Team for advice, supplies, and supernatural soldering abilities.
I'll pass that along to the team while continuing to badger them to...
Agreed. The Columbia team had a great time and are already planning for next year.
Thank you R-Team for making this all happen and for the advice and assistance throughout the weekend.