Sorry for the lazy post, I promise I squinted long and hard for a good 4 seconds at the forum before asking:
Has there been any general consensus or open sourced design for airsoft weapons? Or are...
Type: Posts; User: DresnerRobotics; Keyword(s):
Sorry for the lazy post, I promise I squinted long and hard for a good 4 seconds at the forum before asking:
Has there been any general consensus or open sourced design for airsoft weapons? Or are...
Hey all,
Doing some late spring cleaning and selling off some of my personal stock of Dynamixels. Prices are cheap and firm, have a couple of each, all very lightly used.
MX-106T: $230...
Please contact us directly for tech support, trsupport (at) trossenrobotics.com
Renee and I will both be there actually! Would love to meet up with anyone also attending.
We're going to be officially announcing our TurtleBot 2i platform, which has been developed in...
Just to give those in the thread a heads up, we actually have the PhantomX MK4 release slated for mid 2017, which will include a lot of software updates to get things caught up to the later arduino...
Not competing, but I'll see you guys there. Cannot wait to see how it's come along!
From what I've seen of the Arbotix-M's that have come back, it's almost always a corrupt bootloader that causes this failure. We're not entirely sure why it goes bad, but reflashing a bootloader...
Make sure that you have actions on the pages that those buttons are linking to- the node_server demo app was put together by some folks at Intel for a show, so they had a bunch of custom animations...
MX-28T have slightly less backlash than the MX-64/106, but not by much. 64 & 106 appear to have about the same level.
Zenta- one thing you can experiment with is tighter PID settings on the MX-64,...
Yikes, this is the first incident where I've seen our cables with wires crossed. Good to hear nothing was damaged, you have my apologies about that.
Looks like I've gotta go bark at our cable...
RPI3 Support added with latest image, all dependencies included. https://sourceforge.net/projects/hros1raspberrypiimage/files/Raspberry%20Pi/
Pairing works with the integrated bluetooth but...
We have a colleague who has two humanoids that they no longer need after having completed their projects with them.
There are two HR-OS1's (one assembled, one unassembled) and one fully assembled,...
I'll follow up on your ticket directly to address this officially, but if you have a defective product we'll gladly replace them free-of-charge. If for some reason you were still seeing issues with...
Generally we answer tech support through our ticket system, the e-mail address is on our contact page.
How are you reading the pulses? Generally with encoders you need to attach them to interrupts...
I've actually done this before on some of the custom "Jimmy" robots we built over the course of the 21st Century Robot project, so I can tell you it does indeed work, it's just a bit cumbersome due...
Along with the new OS1 armor stuff I've been working on, I'm going to be doing a full set of armor for the MK3.
Lookin' good! Larger battery should treat you well eh?
Thanks! I just threw this to the top of my todo list for the v1.2 arbotix-pro updates. I honestly don't remember where I pulled that header part from, the Arbotix-Pro was thrown together a bit faster...
1) I'll need to double check the documentation/pictures we have- I didn't put them up. But nice find, I'll look into it!
2 & 3) I have no issue with more info on reprogramming them being added to...
Re: Original question, to be honest documenting the process isn't a huge priority for me right now.
It's sort of one of those 'If you have the skillset/desire to reprogram the firmware, you can...
RS-485 =! TTL
The AX and MX-T series servos all use 5v TTL @ 1mpbs.
Be careful with RS-485, as it's rated for up to 12v. Your adapter may not go that high, but if it does it can surely fry the...
You rock man. This code base is phenomenal.
Comes complete with horn, idler, cable, & hinge frame. Lightly used for testing, intended for a project I no longer have time for.
6x MX-64T - $150 each
2x RX-64 - $100 each
Thank you very much for the report back, glad to hear Renee got you up and running.
Yeah, something changed with recent updates to node.js (I believe) that broke the current implementation of node server. Working on a fix.
Anyone is more than welcome to continue carrying the torch, there's no real info needed from me. Contact Dave at Robogames, he requires a minimum of like 3-4 people to sign up for it, and then...
New walking gait has been pushed into the master branch, please note that it now has default compliance margins set (which will not work for the older, faster cycle gait). Please test this out and...
I've been working on getting updates rolled out for both the OS1 and OS5 3D models (both the endoskeleton as well as armor models), there will be downloads for both STL and STP format for the armor...
Let's not jump to wild conclusions here. Please.
21st Century Robots was an effort that enabled us to launch the project and have me focus on bringing the OS1 & OS5 to market for an entire year....
Are you using the image that ships with the robot? Or a different one? This sounds like you might be using the stock image.
Get out of my head Tician. Hah.
Basically this, we have a couple other projects going at once and are gearing up for a big release for the OS1 stuff as we move out of beta phase. We also didn't...
Unfortunately we don't have any control over the license of the HR-OS1 Framework. I asked ROBOTIS what the Darwin-OP framework was released under, they came back and said GPL was okay... then later...
1) I believe the solutions I linked you wrap the entire Darwin-OP framework. If you're looking for more information on how the library is initialized and a basic teleoperation demo, check the...
As others said, that package is not compatible with the Arbotix-Pro. It's outdated and written for the Arbotix-M specifically. We do have a project in the works that will create a specialized...
I am all for you and any of our users providing feedback, criticisms, and any other commentary on our products.
I take issue with the attitude and tone in which these are presented. There's zero...
You seem to be pretty frustrated, which might be alleviated if you slowed down and had a better understanding of the project and code that is out there. This is indeed a robotic development platform,...
Glad to hear it's working for you. In the future, please submit bug reports via Github Issues section on the main repo along with a description/dump of the failure error log. Makes it much easier to...
Try a fresh pull, and try again. Discrepancy between updates I was making last week on our test branch.
https://software.intel.com/en-us/realsense/devkit
Specifications
- Longer range** (up to 3-4 meters indoors, longer range outdoors)
- Depth/IR: 640x480 resolution at 60fps
- RGB: 1080p at...
This is mostly due to the nature of the vision included in the Darwin package. It doesn't really do a whole lot by itself, blob tracking is a neat party trick but isn't useful without...
The representation on the forums is not accurate to the number of robots in the wild. 98% of our customers never touch these forums. :) I know of about 2 dozen that are actively being used between 2...