Search:

Type: Posts; User: blastdog; Keyword(s):

Search: Search took 0.02 seconds.

  1. Replies
    0
    Views
    2,000

    Question(s) Motion Pages Loop issue

    Im having a problem with my robots program. I want to be able to press the up button on the remote control and make the robot walk forward (its a quad). I have the initial walk forward motion split...
  2. Replies
    4
    Views
    4,626

    Project Re: Crawler/Rover/Humanoid

    Thanks a bunch :) and as far as the feet thing go I found that the more points of contact with the ground there are, the better stability it has :) and I figured out how to program it all and make...
  3. Replies
    4
    Views
    4,626

    Project Crawler/Rover/Humanoid

    Ive been working on my robot to be able to crawl and drive with a four wheel omni wheel drive system and have an upper body humanoid style that is completely built with the exception of a few minor...
  4. Replies
    2
    Views
    3,089

    Question(s) Re: new ax 12+ actuators

    Thanks so much!! :)
  5. Replies
    2
    Views
    3,089

    Question(s) new ax 12+ actuators

    My AX-12+ servos will not show up in my roboplus manager. Right now i have seven of these servos set up in a daisy chain and roboplus only recognizes the last in the chain, the last is the only one...
  6. Replies
    3
    Views
    6,977

    Question(s) Re: Battery or charger problem

    i unplug the battery from the cm-510 when i charge it but it doesnt seem to charge anyways so ill check the connection. the weird part is i didnt have the battery on or even near my robot for like a...
  7. Replies
    3
    Views
    6,977

    Question(s) Battery or charger problem

    I am having a problem with either the battery or charger that came with the bioloid premium kit and I either can't charge it or it won't hold a charge. The lipo smart charger flashes both red and...
  8. Replies
    1
    Views
    2,765

    Question(s) Robot plus program

    I have written a forward motion file and a stationary file and I would like to have so that when I press the up button it runs the forward program and when I'm not it runs the stationary program, but...
  9. Thread: Quad balance

    by blastdog
    Replies
    9
    Views
    5,544

    Question(s) Re: Quad balance

    Will do :) I have a video of it walking that I'll post when I get around to it all I need to do is write the actual program and adjust some timing things :)
  10. Thread: Quad balance

    by blastdog
    Replies
    9
    Views
    5,544

    Question(s) Re: Quad balance

    Thank you sooooooo much :happy: I've fixed the wheels and made them a lot thicker and now it balances great :happy:
  11. Thread: Quad balance

    by blastdog
    Replies
    9
    Views
    5,544

    Question(s) Re: Quad balance

    Thanks for the advice and it will have treads on the wheels too
  12. Thread: Quad balance

    by blastdog
    Replies
    9
    Views
    5,544

    Question(s) Re: Quad balance

    here are some pictures any suggestions?
  13. Thread: Quad balance

    by blastdog
    Replies
    9
    Views
    5,544

    Question(s) Quad balance

    I have recently built a quad and I've figured out how to make it walk but it becomes unbalanced when it lifts up one of the legs and I was wondering how to fix that
  14. Replies
    7
    Views
    9,424

    Re: Want to build a backhoe or a crane ARM

    here's a pic of one i made (http://forums.trossenrobotics.com/showthread.php?t=4902&highlight=quad) it took five Dynamixel AX-12A's and it worked great adn it was just attached with a few of the...
  15. Thread: My Quad

    by blastdog
    Replies
    6
    Views
    5,162

    Just For Fun Re: My Quad

    Haha you caught me but hey the mechs on that game look awesome :) and if I ever make a cover frame it will definitely be from armored core ;)
  16. Thread: My Quad

    by blastdog
    Replies
    6
    Views
    5,162

    Just For Fun Re: My Quad

    Haha it's just too awesome not to ;) I saw yours and it's looking good so far :) if I get more motors I plan to put a body with 2 arms with claws and a turret on the chest, but i need quite a few...
  17. Thread: My Quad

    by blastdog
    Replies
    6
    Views
    5,162

    Just For Fun Re: My Quad

    Currently took the claw off to upgrade the legs by extending them and adding tank treads. So far ive made the frame for the treads with plastic resin and all thats left is to make the treads. Pics...
  18. Thread: My Quad

    by blastdog
    Replies
    6
    Views
    5,162

    Just For Fun My Quad

    Built this quad for fun using the parts that come with the bioloid premium. All thats left is to pragram it now. Im using the Roboplus software that was included and im just starting out so if...
  19. Replies
    4
    Views
    3,298

    Re: rc-100 with zigbee 110

    It is and I got my ir receiver to work somehow but the zigbee still doesn't and at this point I don't want to mess with what works so for now I've just let it be :)
  20. Replies
    4
    Views
    3,298

    Re: rc-100 with zigbee 110

    i have also tried with the ir reciever and the robot still fails to recognize any commands from the controller
  21. Replies
    4
    Views
    3,298

    rc-100 with zigbee 110

    for some reason my rc-100 controller wont work with my zigbee 110. ive checked the ID's and according to other posts they are correct and ive seen in places that the light is supposed to turn green...
Results 1 to 21 of 21