Search:

Type: Posts; User: zhanginou; Keyword(s):

Search: Search took 0.00 seconds.

  1. Question(s) Re: Dynamixel AX-12A won't actuate if the chain is longer than 6

    Hi guys, thanks for your replies!

    My hardware is setup as follows:

    11.1V goes in:
    - 8 dynamixels
    - a voltage regulator that turns the 11.1V into 5V

    The 5V from the voltage regulator output...
  2. Question(s) Re: Dynamixel AX-12A won't actuate if the chain is longer than 6

    Hey tician, thanks for replying.

    Is there any way apart from reducing the length of the cables, to prevent the voltage drop?
  3. Question(s) Re: Dynamixel AX-12A won't actuate if the chain is longer than 6

    Alright, I just ordered it, will post the results once it arrives.

    Aside from that, would you happen to know why some servos' ID reset when too many are daisy-chained together?

    EDIT:
    Also, do...
  4. Question(s) Re: Dynamixel AX-12A won't actuate if the chain is longer than 6

    Thanks for your reply.

    Do you mean this?: http://www.trossenrobotics.com/6-port-ax-mx-power-hub
  5. Replies
    1,144
    Views
    1,164,465

    Sticky: Re: Introduce yourself!

    Hi,

    I'm Victor, currently pursuing graduate studies in mechatronics. I've been introduced to Trossen Robotics this September through its servos Dynamixel AX-12a, for a quadruped robot project I am...
  6. Question(s) Dynamixel AX-12A won't actuate if the chain is longer than 6

    Hi,

    I am building a quadruped robot using 2 Dynamixel AX-12A per limb, so 8 in total, all daisy-chained on the same Serial line of my Teensy 3.6.

    I am using the library developed of Savage...
Results 1 to 6 of 6