Search:

Type: Posts; User: OOrmOnIzArGoR; Keyword(s):

Search: Search took 0.00 seconds.

  1. Replies
    3
    Views
    8,617

    Question(s) Re: Building a robot

    I find www.societyofrobots.com provides good basics on building and programming robots.
  2. Re: Private Message Replys to Appearing on Message History

    Thanks
  3. Private Message Replys to Appearing on Message History

    Hi, I've replied to private messages and my replies are not showing up on my messages folder of my account here on trossenrobotics. How do I make them show up?
  4. Good place to find used Dynamixel servos?

    Do anyone know a good place to find sellers of used Dynamixel MX-64t and MX-28t servos? I am in urgent need of these servos for school project/assignment. I think there has to be some place in the...
  5. Re: Wanted: Dynamixel MX-64T, MX-28T, USB2Dynamixel

    I had not considered servo backlash. I am not familiar with spring loaded joints. How are they constructed? I'm envisioning a single spring with one end of the spring attached to the upper arm and...
  6. Project Robot Arm That Writes. MX-64t & MX-28t servos wanted

    Hi all,

    Do anyone have Dynamixel MX-64T servo, MX-28T servos, USB2Dynamixel adapter, 3-pin cables or servo brackets they wish to sell. I'm doing a school project/assignment in which I will build...
  7. Wanted: Dynamixel MX-64T, MX-28T, USB2Dynamixel

    Hi all,

    I'm looking to buy one Dynamixel MX-64T servo, two MX-28T servos, one USB2Dynamixel adapter, 3-pin cables and servo brackets for MX-64 & MX-28 for a school project in which I will be...
  8. Re: How do I control Dynamixel servos using Arduino from python code?

    Are you saying there would be a delay between USB and the pin output? I would be ok with that as long as bit rate remained the same. So how do I set output pin to mirror usb input? And I'm using...
  9. How do I set Dynamixel servo ID using an Arduino?

    How do I set Dynamixel servo ID using an Arduino?
  10. How do I control Dynamixel servos using Arduino from python code?

    I want to use Arduino as an interface between computer and Dynamixel AX-12A servos. Servo instructions will be written in python code. How do I setup the Arduino to take instructions from USB and...
Results 1 to 10 of 10