Search:

Type: Posts; User: accelleon; Keyword(s):

Search: Search took 0.00 seconds.

  1. Replies
    8
    Views
    9,210

    Re: Suggestion on this diagram

    Not as of yet. I'm working on the sketches in my free time. As for the features: it can be switched between two modes autonomous and remote controlled. Both modes will feed a live signal to my...
  2. Replies
    8
    Views
    9,210

    Re: Suggestion on this diagram

    I felt the Sabertooth 2x5 didn't need to be added to the diagram(I will use it in the project as it is my only option, thanks again for the help with that). I was only adding the main components, but...
  3. Replies
    8
    Views
    9,210

    Suggestion on this diagram

    How does this diagram of my electronic connections look:
    http://accelleon.ucoz.com/electronics_diagram.PNG

    I forgot to mention the lines are wired connections and the arrow in between WA and PC...
  4. Replies
    6
    Views
    4,598

    Question(s) Re: DC motor controller question

    Thanks alot for your help.
  5. Replies
    6
    Views
    4,598

    Question(s) Re: DC motor controller question

    Thanks now all I need to know is where will the wires be connected to on the Sabertooth (the gnd,5v,S1 or S2 terminals). I'm assuming the 3 wires would connect to gnd,5v and S1 I just don't know...
  6. Replies
    6
    Views
    4,598

    Question(s) DC motor controller question

    Ok, so I'm planning out a PhidgetSBC based rover, I have a question about the Phidget servo controller connecting to the Sabertooth 2x5 motor driver. The Phidget servo controller has a PWM connector...
  7. Replies
    11
    Views
    16,362

    Project Re: New Post For Fresh Start On Robot Butler

    They probably decided to be lazy.

    Well anyway it depends on the amount of motors your going to need and what type they are. If your using 4 DC motors for the drive then you'll be fine. But unless...
  8. Replies
    11
    Views
    16,362

    Project Re: New Post For Fresh Start On Robot Butler

    Quote from Robot Shop User Guide:

    "No, at this time it is not possible to stack the shield..."

    I'm guessing that you would need to do some hacking until they come out with a new version. I know...
  9. Replies
    11
    Views
    16,362

    Project Re: New Post For Fresh Start On Robot Butler

    From what I read the Arduino accessories are stacked off of the main controller.

    The Shields don't have any top connectors so nothing can go above those they have to be at the top of the stack....
Results 1 to 9 of 9