LloydF,
We will post what is happening in this forum and also at https://forum.mechwarfare.org/ that jwatte mentioned above. I'm in a Robotics club in Tucson where it will also be talked about....
Type: Posts; User: giantflaw; Keyword(s):
LloydF,
We will post what is happening in this forum and also at https://forum.mechwarfare.org/ that jwatte mentioned above. I'm in a Robotics club in Tucson where it will also be talked about....
That is the thought. Either the library or in Don's garage. Have to see what unfolds. We had an event at the Phoenix Fan Fusion last year but it canceled. The next Fan Fusion is in May. Not sure if...
Hi Indi, we are hoping to start having Mechwarfare battles again in the fall of 2021 starting with a MechBrawl in Tucson. When things start up again we will make more target plates that we could send...
With hopes that the world will be better in September, Fan Fusion has been rescheduled for September 25-27, 2020. We did back out of the late May date but they are now holding our Mechwarfare spot...
So, here is the update on Fan Fusion in Phoenix. RTeam Robotics club has been going back and forth with Fan Fusion to arrive at a reasonable cost for us to attend and hold Mechwarfare. For the space...
swapped out with revA, added names several times
Mechwarfare fight between Numa2 and Odin. Added robot names in several places.
https://youtu.be/XR2ZWxGej2U
Match between GS Marauder and Nomad.
https://youtu.be/TQsarEmRx6o
Match between Unlucky Cat and SuperMegaMicrobot2.
https://youtu.be/f8FjMttPz3s
Match between Nomad and Immortal.
https://youtu.be/atlHYbolZEs
Match 2 of 2 between Domino and Air Pod.
https://youtu.be/5EUMz518aUQ
Match between Sarge and Super Mega Microbot 2
https://youtu.be/ppWJva-1kAg
Match between Apophis and Nomad.
https://youtu.be/HAOaeiASlIY
Showdown at high noon for Malum and Odin.
https://youtu.be/YrxhkEnLY4w
1st match of 3 between 99 and Nomad. Pilot of mech 99 demonstrates good use of ricochet shots.
https://youtu.be/OtX5e6-7e6c
Match between Numa2 and 99.
https://youtu.be/PP70hbJBgfg
Match between 99 and Malum.
https://youtu.be/NktpiD36HYU
Yes, the competition is about true walking robots with guns that fight in an urban environment. One of the reasons for the competition is to promote development of more advanced walking machines. ...
1st match between Immortal and GS Marauder.
https://www.youtube.com/watch?v=NcY3HPdJG9Y
2nd match between Immortal and GS Marauder. Very close, exciting fight to the finish. More to come as I trickle it out. Got back up to speed on the editing tool.
...
Welcome jmpsmash!
My hopper is the oldest (2012) design in our club that doesn't jam. It is a gravity fed with a rotating wheel with 8mm holes to collect 10 bbs at a time and drop one at a time down a tube. When a...
Years back one of the RTEAM guys (Jeff, does the MW PA announcing) built over a dozen hopper prototypes and performed jam studies. This was back when we knew little about this. Over the months he...
Very cool!
I just re-read the 2018 rule set. The 2" was taken out as far as I can see. Section VII paragraph 5 at the Robogames 2018 site.
5. Target plates must be reasonably and FIRMLY mounted on a Mech,...
Yes, it's about 1 inch thick and meant to go in the back of the robot but it could go anywhere. You feed 3 small wire harnesses through the robot to connect the 3 regular plates to the one in the...
I was a little wrong in the previous description. This is the latest rev C plate from late 2017. Still current. Target plate is 3.5 x 3.5 inches with a Velcro strip down each vertical side. The...
They are right angle connectors pointed down. A little above horizontal center. From the backside right of vertical center. I'll get some measurements and a picture to post tonight. No one has...
Very nice
Numa V2 looks great. I'm excited in seeing it up close and in action.
The previous two replies are cut and pastes from somewhere else. Sorry if the discussion starts out as out of nowhere.
The small hole in the heatsink drawing is to allow the AX-12 servo LED to show through. The larger hole is for clearance of servo hardware. The AX-18A is very similar. Only difference is the LED...
I got an assortment of different springs and tried them. Picked the spring that in all 4 knees had the lower middle servo current draw. The spring took the static body weight off the middle servo. ...
The small hole in the heatsink drawing is to allow the AX-12 servo LED to show through. The larger hole is for clearance of servo hardware. The AX-18A is very similar. Only difference is the LED...
I got an assortment of different springs and tried them. Picked the spring that in all 4 knees had the lower middle servo current draw. The spring took the static body weight off the middle servo. ...
How much does Numa V2 currently weigh?
Gertlex,
We will probably do another Mech Brawl 2019 that you could shoot for. Also looking into another alternative to Robogames for 2019.
Yes, unexpected this is. We are planning on having a 2019 Mech Brawl in Tucson like we have had in a previous years. Everyone is invited to compete.
Eric,
Myself and all the guys in Tucson are looking forward to the next V2 step in the Numa Mechwarfare line. It will be great to have a 2 time winning veteran back in the mix. If there is...
This is a series of excerpts showing robot problems that happened at 2018 Robogames Mechwarfare. While these are common problems that occur there are many more that have happened in past Mechwarfare...