Search:

Type: Posts; User: kamondelious; Keyword(s):

Page 1 of 5 1 2 3 4

Search: Search took 0.01 seconds.

  1. Replies
    43
    Views
    223,019

    Re: Numa V2 - Quad Mech

    Looking good Gertlex!

    Can't wait to see some more video. :D
  2. Replies
    39
    Views
    98,659

    Project Re: Twitch - My 3 Servo Hexapod

    Awesome! Well done Sir.
  3. Replies
    84
    Views
    68,053

    Re: 3DOF Quadrupedal AX-12A Mech :: Fang

    Looking good!
  4. Replies
    36
    Views
    68,487

    Re: Mech Warfare 2015

    I could probably make it out for this too.
  5. Replies
    2
    Views
    4,923

    Re: wireless video quiestion

    This question is a bit vague as you don't give any detail of about your robot or computer.

    The easiest solution is a wireless IP camera, easily found online at sites like amazon or newegg. Shop...
  6. Question(s) Re: How does one set the torque of the servos for a moving robot

    Well, based on the quote from the user manual you provided :

    and my own experience, yes it would be possible, but it's very much dependant upon a few things (not listed in any particular order)....
  7. Question(s) Re: How does one set the torque of the servos for a moving robot

    That's the mass of the robot to 1/5th the stall torque of one servo.

    ;)
  8. Replies
    3
    Views
    11,252

    Project Re: Roboceratops - Robot Dinosaur

    Very cool! I'm looking forward to seeing more. Browse: ALDI Circular and Meijer Sale Ad on Weekly Circulars.
  9. Re: AX12 Red light blinking - no motor activity - how to request

    hahaha, quite possibly, but I couldn't find any of the other threads when I was looking for them earlier. I've played with recovering AX12 servos from errors a bunch in the past and chimed in on a...
  10. Re: AX12 Red light blinking - no motor activity - how to request

    Not in the slightest, it only allows you to use the servo again and why I recommend putting the robot into a safe position to cool down. I also mentioned that playing with the temperature limit...
  11. Re: AX12 Red light blinking - no motor activity - how to request

    I could be wrong, as I haven't played with this in a while, but I believe both are resettable/recoverable in software.
    You need to reset the Torque Enable and Alarm Shutdown registers in both cases....
  12. Replies
    227
    Views
    208,741

    Re: Meet Hi No Hikari

    hahaha Awesome DB!
  13. Replies
    227
    Views
    208,741

    Re: Meet Hi No Hikari

    Great job DB! That looks fantastic.
  14. Replies
    5
    Views
    15,168

    Re: 90 degree joint / miter gears

    How about a universal joint? I don't know what your options are like for something off the shelf, but I wager you could make something pretty decent.
  15. Replies
    55
    Views
    44,952

    Re: MX64 Biped

    You can use pypose, it is the default firmware loaded on the Arbotix.
  16. Replies
    20
    Views
    23,081

    Re: Mech Armor

    I tested out foam-core with my first mech and it didn't stand up to well being shot from 6' away with a gun that's not as powerful as the AEGs. An AEG shooting fully automatic would shred it pretty...
  17. Replies
    47
    Views
    47,094

    Re: Micro Crawler

    Very cool Jon!
  18. Replies
    15
    Views
    14,429

    Re: Xbee reliability

    I had an issue like this a couple years go. The fix ended up being changing the channel my wireless router was using. Might be worth checking which specific frequency your home wireless network is...
  19. Re: Dynamixel SDK linux: COMM_RXTIMEOUT error

    Here's what I did to get the basic functionality working. The howto docs on Xevel's site miss a few changes.


    $ diff -b robotis/src/dxl_hal.c robotis/xevel_src/dxl_hal.c 22c22
    < struct...
  20. Replies
    4
    Views
    7,634

    Re: Dual Axis joint using AX-12s?

    Why not reference any of the AX-12 kits? They all use the same sort of design using standard AX series frames.

    Take a close look at the ankles in the pictures here :...
  21. Replies
    20
    Views
    23,555

    Re: My adventures in 5.8GHz vdeo

    Hey Jwatte, have you seen the, relatively, new Raspberry Pi camera module? I picked up a couple of these to play with. Pretty impressive little camera and integrates great with the Pi. The camera...
  22. Replies
    5
    Views
    11,048

    Re: AX12A Baud Rate

    If you set the baud rate register value to 0, then your baud rate is 2000000.0 bps based on how they calculate it.
    Speed(BPS) = 2000000/(Data+1)...
  23. Replies
    5
    Views
    8,078

    Re: AX12A sync write

    Have a look at BioloidController::writePose() since it does a sync write. You may want to make use of the pose based code already there, or modify it to meet your needs.
  24. Replies
    5
    Views
    8,078

    Re: AX12A sync write

    Here's silly question. Which/whose library are you using?

    #include <ax12.h>
    #include <BioloidController.h>

    This leave a little too much guess work. Arbotix? Your own? From someone's blog? ...
  25. Replies
    65
    Views
    79,707

    Re: USB2AX v3.0a feedback

    Great! Thanks for the input. I will play with it as is for a bit to get a feel for it and then play with updating the firmware. I'll let you know how that goes. ;)
  26. Replies
    40
    Views
    30,286

    Re: Robust, affordable gun design

    jes1510's dual gun motor driver is still a great option.

    http://forums.trossenrobotics.com/showthread.php?3907-Dual-Gun-motor-driver
  27. Replies
    65
    Views
    79,707

    Re: USB2AX v3.0a feedback

    Yeah, that was my thinking too, but 32 * 6 = 192 bytes of data. Add on the 6 bytes for the rest of the return packet and we're at 198 bytes. The chip has 2.5kb. ...
  28. Replies
    65
    Views
    79,707

    Re: USB2AX v3.0a feedback

    Hey Xevel,

    Why does the SYNC_READ functionality have the 6 byte data length limitation?

    From the documentation :

    http://xevelabs.com/doku.php?id=product:usb2ax:advanced_instructions

    It's...
  29. Replies
    51
    Views
    221,023

    Project Re: Biayered-X

    Looking good DB!

    I really like the standing up sequence.

    Keep up the good work!
  30. Replies
    15
    Views
    22,173

    Re: airsoft drivers?

    I can't say I understand what this part is, but based on it's ratings, it's not likely to handle the current from your gun. Or not for very long.


    These are cool, but the Picoswitch won't go...
  31. Sticky: Re: MW 2013+ Ruleset Additions and Changes Discussion

    I just confirmed with Andrew that the classes are for the Battle Scenario game play modes. The regular league play is to stay the same with maybe a few tweaks to the rules.

    I like the shorter...
  32. Sticky: Re: MW 2013+ Ruleset Additions and Changes Discussion

    Conceptually I like this idea, but there would have to be a lot of teams involved, showing up ready, before it would be practical. Definitely worth revisiting as popularity grows.
  33. Sticky: Re: MW 2013+ Ruleset Additions and Changes Discussion

    Would a biped really have a 2 weapon requirement? I've gotten away from that because of weight and trying to balance the extra momentum that comes with it.



    My thinking on this has always...
  34. Replies
    41
    Views
    77,272

    Re: TwitchMX - The Mech of Many Feet

    Great job Gertlex!
  35. Replies
    41
    Views
    77,272

    Re: TwitchMX - The Mech of Many Feet

    Looking good Sir!

    Can't wait to see this bad boy walking.
  36. Replies
    65
    Views
    79,707

    Re: USB2AX v3.0a feedback

    Thanks tician!

    :D
  37. Replies
    65
    Views
    79,707

    Re: USB2AX v3.0a feedback

    Indeed. I wouldn't mind having a couple handy also.
  38. Re: Servo Torque required for Biped and Quadraped

    The Bioloid Comprehensive and Premium kits both feature quite functional bipeds and quads, so I'd say the AX-12 has enough torque. It's been proven at every Mechwarfare event (and clones) that...
  39. Thread: 00Ze

    by kamondelious
    Replies
    10
    Views
    12,560

    Re: 00Ze

    Looking like a good time so far.

    :D
  40. Replies
    7
    Views
    10,043

    Re: Trouble Running Pypose (Mac)

    Is there a /Users/benbrummel/Desktop/ARM 2013/arbotix-0015/pypose/tools/ directory? If so, what is in it?

    I have these :

    $ ls -1 tools/
    models
    NukeEditor.py
    NukeEditor.pyc
    PoseEditor.py...
Results 1 to 40 of 171
Page 1 of 5 1 2 3 4