Search:

Type: Posts; User: tician; Keyword(s):

Page 1 of 13 1 2 3 4

Search: Search took 0.03 seconds.

  1. Replies
    274
    Views
    93,681

    Project Re: More Mule then Rover?

    Just needs a new boot on the spark plug connector... and might be a bit under-powered for that alternator at full load. 1[hp] is 746[W], so even 100% conversion efficiency won't give you full 24V...
  2. Replies
    10
    Views
    1,642

    Re: Novel leg/chassis design

    For linkage based walking robots, see also: https://www.youtube.com/user/psyclopz http://www.nidona.com/marauder.html
  3. Replies
    10
    Views
    1,642

    Re: Novel leg/chassis design

    Which is the undecided factor that goes in the square tube cutout in the actuated end of the linkages. My first thought for that was solenoid, then linear actuator (threaded rod coupled to a small...
  4. Replies
    6
    Views
    1,145

    Re: Power for eight (8) Dynamixel XM-430-W350-R

    batteryspace.com still sells plenty of LiFePO4 cells, and assorted e-bike sites sell them as well.

    The 'accurate positioning on a plane' bit says indoor with human interaction not outdoor speed...
  5. Replies
    6
    Views
    1,145

    Re: Power for eight (8) Dynamixel XM-430-W350-R

    bleh. I've been encountering lots of people not reading for comprehension recently... one in particular at work last week.

    jwatte, they mentioned in the very first sentences: four independently...
  6. Question(s) Re: U2D2 Power Hub and LIPO Battery 11.1V 1800mAh LB-012

    The problem is that battery uses a Deans / T-connector and the board does not have that anywhere on it. So, you need something like this (https://www.trossenrobotics.com/battery-wiring-harness) or...
  7. Replies
    4
    Views
    2,247

    Re: The Raspberry pi 4 Model B

    In theory, the RPi4+4GB is more powerful than my netbook in its default configuration (2-core 1.0GHz/1.33GHz, 4GB, USB2, Fast Ethernet, 802.11n)...

    Probably will pick up one of the RPi4+4GB in the...
  8. Thread: Rip Van Winkle

    by tician
    Replies
    5
    Views
    1,394

    Re: Rip Van Winkle

    I almost posted before about this in one of the Malum IK threads, but that ODrive board brings the ick back to the surface...
    if you are not using BGA ICs with sensitive power requirements and/or ...
  9. Thread: Malum IK

    by tician
    Replies
    58
    Views
    10,576

    Re: Malum IK

    How has your experience with MacroFab been? Spent an hour or so assembling some PCBs* for small scale production (Seeedstudio PCBs and stencils plus low-temp solder paste), but hand producing these...
  10. Replies
    4
    Views
    1,635

    Question(s) Re: AVRDUDE ERROR - arbotix board

    It is possible - although not probable - that the FTDI dongle you are using is not plugged into the arbotix correctly, or it is unable to provide enough power to the arbotix. Are the jumpers set...
  11. Question(s) Re: AX12-A not communicating after failed firmware recovery

    Usually, the reason for an AX-12 failing to move when not under significant weight loading is some sort of mechanical interference like cables getting wrapped around frames or wedged into gaps...
  12. Replies
    38
    Views
    7,427

    Re: Malum Gun Sub-thread

    So what you're saying is I really should put in a bit of effort into making this ~2"-OD x ~6"-L fully self-contained airsoft cannon holding ~320 BBs in a single-file ratcheting magazine with breech...
  13. Replies
    38
    Views
    7,427

    Re: Malum Gun Sub-thread

    Stop thinking rigidly and things will stop breaking.
  14. Replies
    38
    Views
    7,427

    Re: Malum Gun Sub-thread

    That thing is the essence of a one-way bearing: shaft/wiper spins one direction and it removes the roller/pin/BB from contact with the housing completely decoupling motion of shaft and housing;...
  15. Replies
    38
    Views
    7,427

    Re: Malum Gun Sub-thread

    Congrats, you just reinvented the one-way roller bearing. ;-) Hope your motor can handle repeated, sustained stalling.
  16. Replies
    38
    Views
    7,427

    Re: Malum Gun Sub-thread

    Only equivalent if the hopper is also rotating relative to the fixed wiper. Otherwise, the fixed 'wiper' is just a blockage helping keep BBs away from the hole/sprocket.

    Perhaps something like...
  17. Replies
    38
    Views
    7,427

    Re: Malum Gun Sub-thread

    Most of the designs I've pondered involve single-file magazines to completely eliminate the need for sorting BBs during combat as that has been the greatest source of issues people have been having...
  18. Question(s) Re: Do I have to unplug the balance connector from the loader before use ? (LiPo)

    Definitely need to know more about the balance charger you are using to say for certain, but...

    Does the balance connector even need to be disconnected when not charging? Probably not.

    Most...
  19. Replies
    4
    Views
    1,174

    Re: MX-64 bricked after update

    So they are 'bricked' in the sense that they cannot be upgraded, but work fine otherwise? That sounds entirely like a bootloader software issue. I know some persistent parameters were moved around in...
  20. Thread: Ax12/18 pid

    by tician
    Replies
    9
    Views
    4,750

    Re: Ax12/18 pid

    Also this with AX-12/18 servos: https://www.youtube.com/watch?v=DVq8Vp798gg
    It is mostly the DARwIn-OP framework and gait engine, but with cheaper servos...
  21. Replies
    1,117
    Views
    601,954

    Sticky: Re: Introduce yourself!

    https://www.manualslib.com/products/White-Box-Pc-Bot-914-3875566.html and http://www.theoldrobots.com/OddsEnds2.html have many manuals, but no software.
  22. Replies
    19
    Views
    3,375

    Re: Dumb Idea: So like... what about jumpjets?

    ...nope. 8g NOX is not enough to lift a mech. Isp would be roughly 260~110[s] with 8:1 NOX:diesel mass ratio with chamber pressure dropping from ~900[psi] to ~30[psi] as the NOX is depleted from the...
  23. Replies
    19
    Views
    3,375

    Re: Dumb Idea: So like... what about jumpjets?

    oh, dear. Someone please save me. I'm giving serious thought to building a N2O+alcohol pressure-fed liquid rocket engine using 8g N2O chargers and a few mL of denatured alcohol, and throttled by a...
  24. Replies
    19
    Views
    3,375

    Re: Dumb Idea: So like... what about jumpjets?

    Dumber idea would be a true jump jet using a nitrous oxide cartridge in a throttled micro-scale monopropellant, hybrid, or liquid fuel rocket engine.
  25. Replies
    5
    Views
    1,469

    Re: Dynamixel MX-28 no longer turning

    Has the cable assembly to the first servo in the leg been damaged? If you plug the power/comm cable assembly into the spare connector on the other end of the leg, do any of the servos appear?
  26. Replies
    1
    Views
    1,329

    Re: Bioloid Premium Kit

    The comprehensive kit was discontinued many years ago and the Premium kit has gone through several revision/updates as well. There are no upgrade kits, but the individual parts are available from...
  27. Replies
    274
    Views
    93,681

    Project Re: More Mule then Rover?

    Yet airplanes still break apart more often than you would hope because stress fractures can be difficult to impossible to detect visually. They are detected/tracked during scheduled...
  28. Replies
    274
    Views
    93,681

    Project Re: More Mule then Rover?

    That's actually the rough process for determining tear-out limits for fasteners in holes, but it says nothing about the rest of the bracket surviving. Also, non-ferrous materials have finite...
  29. Replies
    4
    Views
    1,936

    Re: Puppet Master/ Slave setup

    How big is the puppet? Does it have to support its own weight at all times (free standing, bolted to a floor, hanging off wires, etc.)? Does it have to physically interact with other objects (lift a...
  30. Replies
    2
    Views
    1,348

    Re: Arbotix and RoboPlus

    The arbotix is not immediately compatible with any part of RoboPlus.

    The Xbee/FTDI UART of the arbotix does not talk directly to the dynamixel buss, so you have to program the arbotix to act as a...
  31. Replies
    9
    Views
    2,633

    Re: dynamixel issue demagnetize/magnetize?

    The vast majority of power supplies can regulate in only one direction (input to output) by limiting how much energy gets transferred from the input to the output. If anything pushes energy back onto...
  32. Replies
    9
    Views
    2,390

    Re: PhantomX + CM9.04 but no Xbee!

    The Phoenix code does not use NUKE or PyPose. Phoenix is a completely independent gait engine developed by several lynxmotion forum members for their hobby servo multi-leg robots and their...
  33. Replies
    81
    Views
    36,737

    Re: First steps for Super Mega Microbot

    Is the lack of rigidity a bad thing, given you have been making this thing jump about? Elastic elements are a very big deal when dealing with non-trivial masses/velocities and less than smooth motion...
  34. Replies
    81
    Views
    36,737

    Re: First steps for Super Mega Microbot

    http://www.etotheipiplusone.net/?p=4688

    Onyx is plenty strong enough for full-combat beetleweight robots, so will likely be good enough for MechWarfare as long as you use proper wall thicknesses...
  35. Replies
    274
    Views
    93,681

    Project Re: More Mule then Rover?

    Mechanical relay ratings are mostly about thermal limits of the contacts and wiring, and not about welding itself closed. Since a relay failing closed is most likely to happen during the sparking...
  36. Replies
    274
    Views
    93,681

    Project Re: More Mule then Rover?

    Two 60 Ohm coils in series would be 120 Ohm. 24V / 120 Ohm == 0.2A and ~4.8W of power (most of it as heat once the relay has been closed). 2.4W in a small plastic package might not be much of an...
  37. Replies
    274
    Views
    93,681

    Project Re: More Mule then Rover?

    How hot is hot? What is the maximum running current of the entire drive system?
  38. Replies
    26
    Views
    8,504

    Re: Starting a quad build - A couple questions

    Only occurred a few minutes after my last post that most of the toy guns I had throughout childhood never used a barrel for anything other than appearances, and most of these things are still damn...
  39. Replies
    26
    Views
    8,504

    Re: Starting a quad build - A couple questions

    With an impact based weapon, a long tight-tolerance barrel does little other than reduce energy. It is easiest to think of it in terms of kicking an air-filled ball. Kicking a ball down a tube won't...
  40. Replies
    26
    Views
    8,504

    Re: Starting a quad build - A couple questions

    Nope. Can never be anything installed directly inside a PC and even if it could be guaranteed we were using a full PC capable of accepting any cards, PCI-Express would still be a bigger pain in the...
Results 1 to 40 of 500
Page 1 of 13 1 2 3 4