Search:

Type: Posts; User: Trevor; Keyword(s):

Search: Search took 0.00 seconds.

  1. Replies
    4
    Views
    1,394

    Question(s) Re: AVRDUDE ERROR - arbotix board

    Just a thought, as I bricked one of my Artibox boards a few days ago, let me know if it is possibly a similar situation. I was finished loading a sketch onto it and had the servos running properly...
  2. Replies
    2
    Views
    998

    Question(s) Re: Using Bioloid Library With Servo Modes

    Thanks for the reply KurtEck

    The modes are set using the ax12 library easily enough, there are macros already built for it. I tried it again today, without the wheel mode servo in the mix, just...
  3. Replies
    2
    Views
    998

    Question(s) Using Bioloid Library With Servo Modes

    Good Morning

    I was hoping someone else has run into this issue, and possibly had some insight. I want to run three Mx-Servos, in each mode available. ie)

    Servo_1 in Wheel_Mode
    Servo_2 in...
  4. Replies
    1
    Views
    758

    Question(s) Dynamanager finds mx-28t but not mx-106T

    Hello I am new here, I just received my first three dynamixels, and an Arbotix-m board. I was successful naming the two mx-28t motors to id 2,3. Dynamanager will not see the Mx-106T however. ...
Results 1 to 4 of 4