Search:

Type: Posts; User: jodell; Keyword(s):

Search: Search took 0.00 seconds.

  1. Replies
    10
    Views
    11,421

    Re: What programming editor do you recommend?

    I do most all of my programming with vim. The neat thing about using it for hr-os1 or other small computer projects is that it's included with most all Linux distros by default. Just ssh to the...
  2. Replies
    2
    Views
    4,982

    Re: CAD library of servos and standard parts?

    I usually start with the HR-OS1 CAD model for any dynamixel based projects. It contains the model for the AX-12/18 servos as well as most of the smaller Interbotix brackets. Also, Robotis has CAD...
  3. Thread: Wall E

    by jodell
    Replies
    2
    Views
    27,915

    Project Re: Wall E

    I've been thinking about building a Wall-e also but I don't have the time for it yet. I found a Yahoo Wall-e builders group that gives you access to a lot of Wall-e specific info, files, and people...
  4. Replies
    23
    Views
    77,202

    Re: mAh or C. Which is more important?

    If I recall, 1C is the milliamps that the battery can put out in 1 hour. For example, if you had a 1000mAh battery then 1C is 1000mA or 1 amp. If you had a 2000mAh battery then the same 1C rating...
  5. Replies
    7
    Views
    7,254

    Re: Suggestions for setting up a Mac Book Pro...

    Parallels might have a way to create a shared folder between the guest and host OS. I've never used Parallels but I know that Fusion can do it.

    You can also just setup an NFS export on linux and...
  6. Replies
    7
    Views
    7,254

    Re: Suggestions for setting up a Mac Book Pro...

    I wouldn't bother with dual booting or boot camp. I use VMware Fusion but Parallels is probably about the same. It's really easy to run OSX and windows and linux all at the same time on different...
  7. Replies
    29
    Views
    31,985

    Re: 3D Printer Knowlege and advice for upgrading

    I have a Formlab resin based printer. In general, I would not recommend this type of printer for creating any final robot parts - at least not yet. While they have a new "tough" resin that I have not...
Results 1 to 7 of 7