Search:

Type: Posts; User: explojr; Keyword(s):

Search: Search took 0.00 seconds.

  1. Replies
    33
    Views
    11,471

    Question(s) Re: Hexapod SSC-32 connecting to Lynxterminal

    My first jumper, like Adrenlynn said had to be removed.
  2. Replies
    33
    Views
    11,471

    Question(s) Re: Hexapod SSC-32 connecting to Lynxterminal

    BUT!! I just plugged it back into my other laptop - with the dongle and It works - I got a SSC32-V2.03XE
  3. Replies
    33
    Views
    11,471

    Question(s) Re: Hexapod SSC-32 connecting to Lynxterminal

    Ok. Progress!! The green light went out. Now will not accept any "ver" input however the register button works! The H2 seq button works! Firmware Button Works!
  4. Replies
    33
    Views
    11,471

    Question(s) Re: Hexapod SSC-32 connecting to Lynxterminal

    question 1) "What are the specific jumper settings on your card - can you take a photo of them?"

    Ok I took pictures but the COM port pins are not labeled.

    question 2)"The green light comes...
  5. Replies
    33
    Views
    11,471

    Question(s) Re: Hexapod SSC-32 connecting to Lynxterminal

    Thanks Adrenalynn, Installing a serial port didn't seem like a good option, as I need this computer (a laptop) for work.. modifying it might be troublesome.

    So I found a IBM Thinkpad on ebay....
  6. Replies
    33
    Views
    11,471

    Question(s) Re: Hexapod SSC-32 connecting to Lynxterminal

    Thanks for all the help Adrenalynn, After trying all this again on another computer (running xp) I am now looking at ebay - and a computer with a native RS232 serial port.
  7. Replies
    33
    Views
    11,471

    Question(s) Re: Hexapod SSC-32 connecting to Lynxterminal

    Ah, very good! Ok I tried that. Its the same as if I connect it to the serial point connecter. I get #OP118OS5000 then I type "ver" (enter) no response (of course). So where is the problem? In the...
  8. Replies
    33
    Views
    11,471

    Question(s) Re: Hexapod SSC-32 connecting to Lynxterminal

    Ok so I uploaded some pictures.

    1) Tried jumpering pins 2 and 3 to dongle (picture 1) . No response. Lynxterm would not recieve any input from keyboard.

    2) With dongle and serial port...
  9. Replies
    33
    Views
    11,471

    Question(s) Re: Hexapod SSC-32 connecting to Lynxterminal

    Ok so I uploaded some pictures.

    1) Tried jumpering pins 2 and 3 to dongle (picture 1) . No response. Lynxterm would not recieve any input from keyboard.

    2) With dongle and serial port...
  10. Replies
    33
    Views
    11,471

    Question(s) Re: Hexapod SSC-32 connecting to Lynxterminal

    Ok interesting..
  11. Replies
    33
    Views
    11,471

    Question(s) Re: Hexapod SSC-32 connecting to Lynxterminal

    Yes, I have this dongle. This is the one Lynxterm recommends too. When I send the "ver" nothing happens, the light stays on. Is there another USB connecter that connects straight through?
  12. Replies
    33
    Views
    11,471

    Question(s) Re: Hexapod SSC-32 connecting to Lynxterminal

    Oh, Sorry I wasnt clear. Since I am using this UC232R-10 USB adapter I checked the computers control panel. The USB was installed on COM port 6. Also the Lynxterm is set to Com port 6. Is there some...
  13. Replies
    33
    Views
    11,471

    Question(s) Re: Hexapod SSC-32 connecting to Lynxterminal

    Oh, sorry I wasnt clear. Since I am using this USB adapter UC232R-10. I meant that I checked in the control panel of my computer to see where the USB adapter was installed. The computer reads the...
  14. Replies
    33
    Views
    11,471

    Question(s) Re: Hexapod SSC-32 connecting to Lynxterminal

    The ports match up. They are both set to port com 6.
  15. Replies
    33
    Views
    11,471

    Question(s) Re: Hexapod SSC-32 connecting to Lynxterminal

    Ok, I turned off the echo prolem. The SSC-32 board has a green light. Connected to my computer (used a UC232R-10 serial adapter cable recommended by Lynxterm site). I tried matching the baud rates at...
  16. Replies
    33
    Views
    11,471

    Question(s) Re: Hexapod SSC-32 connecting to Lynxterminal

    Thanks.. again. I will try those things
  17. Replies
    33
    Views
    11,471

    Question(s) Re: Hexapod SSC-32 connecting to Lynxterminal

    Thanks! Pehaps I am in more of a pickle than I thought. The "vveerr" command doesnt return a firmware version.
  18. Replies
    33
    Views
    11,471

    Question(s) Hexapod SSC-32 connecting to Lynxterminal

    Hello, This is my first time posting, so excuse me if I get it wrong. Trying to put together a phoenix hexapod kit. I have everything working properly up until trying to connect the SSC-32 board to...
Results 1 to 18 of 19