Search:

Type: Posts; User: r3n33; Keyword(s):

Page 1 of 9 1 2 3 4

Search: Search took 0.01 seconds.

  1. Re: Question: Using Arduino IDE 1.8.1 and Can't See My ArbotiX-M on the Board List

    Currently everyone is tasked with other things. What Kyle was testing for 1.6.x is the best documented solution from Trossen.

    I've been using Arduino 1.8.whatever and tician's board definition on...
  2. Replies
    45
    Views
    36,310

    Project Re: DIY FSR Feet for the HR-OS1

    It's been awhile since I've messed with the FSR feet as well. I was using a Trinket for communication on the DXL bus and had a diode between TX and RX. Pretty sure there was some software logic...
  3. Replies
    13
    Views
    10,808

    Project Re: Xl-320 Based Hexapod

    Love the look of this one.. Nice stuff!
  4. Replies
    11
    Views
    3,832

    Re: AX-12 led light constant on, error?

    What address did you use for Trossen support and what is your ticket number? I do not see a support request for your issue in the system.

    [email protected]
  5. Re: Question: Using Arduino IDE 1.8.1 and Can't See My ArbotiX-M on the Board List

    Whoa! Thank you! I updated to 0.0.2 and tested the ROS sketch on an ArbotiX-M in Arduino 1.8.2 with success.

    This is great.
  6. Replies
    2
    Views
    2,085

    Re: Robot Block Party!

    Party time! :D
  7. Replies
    2
    Views
    4,587

    Re: How useful it is to use ROS?

    Only days later do I find a new example of ROS on the HR-OS1.

    You can find more information about this video on the author's github and the youtube video description.
    ...
  8. Replies
    2
    Views
    4,587

    Re: How useful it is to use ROS?

    :sad: zero answers but I think that's because not many have done so. So far I've only used ROS on my OS1 in one instance and I was using it as a puppet to control another ROS robot over the network....
  9. Replies
    63
    Views
    36,616

    Project Re: WinRME ( Robot Motion Editor for Windows )

    Sorry I missed this. At the moment I don't recall. I haven't used the software for a while. If you are still interested let me know and I'll get it in my queue. The WinRME source would serve more...
  10. Replies
    20
    Views
    12,301

    Re: Falling-Up Robot Project

    Sweet project! I love how massively tall this robot stands. Might be pretty crazy to scale it wider and make something like wall dividers that you or two people could push around.
  11. Replies
    59
    Views
    38,216

    Project Re: MX-Phoenix hexapod and some more

    Wooo! I saw these on instagram when I woke up. Very nice job :D

    Afaik there isn't an available 3d printed foot switch for the PhantomX.. I'd love to try it out sometime ;)
  12. Project Re: Some questions and thoughts about new Hexa Project

    You might also consider trying the firmware you initially flashed to the Arbotix just to see if things start working. It does sound like it could be the power source or you possibly have a break or a...
  13. Replies
    8
    Views
    4,132

    Re: What have I been up to lately?

    Thx. Chip-E is a simple bot but the combination of the robotgeek servos and the smooth oscillations do bring it to life. At some point it would be fun to see an alternate shell made or even...
  14. Project Re: Some questions and thoughts about new Hexa Project

    afaik foot sensors are kinda experimental. There isn't any one implementation followed by a large number. You'll likely have to experiment with your own solution like on Zenta's latest quad. On a...
  15. Replies
    59
    Views
    38,216

    Project Re: MX-Phoenix hexapod and some more

    That terrain video :robotsurprised:

    Such nice work Kåre! It moves so smooth and really keeps a level body. Are you using any type of inertial sensing or does the body remain level with the foot...
  16. Replies
    8
    Views
    4,132

    Re: What have I been up to lately?

    Hah thanks jwatte but it isn't all free time. Sometimes it's work time too but I'll admit they can be hard to distinguish every now and again.
  17. Replies
    8
    Views
    4,132

    Re: What have I been up to lately?

    Thanks Kurt! Most certainly fun if nothing else :)



    That looks awesome! HD and 3D video while flying has got to be pretty amazing. What size frame do you need for that kind of payload and what...
  18. Replies
    8
    Views
    4,132

    What have I been up to lately?

    Such a big question to answer since there's been a lot going on and a while since I've taken some time to reflect.

    Some months ago there was talk about making it to the 2016 IRC in Korea and even...
  19. Thread: RPi Hexapod

    by r3n33
    Replies
    9
    Views
    5,885

    Project Re: RPi Hexapod

    Cool project!

    How did you like using Fusion 360? I know of a few people who've tried it out recently and made some neat things :)

    Your future plans look interesting, hope to see more for sure
  20. Replies
    16
    Views
    11,644

    Re: Support for Arduino 1.6.0?

    Lol 1.8.0

    If I wasn't so tired from updating arm manipulation packages all night I might have a look. It sure is some kind of challenge to keep up with all these interests isn't it?
  21. Replies
    14
    Views
    15,855

    Sticky: News/Announcement Re: ArbotiX 1.6 Files / Libraries

    Oh maybe this thread is a better one to say thanks Kurt.. Your work here is helpful to me :D
  22. Replies
    16
    Views
    11,644

    Re: Support for Arduino 1.6.0?

    Hey Kurt.. Thank you for this. I'm working with Arduino 1.6+ and the Arbotix-M and now I can flash the ROS sketch I need :)
  23. Replies
    3
    Views
    2,999

    Question(s) Re: CYRF6936 radio + arduino 2560

    There is a link on the page to download the CYRF6936 library and the source contains all the information you need to work with the class. The guy even provides an example sketch working with the lib...
  24. Replies
    3
    Views
    2,999

    Question(s) Re: CYRF6936 radio + arduino 2560

    Googled it and found a library for working with the 6936 here http://www.pagemac.com/projects/arduino_cyrf6936
  25. Replies
    1
    Views
    2,641

    Re: Adding RME actions to Vision Processing

    Sounds doable. Modify the head tracking program to include the action module and enable only the arm joints in that module. Then call the action you want while the head tracking program is running.
  26. Replies
    2
    Views
    1,747

    Re: Where to buy sprockets in Canada

    Can't you weld that sort of thing? That's usually what I see people doing on youtube.
  27. Replies
    59
    Views
    38,216

    Project Re: MX-Phoenix hexapod and some more

    Sure looks nice! The smoothed parts photo really nicely. Can't wait to see it moving around and towering over stuff ;)
  28. Replies
    2
    Views
    3,386

    Re: Which ROS release for dynamixel support?

    Quite a bit is well tested with Indigo. That's not to say you won't get along fine with Kinetic also but if you start seeking info about past projects you'll likely find a lot more in Indigo and...
  29. Replies
    17
    Views
    6,805

    Question(s) Re: Trossen motor encoder not working properly

    I took a look into your issue this morning and at first I found similar results. With the encoders running at 3.3V and a pullup on channel A and B I'd see missed pulses.

    6764 6765

    After...
  30. Replies
    17
    Views
    6,805

    Question(s) Re: Trossen motor encoder not working properly

    This is the raw signal I see from those encoders:

    6762
  31. Replies
    4
    Views
    3,166

    Question(s) Re: Wireless control upgrade!

    I'll second the use of the ESP8266. They are cheap and have a number of examples to build from. You can find them from various distributors and styles. Sparkfun for example has a board with built in...
  32. Replies
    59
    Views
    38,216

    Project Re: MX-Phoenix hexapod and some more

    Looks awesome so far!

    You can find that tibia model in a HR-OS5 repo ( https://github.com/Interbotix/HROS5-3D-Models/tree/master/Assembly_STEP ) ;)
    or...
  33. Thread: XL_Quad

    by r3n33
    Replies
    8
    Views
    7,335

    Re: XL_Quad

    Cute! I like it.. lots of parts hey?
  34. Replies
    3
    Views
    2,789

    Question(s) Re: Create service intel edison

    I needed something similar with an Edison project in the past. You can find my solution on github:

    https://github.com/r3n33/EddieBalance/tree/master/extras

    Can't guarantee Intel has changed...
  35. Replies
    2
    Views
    3,481

    Re: HR-OS1 just getting started

    Sounds like you have made forward progress on your own. Indeed a good number of questions have been answered in other threads and with everything open source you can dig in and find some solutions to...
  36. Re: How to install a functional ROS with KevinO's hexapod_ros on a Raspberry 3?

    I'm heading out of town so I won't be able to help much. If you don't understand how the URDF / xacro file are assembled I recommend following the tutorials.

    http://wiki.ros.org/urdf_tutorial
    ...
  37. Discussion Re: What would hou do if you could have 1ms loop on the whole robot?

    Sweet photo album! I'm diggin the SSSLidar :)
  38. Replies
    6
    Views
    4,659

    Question(s) Re: Purchase Darwin-OP parts?

    I believe the Arbotix-Pro is on hold until an updated version is released. Andrew is working on some improvements to the design.
  39. Replies
    12
    Views
    11,424

    Project Re: Pablo, Land Art artist

    Nice work! Pablo is coming along nicely :)
  40. Replies
    12
    Views
    4,723

    Re: Cheap Toaster oven or Skillet?

    While not completely satisfied with the performance of my cheap oven it does get the job done for this sort of thing.. It's been modified a with a Zallus reflow controller but they don't seem to be...
Results 1 to 40 of 344
Page 1 of 9 1 2 3 4