Search:

Type: Posts; User: gmui; Keyword(s):

Search: Search took 0.00 seconds.

  1. Replies
    2
    Views
    2,772

    Question(s) Re: AX12A power consumption

    Thanks - gotta get me one of those...
  2. Replies
    2
    Views
    2,772

    Question(s) AX12A power consumption

    Does anyone know or know how to determine the power draw for AX12A servos that aren't being driven? I.e. set with torqueEnabled = false. We're powering the Master arm with 4 AX12As and trying to...
  3. Replies
    13
    Views
    10,149

    Question(s) Re: Attaching hobby servos stops AX-12A from working

    Thanks for all the help in looking into this. I think the problem I faced just running the attach code and failed servo calls were due to a bad board. Using the same code and wiring on another (3rd...
  4. Replies
    3
    Views
    3,198

    Question(s) Arbotix-M ISP pins

    I want to try and recover an Arbotix-M that seemed to go bad (can't upload via FTDI). I want to try restoring the bootloader with an ISP but the one I have has 10 pins instead of 6. I found this...
  5. Replies
    13
    Views
    10,149

    Question(s) Re: Attaching hobby servos stops AX-12A from working

    It seems like it's my Arbotix-M. As I said it worked on another board when I only had the AX12As and servos installed. I thought it may have been all the wiring on the first board that was causing...
  6. Replies
    13
    Views
    10,149

    Question(s) Re: Attaching hobby servos stops AX-12A from working

    Do you think there might be a capacity problem of having 7 AX12As driven in a slave arm, 9 pushbuttons, 1 toggle, 1 potentiometer and 4 AX12As as a master arm be too much for the Arbotix-M?
  7. Replies
    13
    Views
    10,149

    Question(s) Re: Attaching hobby servos stops AX-12A from working

    So it doesn't appear to be software related. I used another Arbotix-M and just plugged in the dynamixel serial cable and the servo (along with the 5V jumper) and it can read all the AX12A servos...
  8. Replies
    13
    Views
    10,149

    Question(s) Re: Attaching hobby servos stops AX-12A from working

    Thanks for your reply and help Kurt.

    Yes - Arbotix-M and Arduino 1.6.10

    It works (i.e. AX12A servos can be called without error when the servo is plugged in but the servo attach function is not...
  9. Replies
    13
    Views
    10,149

    Question(s) Attaching hobby servos stops AX-12A from working

    I'm trying to attach a micro servo to my PhantomX robot arm and am having issues attaching the hobby servos. Prior to attaching the servos to a pin (12-15), dynamixel calls work ok (e.g....
  10. Replies
    3
    Views
    7,943

    Re: Shoulder / Elbow paired servo calibration

    Thanks for the quick response and suggestions. I captured the position values of the tandem servos and the actual positions were pretty different from the 1023 - x theoretical position value. ...
  11. Replies
    3
    Views
    7,943

    Shoulder / Elbow paired servo calibration

    Hi,
    For the shoulder and elbow joints, the PhantomX Reactor Arm has 2 mirrored servos that work together to share the load. In trying to create a Master / Slave control, I read the position of the...
  12. Replies
    10
    Views
    12,345

    Re: stk500 Error with new Arbotix-M board

    Thanks for the reply Tyberius,

    I did get in touch with Trossen support and they tried to help me. I was going to order another board as a replacement / backup so they went ahead and included an...
  13. Replies
    10
    Views
    12,345

    Re: stk500 Error with new Arbotix-M board

    I appear to be having the same problem with my Arbotix-M board. It's been working for a couple months but just all of a sudden it stopped working. I checked everything above already (except for...
  14. Replies
    6
    Views
    6,407

    Question(s) Re: Cable length limit for Dynamixel AX-12A?

    Thanks again for the input. I'll give t his a try. Interestingly, I was able to use 5 servos / hubs to connect 6 250mm wires together and it worked fine. Perhaps it was a problem with the cable I...
  15. Replies
    6
    Views
    6,407

    Question(s) Re: Cable length limit for Dynamixel AX-12A?

    Thanks for the idea. I'll need to get another Arbotix-M to try that but I have an Arduino Mega 2560 and a USB2AX on the way. It sounds like I might be able to do something similar with those...
  16. Replies
    6
    Views
    6,407

    Question(s) Re: Cable length limit for Dynamixel AX-12A?

    Thanks for the reply. Right now I have them all on the same DXL bus and driven by one program. Loop basically gets all the servo positions of the master and then does a single dxlSyncWritePosition...
  17. Replies
    6
    Views
    6,407

    Question(s) Cable length limit for Dynamixel AX-12A?

    Hi!

    I have a PhantomX Reactor Robot Arm Kit and am trying to control it with a Master/Slave system. The master arm is driven by the same Dynamixel AX-12A servos as the Slave arm and works fine. ...
  18. Question(s) Re: Instructions for "Relaxing" the Dynamixel AX-12A

    Sorry, I see that this was asked in a previous thread here already:

    http://forums.trossenrobotics.com/showthread.php?7501-Using-AX-12A-in-zero-torque-mode&highlight=relax

    Unfortunately, it's...
  19. Question(s) Re: Instructions for "Relaxing" the Dynamixel AX-12A

    I know this thread is a little old, but I am trying to something similar (master/slave control) and had a question about the torque off behavior of the AX-12A servos. I have the dxlFollower example...
  20. Thread: Turbo Fuse

    by gmui
    Replies
    1
    Views
    7,514

    Turbo Fuse

    I just received the PhantomX robot arm and had a question about using Turbo Fuse for securing the screws. If I plan to build the arm but then intend to either mod it or take it apart, should I use...
Results 1 to 20 of 20