Search:

Type: Posts; User: SoCalTechTeacher; Keyword(s):

Search: Search took 0.00 seconds.

  1. Replies
    3
    Views
    1,747

    Re: PhantomX Hexapod Boot Delay?

    Yes, the power switch
  2. Replies
    3
    Views
    1,747

    PhantomX Hexapod Boot Delay?

    With the help of this board I built the PhantomX Hexapod and have used it several times a month. Recently I noticed a lag or delay (10+ seconds) to the bot "waking up" (legs move) form the time the...
  3. Replies
    38
    Views
    9,794

    DynaManager Not Finding Servos

    Building the PhantomX Hexapod and am trying to use the DynaMannager as instructed to ID the servos.

    I keep getting the same message "No Servo Found"
    1) I am using the ArbotiX-M Board
    2) I have...
  4. Re: Question: Using Arduino IDE 1.8.1 and Can't See My ArbotiX-M on the Board List

    I'm on step 6: Program the ArbotiX-M Robocontroller to Control a DYNAMIXEL ServoIt is directing me to connect the ArbotiX-M board to and external power supply. I don't have a 12v power adapter...
  5. Re: Question: Using Arduino IDE 1.8.1 and Can't See My ArbotiX-M on the Board List

    For the benefit of any other lost soul like myself.
    I found the issue: FTDI cable was reversed.

    Thanks to the board for your tolerance and support.
  6. Re: Question: Using Arduino IDE 1.8.1 and Can't See My ArbotiX-M on the Board List

    So I uninstalled Arduino 1.8.2 and installed 1.0.6. Brought over the recommended files. Connected to the controller. Located the correct board. Everything is great. Then I try to upload the...
  7. Re: Question: Using Arduino IDE 1.8.1 and Can't See My ArbotiX-M on the Board List

    Thank you all. I will revert to 1.0.x.
  8. Re: Question: Using Arduino IDE 1.8.1 and Can't See My ArbotiX-M on the Board List

    So. I should ditch Arduino 1.8.1 and revert back to 1.6.x?
  9. Question: Using Arduino IDE 1.8.1 and Can't See My ArbotiX-M on the Board List

    Thank you all for your time...
    I've built a Phantom X Hexapod Mark III

    This my first arduino rodeo. I've followed the instructions from the Trossen site and downloaded the file library zip file....
Results 1 to 9 of 9