Search:

Type: Posts; User: Ulysse; Keyword(s):

Search: Search took 0.01 seconds.

  1. Replies
    12
    Views
    12,106

    Project Re: Pablo, Land Art artist

    Soon ready to work, remains to make the tool to trace (this one is a prototype).


    https://youtu.be/UG6rtTHKjbA
  2. Replies
    12
    Views
    12,106

    Project Re: Pablo, Land Art artist

    Some news from Pablo :

    https://youtu.be/_5T0tlDGh2c
  3. Replies
    1
    Views
    2,434

    Question(s) Re: wheelchair motor : removal of wheel hub

    Hi,
    to remove the wheel of Pablo :

    6675

    Do I understand the question?
  4. Replies
    12
    Views
    12,106

    Project Re: Pablo, Land Art artist

    The chalenge of Pablo today : follow a programmed path and return to the starting point without using GPS.

    Not so bad. Small Errors are cumulative but nothing nasty, the final attitude will be...
  5. Replies
    12
    Views
    12,106

    Project Re: Pablo, Land Art artist

    Et voilĂ 
    Pablo is now equipped with an electronic compass.


    https://www.youtube.com/watch?v=4f5pMFEfb0M
  6. Replies
    12
    Views
    12,106

    Project Re: Pablo, Land Art artist

    Thrue, crabs are at the beach and cow is in the field. :wink:
    Seriously, PABLO lost its battery (12 VDC ), so it is now connected to the mains by a power supply to continue to develop. The Adafruit...
  7. Replies
    12
    Views
    12,106

    Project Re: Pablo, Land Art artist

    Thank you for your support !

    Today we test odometry (video).
    The goal is to validate the measurement of distances with 2 odometrics sensors, one by wheel., the average of the two is calculated....
  8. Replies
    12
    Views
    12,106

    Project Re: Pablo, Land Art artist

    To prepare a plot, I first select the shape to draw in the sand. I chose the DXF format as it is wide spread and it contains vectors. later I can use another format.
    I then use an C# application to...
  9. Replies
    12
    Views
    12,106

    Project Pablo, Land Art artist

    Pablo is a French autonomus rover using motors, sabertooth controller, GPS, odometer ... The goal is to draw large drawings on the French beaches.
    The mission is prepared before departure, the...
  10. Replies
    1,117
    Views
    600,531

    Sticky: Re: Introduce yourself!

    Hi, I'm Ulysse, from France. I try to buid an autonomous rover called PABLO using motors, sabertooth controller, GPS, odometer ... C # Programming with visual studio.
    The goal is to draw large...
Results 1 to 10 of 10