Search:

Type: Posts; User: jstarne1; Keyword(s):

Search: Search took 0.00 seconds.

  1. Thread: 19x AX-12A

    by jstarne1
    Replies
    1
    Views
    10,320

    Re: 19x AX-12A

    Hi are these still available? I might like to work out something. Thanks
  2. Replies
    3
    Views
    5,991

    Question(s) Re: How to start off in microcontrollers?

    @jheckman if your looking for an inexpensive learning platform a EZB uses a Atmega 128 with 40mhz clock. It has a wireless Bluetooth connection to be controlled by a PC. You can learn scripting ,...
  3. Project Re: JARVIS 2000 , a tomy omnibot 2000, vacuum, pc inside and lots of custom parts

    47284729
    I decided to use the original wheels but recoat the gray dry rubber with new black plastic dip. They look great now.
  4. Project Re: JARVIS 2000 , a tomy omnibot 2000, vacuum, pc inside and lots of custom parts

    4727 here is my proposed wiring diagram though it may differ slightly.
  5. Project Re: JARVIS 2000 , a tomy omnibot 2000, vacuum, pc inside and lots of custom parts

    Error double post
  6. Project Re: JARVIS 2000 , a tomy omnibot 2000, vacuum, pc inside and lots of custom parts

    I have not picked placement for the microcontrollers yet , the two EZ Boards with 128 AT Mega chip with Bluetooth connectivity. I do want to put a motherboard in however so it can be more autonomous....
  7. Project Re: JARVIS 2000 , a tomy omnibot 2000, vacuum, pc inside and lots of custom parts

    4725
    This was my first idea for battery placement but I'm concerned about how high up the torso I put weight.
  8. Project Re: JARVIS 2000 , a tomy omnibot 2000, vacuum, pc inside and lots of custom parts

    I'm prepping a couple batteries for use with the robot, large wire and xt60 turnigy 60 amp connectors4724
  9. Project Re: JARVIS 2000 , a tomy omnibot 2000, vacuum, pc inside and lots of custom parts

    It fits in the frame well , sorry it uploads twice sometimes.4723
  10. Project Re: JARVIS 2000 , a tomy omnibot 2000, vacuum, pc inside and lots of custom parts

    4720 , this is the battery monitor display I retro fitted into the area where the clock was originally mounted. It shows voltage , temp, wattage being used and amps. They are separated into each...
  11. Project Re: JARVIS 2000 , a tomy omnibot 2000, vacuum, pc inside and lots of custom parts

    4717
    47184719
  12. Project Re: JARVIS 2000 , a tomy omnibot 2000, vacuum, pc inside and lots of custom parts

    4714
    Here you can see the delicate gear setups for the wrist turn and claw to close. I will gut all this out and reinforce the plastic shell with fiberglass. Then maybe something a little more up to...
  13. Project Re: JARVIS 2000 , a tomy omnibot 2000, vacuum, pc inside and lots of custom parts

    4711
    This was the original Omnibot 20004712
    This is the shark vacuum behind the soon to be completely renovated Omnibot. The idea here was to make it into a backpack.4713
    The robot is 27 years old...
  14. Replies
    3
    Views
    16,365

    Just For Fun Re: Omniduino - Tomy Omnibot hack!

    I'm doing a Omnibot 2000 rebuild and upgrade to all modern electronics, servos, motors and additional abilities.
  15. Project Re: JARVIS 2000 , a tomy omnibot 2000, vacuum, pc inside and lots of custom parts

    This is my first "real" robot but I've been into electronics and such for a while. If you have seen a Omnibot 2000 you will notice only the head and arms are the same , the torso is from a Robbie...
  16. Project Re: JARVIS 2000 , a tomy omnibot 2000, vacuum, pc inside and lots of custom parts

    I'm using two EZ boards from EZ-Robot.com . one board is for the arms , and neck. The other for the fixed ultrasonics around the base and IR cliff sensors under the base too. Both boards will be...
  17. Project JARVIS 2000 , a tomy omnibot 2000, vacuum, pc inside and lots of custom parts

    Hello all, this is my first autonomous robot project ... Technically my first robot at all since I started and I've had a couple side projects since like a air soft robot and Robot Squeegee floor mop...
  18. Replies
    5
    Views
    4,519

    Re: Question about mechs

    Nothing wrong with a lower cost bracket of competition. These robots cost hundreds or more at times so thats a cool idea.
  19. Thread: EZ-Robot kit

    by jstarne1
    Replies
    12
    Views
    9,659

    Re: EZ-Robot kit

    Sry my phone double posted
  20. Thread: EZ-Robot kit

    by jstarne1
    Replies
    12
    Views
    9,659

    Re: EZ-Robot kit

    It says in the rules connecting to the wifi router provided is not required. So I cant use my ez robot cam even though lots of them can be in the same room and it doesn't affect my wifi? If thats...
  21. Thread: EZ-Robot kit

    by jstarne1
    Replies
    12
    Views
    9,659

    Re: EZ-Robot kit

    It says in the rules connecting to the wifi router provided is not required. So I cant use my ez robot cam even though lots of them can be in the same room and it doesn't affect my wifi? If thats...
  22. Thread: EZ-Robot kit

    by jstarne1
    Replies
    12
    Views
    9,659

    Re: EZ-Robot kit

    The cam is wifi but it connects directy to a paired usb receiver. You can run as many as you want in the same room or even mutliple cams on one robot. Ez robot is a great platform. Im building 4...
  23. Replies
    7
    Views
    9,514

    Re: For Sale: 2x Lynxmotion Scout(BIG!!)

    Are these still available. I see this thread is a couple months old. And do you accept trade?
  24. Re: Camo Omnibot Warrior w/ Tracks for Beginner class powered by EZ-Robot by J. Starnes

    4240 here is my brother holding up the gun arms we were thinking of using.
  25. Camo Omnibot Warrior w/ Tracks for Beginner class powered by EZ-Robot by J. Starnes

    4238mg4239
  26. Re: Rattler warrior for beginner class powered by Ez-Robot , by J Starnes

    The center cannon uses air to launch nerf type darts. It is fully automatic. The side guns are cyber strike electric airsoft weapons. I have seen these in pics except with the handles cut off in...
  27. Re: Rattler warrior for beginner class powered by Ez-Robot , by J Starnes

    Couple more picshttp://www.ez-robot.com/uploads/20121022_011120-634864580383125000.jpghttp://www.ez-robot.com/uploads/20121022_011731-634864595978125000.jpg this is side view sitting on my couch with...
  28. Rattler warrior for beginner class powered by Ez-Robot , by J Starnes

    Hello this is my very first post and im already a member at ez-robot for nearly a year. Im building both my robot and brothers first mech warrior for beginner class. Using a 2.4 ghz serialized cam...
Results 1 to 28 of 28