Search:

Type: Posts; User: metal; Keyword(s):

Search: Search took 0.00 seconds.

  1. Replies
    3
    Views
    5,289

    Question(s) Connection Understanding

    I have a Problem with the Power of AX12. I have a Raspberry PIE an USB2AX and and 6 Port Hub. I have played with RC Cars and ESC's a lot but i thing from the USB2AX i can only connect GND and the...
  2. Replies
    149
    Views
    298,282

    Sticky: Re: MW 2013+ Ruleset Additions and Changes Discussion

    Ok thats another good thing why they use RFID. So they also can made 2 Weapens allowed. Because the Robot have to stay on another Label for a defined time to armed the second wepaon (activate 2...
  3. Replies
    149
    Views
    298,282

    Sticky: Re: MW 2013+ Ruleset Additions and Changes Discussion

    Hello from Austria..

    I have a capture the flag idea. The RFID System is very nice.. But in the original Capture the Flag you lost the Flag when you got to much damage.
    So they have do Pick up...
  4. Replies
    2
    Views
    9,537

    Arduino Due vs Arbotix vs Axon2

    I would know, which controller did you give a chance? Is the new Adruino Due better then the Arbotix?

    I say (in my mind) the arbotix have a bigger community then the Axon2. But the Axon 2 have...
  5. Replies
    6
    Views
    10,355

    Question(s) Re: Beginner from Austria

    Thanks for the realy great answers.. i think i start with a bioloid premium kit. so i can use the servos in the future with an arbotix..

    i also start language tranfer to german for the arbotix...
  6. Replies
    34
    Views
    34,195

    Re: Selling : AX-12+ servos / Bioloid Primium Kits

    a bioloid premium left?
  7. Replies
    6
    Views
    10,355

    Question(s) Beginner from Austria

    Hey Folks,

    my Name is Daniel i was born in austria, i am 30 years old, and i will start in robotics.
    My skill that i have are: c++, c#, java, arduino, multiwiicopter, modell plane flying.

    I...
Results 1 to 7 of 7