Search:

Type: Posts; User: ZeeGee; Keyword(s):

Search: Search took 0.03 seconds.

  1. Replies
    16
    Views
    27,233

    Re: Cell phone as a microcontroller?

    well, actually I was not referring to unlock, but rather developing apps (especially native apps, as opposed to midlets) on the phone. This is because a lot of phones have nice conectivity devices...
  2. Replies
    6
    Views
    9,637

    Re: SSC-32 and Sabertooth 2x5

    Thanks Dave & Tyberius. I actually figured out late yesterday: it's exactly the same as what Dave mentioned. Turning switch 6 to OFF (i.e. micro controller mode) will resolve the issue.

    But I'm...
  3. Replies
    6
    Views
    9,637

    SSC-32 and Sabertooth 2x5

    I'm using SSC-32 to control two DC motors via Sabertooth 2x5, however I'm seeing some strange "deadzone" beahvior on S2 (channel 2). Basically I can do full forward and backward on S1, but with S2,...
  4. Replies
    36
    Views
    32,393

    Re: Making a Pan Tilt work with Joy stick

    So here's the code in the attachment. I did not get a chance to work on it, so it basically won't work out-of-box on your PC because it requires certain set up.

    The code receives data from a USB...
  5. Replies
    36
    Views
    32,393

    Re: Making a Pan Tilt work with Joy stick

    sure, folks. I'll attach it here once I get home from work.
  6. Replies
    36
    Views
    32,393

    Re: Making a Pan Tilt work with Joy stick

    I actually just did this recently.

    My setup: Logitech PS3 controller with USB interface, SSC-32 controller

    My program is based on this C# USB HID Device component here:...
  7. Replies
    16
    Views
    27,233

    Re: Cell phone as a microcontroller?

    Cell phone manufacturers tend to lock their phones down. So I'm pretty sure modern cell phones get the processing power and the interfaces to do so, but it might be hard to open it up.

    You might...
  8. Replies
    3
    Views
    5,231

    Re: Nokia in Bioloid?

    Sorry I was wrong. According to this post: http://www.internettablettalk.com/forums/showthread.php?t=13059. It did support USB host, and the OP actually succeeded in doing a USB to serial (with some...
  9. Replies
    3
    Views
    5,231

    Re: Nokia in Bioloid?

    I doubted if USB to BUS board will work because that'll require the tablet to support USB host mode; but I think the tablet probably only work as a slave device. Best bet is still probably a...
Results 1 to 9 of 9