Hum I live up in Prescott, how do I keep or get updated on this.:rolleyes:
This could be fun.
Type: Posts; User: LloydF; Keyword(s):
Hum I live up in Prescott, how do I keep or get updated on this.:rolleyes:
This could be fun.
Very nice Idea.:rolleyes:
Much better than my tenny runner approach and turning more screws than my fingers would like. If you get any breaks on the pi-4 that would be fun to try. My HROS-1 is...
Ah heck! The NeoPixel LED's are not working. Sigh, on inspection the servo cable used was not modified, so I'll order some WS2812B and do it my self. Still it was almost a perfect build. I'll let...
No. Sorry I have not upgraded this robot past the rp-3, sigh!:wink:
Rick to the rescue.:veryhappy:
Naturally it is interbotix. Only word I did not try, although i did not think "dam robot" was going to work anyway..
So off the the races. I'll post some pictures as...
I have my new Hexapod on the charger. Ran updates and noticed hum I do not know the password for this robot.
This robot needs a few links to the software for it to be usefull. It is running ROS1...
Hum. Well I did find ROS Robotics Projects (second edition). It seem to be up to date. YEA!:rolleyes:
I am running ROS1 on Noetic ninjemys and Ubuntu 20.04. There are Like 6 setups offered on the ROBOTIS WEB page now.
I have my pi4 working with the ROS1 and the Raspberry pi3B+ on ROS2 with Dashing...
There is a new ubuntu-mate-desktop for 18.04 for the rpi4. :tongue:
https://www.youtube.com/watch?v=fZbJIe2oj8k
I finally put a manipulator onto my waffle-pi, and it works yea!! :tongue:
7655
I Love this robot arm, I Have two with plates and one on a tb3 waffle which is being upgraded to a PI4, woot!. It is a great way to Learn the ins and outs of robotic arms with ROS industrial. I do...
It looks like Ubiquuity has a image for the rpi4.:wink:
Note (I should note that this is Loaded with ROS Kinect 16.04.)
For a direct download:
https://downloads.ubiquityrobotics.com/pi.html
:o Yep, sorry about that, I think I fixed the original post to be accurate.
This is really a nice bot with a price point that is really nice so...Yea! I am playing with the SDK now.:cool:
It seem...
Temi the Robot has movement and navigation capabilities runs off of it's 2 ARM computers and uses a set of 16 sensors
including a Lidar, depth cameras…
The Specs:...
Hum. They have a setup were you can switch back and forth to see the code in python or scratch, but they have so many built
in specialty routines that can do: follow me and face detection, and hand...
I have been playing/working :tongue: with this robot and am now starting to program it.
It took 2 hours to build and is, loads of fun. ( price $499.00 )
https://www.youtube.com/watch?v=hoTK9CZBnaE...
Yea, once Ubuntu officially supports Buster things will really take off.
I am not sure when that is.:confused:
Take a look at this book and see what is a good start. The download link is at the bottom of the page.
https://community.robotsource.org/t/download-the-ros-robot-programming-book-for-free/51
HUM. what do you know about:
1). ROS ( Robot Operating System ) ?:)
You can run the simulator but for me $250 or so a servo is much better than a grand ea.
2). Are you trying to build a industrial...
Someone pointed out this Open_manipulator_6dof_application. https://github.com/zang09/open_manip...of_application
I have used this and it works great, I did have the
3-d parts machine out of...
If it is true that Walmart is going to carry the rpi4, this could be the pi's chance to really shine.:cool:
I am now cheering for the PI4. I have the Raspbian Desktop Image up and running but No ROS image and I could not get that ROSberryPI...
I got my first RPI4 today have the Raspberry Desktop running and am now working on ROS. Happy day's :wink:
(Note. Tried a 1080p monitor, and this board runs way hot even with heat sinks in 4k with ...
Someone pointed out this Open_manipulator_6dof_application. https://github.com/zang09/open_manipulator_6dof_application
I have got to try this out.
If your haveing troble updateing this is why.
"The machine hosting build.ros.org 47, which is the build farm for ROS 1, was recently compromised. We took that machine offline and are in the...
Well I have 2 of the new rpi4's with 4GB of Memory on pre-order. This will be nice....
The Intel RGB camera stopped working, it turns out the dd_dynamic_reconfigure came up missing in the install instructions some place along the way. So I used github to download the source and all is...
LOL and unfortunately there is no RTC (Real Time Clock) on this model.:tongue:
Sweet! Got the pick and place example to work. It would seem there was a typo, on there web page.
On section 9.1.3.3, after launching the arm initialization routine, they use this command line to...
75187519
The fan was overkill as I have never been able to get it hot enough to turn on:sad:
Once booted onto the USB this is a full on speed demon with V2 camera and as far as I can tell a...
I noticed that most, if not all the TB3 files are now on ROS Melodic Ubuntu 18.04 :happy:
Has anyone tried running the TB3 on Ubuntu 18.04 yet?
I have this new SBC the Jetson NANO. I configured...
God knows what happened, but I rebuilt Ubuntu and the ROS packages and everything is Okay now :o
This was easier than running all them bug reports. (Note. Found if you are playing with the End...
Hum, that last link may be useful, thank you.
I am so unhappy. The dynamixel-workbench will no longer compile, which make the arm :confused: dead. I hope they fix it, not sure how to get
one of there programmers to look at what the hell he is...
I updated everything an ran it on Ubuntu Mate, installed ROS, because i have plans :cool:, and everything seems to be working, with a little work on the ps3.
I have had issues with rubber products and the dry hot air of Arizona ( just nasty to most plastic's). Anyhow when I printed
out these wheels they have three groves in them that are exactly the size...
I am happy to report that I have been able to get everything working, with the exception of the RC100 joystick with the OpenManipuiator. It should work but hum:confused: I am still working on that...
7453
The default configuration for the manipulator is on the u2d2 or a USB serial connection, and it works really well.
They have a direct link to some STL files for 3-D printers, so I printed some...
I printed out and put the tire and caster configuration from the turtlebot3 friends Carrier, onto my tb3 to see if it would help with getting up onto carpets. It worked and works, giving me just...
744374447445
Here it is. I downloaded the build instructions, as this one comes with no instructions, but useful links :wink:
There Disclaimer really needs to be more visible. i.e Base plate is...