Search:

Type: Posts; User: jveejay; Keyword(s):

Search: Search took 0.00 seconds.

  1. Replies
    24
    Views
    32,115

    Re: Beta Tester Roll Call

    Indeed -- that's what I'm picking up today from Intel ;)
  2. Replies
    24
    Views
    32,115

    Re: Beta Tester Roll Call

    I've got vision processing through the PiCamera. With the Edison it was a black hole, I had no idea what to do so I took it out and went with the Pi. So now Harvey is able to detect faces. But I've...
  3. Replies
    24
    Views
    32,115

    Re: Beta Tester Roll Call

    Looks great! Wow you really managed to get it to walk with that USB hub huh?!
  4. Replies
    1
    Views
    4,785

    Broken part -- needing replacement

    Hi there Trossen folks,

    I broke my neck plate (P1 I believe), and I was wondering if it is possible to get a replacement for it. My work has pretty much come to stand still without it, so it would...
  5. Sticky: Re: Google Hangouts HR-OS1 Beta Development Open House

    Curious, are we doing this?
  6. Replies
    25
    Views
    48,255

    Re: node_server example

    I hear ya, I'd make the same call.

    IMHO, we should standardize the pages on app.js, instead of hardcoding it as it is right now.

    For e.g., in my setup, I basically have the system populate its...
  7. Replies
    25
    Views
    48,255

    Re: node_server example

    OK, I think I will just push my code changes sometime in the next day or two. Then you should be able to use the demo code. Sorry, I'd push right away but I just threw out my Edison and put in the Pi...
  8. Replies
    11
    Views
    29,832

    Sticky: News/Announcement Re: Fixed Camera Wiring Diagram

    Sweet. Thanks for letting me know. I was counting on using the RPi 2 camera, so that I can leverage the SoC fully for fast processing of video. I had to get an extension cable because the 150mm...
  9. Sticky: Re: Google Hangouts HR-OS1 Beta Development Open House

    Works for me, and it would be terrific to have another meet-up with everyone. I'm dying to see what people are doing with their robots. I'm not the creative kind, haha. So you can imagine why I am...
  10. Replies
    11
    Views
    29,832

    Sticky: News/Announcement Re: Fixed Camera Wiring Diagram

    By the way, I have not used the RobotGeek VGA USB webcam. Do you guys have prior experience with it? Could someone describe your experience? I haven't played with it enough, so it is possible that it...
  11. Replies
    11
    Views
    29,832

    Sticky: News/Announcement Re: Fixed Camera Wiring Diagram

    I originally built the bot fully using the Edison, but then the camera seemed to be a big issue since the performance is rather weak with the Edison. You can't get enough FPS doing real-time vision...
  12. Replies
    11
    Views
    29,832

    Sticky: News/Announcement Re: Fixed Camera Wiring Diagram

    Hey there,

    Where can I find the specs on the camera? Also, is there any reason that we can/not use the raspi camera with the Pi?
  13. Replies
    25
    Views
    48,255

    Re: node_server example

    I was in touch with them, and Andrew said that they won't be posting that because it shouldn't require that. He said he is going to look into it this evening. Apparently, that's some legacy code...
  14. Replies
    49
    Views
    126,790

    Sticky: News/Announcement Re: HR-OS1 Documentation

    So who is using Edison? I'm using it, and I'm already frustrated because I can't hook up the camera to it, let alone think about other peripherals. What are the thoughts here going forward Kyle?! Is...
  15. Replies
    21
    Views
    51,451

    Sticky: Re: Welcome HR-OS1 Beta Testers! Introduce yourself

    Hi,

    Scientist, professor, learner, educator... that's me! I'm from Austin, and I'm a professor at The University of Texas at Austin. I've gotten interested in the HROS1 because I'm curious about...
  16. Replies
    25
    Views
    48,255

    Re: node_server example

    Hey there,

    I have been able to get it up and running, but only by writing the missing code in the app.js file. The app.js server file is incomplete, there are still pending functions that need to...
  17. Sticky: Re: Google Hangouts HR-OS1 Beta Development Open House

    Hey guys,

    When is the next hangout?!
Results 1 to 17 of 17