Search:

Type: Posts; User: jwatte; Keyword(s):

Page 1 of 13 1 2 3 4

Search: Search took 0.06 seconds.

  1. Replies
    9
    Views
    193

    Re: Dumb Idea: So like... what about jumpjets?

    If you could actually bring that to the competition, all the drinks and food for you are on me for the duration.
    No matter that open fire is against the rules and nobody would actually compete...
  2. Replies
    5
    Views
    165

    Question(s) Re: Parallel Robot kinematics

    You say numerical analysis, but do you have trigonometry? Linear algebra? Calculus?

    Assuming you know how to project from 3D to 2D (project along plane normals) the what you do is calculate the 3D...
  3. Replies
    9
    Views
    193

    Re: Dumb Idea: So like... what about jumpjets?

    Funny you should say that ... I did the math on it a couple of years back, and I could strap two EDFs with angled actuators, AND a battery big enough to run them for a total of 40-60 seconds, onto...
  4. Replies
    23
    Views
    3,584

    Re: Mech Warfare at Bay Area Maker Faire 2019

    I just received the registration link by email (thanks, guys!) but I don't know when the last possible date is.
  5. Replies
    5
    Views
    165

    Question(s) Re: Parallel Robot kinematics

    So, at the top there are three single-axis rotational joints, each set 120 degrees apart. They each establish a plane within which each "femur" rotates.

    Then each femur has a parallel linkage of...
  6. Replies
    5
    Views
    165

    Question(s) Re: Parallel Robot kinematics

    What, specifically, do you need help with? Do you have a sketch of the links and actuators?

    In general, if you have 4 DOF but want to constrain 6 DOF (position + orientation) you're screwed,...
  7. Replies
    17
    Views
    2,634

    Re: PhatomX with XL430-W250 servos

    No, I have not played with the data sendback. I look forward to hearing what you find!
  8. Replies
    1
    Views
    289

    Question(s) Re: Denavit–Hartenberg parameters

    I just multiply out the transforms from the root using 4D matrices (graphs/physics-simulation style,) so I don't use that convention.
    Also, I express the transforms using identity in the "servo is...
  9. Replies
    17
    Views
    2,634

    Re: PhatomX with XL430-W250 servos

    Yes, that's correct! You should put in 3.3V to 5V on the red wire, ground on the black wire, and you will get out UART at 115200 bps, 8 bit bytes, 1 stop bit, no parity.
    The protocol itself is easy...
  10. Replies
    247
    Views
    83,588

    Project Re: More Mule then Rover?

    It's a robot controlled lift! Stylish!
  11. Re: How to use nrf24l01 wireless module with Arbotix-M Robocontroller & Arduino Mega 2560 r3 to communicate between each other?

    You need to make the appropriate connections to the NRF chip, which includes the SPI bus and the chip-enable signal.
    Any available digital pin "ought" to work for Chip Enable -- it's a low-bandwidth...
  12. Question(s) Re: AX-12A - When Reading Present Position Getting Inaccurate Reading

    A status packet is a response with zero data. They're pretty much the same thing.
    A command packet and an instruction packet are names for the same thing, too.

    It can't possibly be the case that...
  13. Question(s) Re: AX-12A - When Reading Present Position Getting Inaccurate Reading

    I would not expect ser.readline() to return a proper response. The response packet has a very similar format as the command packet, and needs to be appropriately decoded.
  14. Replies
    3
    Views
    539

    Re: Sync_write to multiple servos

    Is the problem in the servos, or with the board/sketch?
    Is this a buffer overflow problem in the "serial tosser" code?
    If you hook up a scope/logic analyzer to the servo TTL bus, does the 10+...
  15. Replies
    17
    Views
    2,634

    Re: PhatomX with XL430-W250 servos

    The receiver outputs this protocol:
    https://github.com/jwatte/donkey_racing/blob/master/teensy_hat_firmware/FlySkyIBus.h
    It's ten 16-bit integers with some surrounding framing information.
  16. Replies
    34
    Views
    14,193

    Re: Numa V2 - Quad Mech

    Peanuts incoming:

    For Onyx (RIP) I defined a "standard leg" where the coordinate system is "forward/back," "out/in," and "up/down."

    The IK solution then runs in terms of this standard leg, and...
  17. Replies
    1
    Views
    468

    Re: Cobot Research and Development

    Looks awesome!

    Make it bus away the table once it's empty, perhaps?

    Sing and dance for birthdays? (and serve/cut cake?)
  18. Replies
    23
    Views
    3,584

    Re: Mech Warfare at Bay Area Maker Faire 2019

    I would love STL files!
    Do these mount to the Double Eagle AEGs, or some other kind?
  19. Replies
    247
    Views
    83,588

    Project Re: More Mule then Rover?

    That sounds exciting!

    Curiousity killing cats:
    How is the "L" part attached? Welded?
    How thick is the plate that the bolts go through?
  20. Replies
    23
    Views
    3,584

    Re: Mech Warfare at Bay Area Maker Faire 2019

    Yeah, some kind of light preload on the feed seems needed. The design I've been using seemed to have a 10-15% dry fire / false load rate.
    The twisty 1/4" spring feed seemed alright, although I don't...
  21. Replies
    17
    Views
    2,634

    Re: PhatomX with XL430-W250 servos

    The U2D2 (and, to be fair, the USB2AX,) both are kind-of expensive for what they are: A $2 chip on a board with some connectors.
    Sure, the market might be only a few hundred, so you'd need a fair...
  22. Replies
    17
    Views
    2,634

    Re: PhatomX with XL430-W250 servos

    I've had great luck with the FS-i6S controller/receiver: https://amzn.to/2T7pP5J The receiver actually spits out a simple protocol of reveived data over serial port, so you don't need to decode the...
  23. Replies
    1
    Views
    925

    Question(s) Re: How can I connect ROS with Unreal engine?

    I've only created Unreal plugins in Visual Studio. There, the integration is actually very nice.

    I imagine if you have an exposed function in your plugin and you can call it from Blueprint, then...
  24. Replies
    247
    Views
    83,588

    Project Re: More Mule then Rover?

    Interesting!

    How do you figure out where the main flex is coming from? Do you have video from the sides while it's doing it?
  25. Replies
    247
    Views
    83,588

    Project Re: More Mule then Rover?

    Only one way to settle this: Build TWO snow plowing mules, one with an aluminum bracket, and one with steel, and measure what the relevant bracket lifetimes are under equivalent workloads!
    ...
  26. Replies
    247
    Views
    83,588

    Project Re: More Mule then Rover?

    Sure, aluminum will fatigue and break, but, you know, they make airplanes out of it. With enough safety margin, you'll be fine :-)

    Anyway, if he wants to make another bracket because he enjoys...
  27. Replies
    247
    Views
    83,588

    Project Re: More Mule then Rover?

    It's the torque, more than the power, that matters for your bracket. Think of it this way: A motor that is stalled develops zero power (at the shaft) but develops a lot of force at the mount!
    You...
  28. Re: How to change the speed of the AX12a and Read its current speed ?

    The value range is documented in the manual for the servo. I don't remember the exactly values, but because it's a 2-byte register, the value range is higher than 0-255.
    The "_L" and "_H" are the...
  29. Replies
    4
    Views
    831

    Question(s) Re: torque control for ax 12a

    Yes, almost all motors of this kind have a continuous duty rating of 20-25% of the maximum instantaneous rating. It's a fact of physics.

    There is another thread on this board about adding external...
  30. Replies
    23
    Views
    3,584

    Re: Mech Warfare at Bay Area Maker Faire 2019

    That's 10 minutes from where I live and 5 minutes from where I work, so ... yeah, I'll have to be there. I'll borrow my daughter's AX-12 based 'mech. (Onyx has donated too many pieces to be...
  31. Replies
    3
    Views
    748

    Re: C program for AX

    Yes, a zero bit is sent as wire-to-ground on the TTL UART bus. It works fine to wire a microcontroller UART straight to the servo, EXCEPT when the servo tries to send a response back, the...
  32. Replies
    6
    Views
    1,223

    Re: XL430-W250 Stop moving randomly

    Are you sure it's the motor? If so, is it signaling an error? (Not reading status back is in general a bad habit, because it makes debugging harder.)

    If you hook up a scope or logic analyzer on...
  33. Re: Dynamixel MX-64T Torque control with Arbotix

    Have you enabled torque with register 24?
  34. Replies
    4
    Views
    831

    Question(s) Re: torque control for ax 12a

    If the servo cannot get to the desired goal, it will generate an error to tell you this. The practice of "set a goal position that is not achievable" is not generally useful for controlling these...
  35. Replies
    6
    Views
    1,223

    Re: XL430-W250 Stop moving randomly

    Not really. The main question is if you have command response turned on; if so, you may have to wait for a timeout if the servo didn't get the packet (because sometimes it's slighlty slow to...
  36. Replies
    4
    Views
    1,097

    Re: Puppet Master/ Slave setup

    Is the theory that you have two robots, one to capture the pose, and one to play it back?
    That would require software.
    The user "tician" on this board used to support a graduate art program that...
  37. Replies
    3
    Views
    850

    Project Re: Sinusoidal Servo control using MATLAB

    I don't know how fast Matlab can run -- can it run at 100 Hz itself? If not, then you're going to have to live with whatever it can do ...
  38. Replies
    3
    Views
    850

    Project Re: Sinusoidal Servo control using MATLAB

    The best you can do is to send a very high speed stream of updates -- say, 100 Hz -- for where you want the position to be.

    Let the control algorithm and damping inherent in the servo then drive...
  39. Replies
    4
    Views
    1,097

    Re: Puppet Master/ Slave setup

    The RoboPlus software that comes with the Dynamixel series of servos can do some of those things without programming.
    You have to read the instructions, which are sometimes hard to just FIND, and...
  40. Question(s) Re: Dynamixels AX-12A on OpenCM 9.04 + OpenCM 485: how to send instruction packets

    Here's my setup code for OpenCM 9.04:


    void DxlIO::begin() { afio_remap(AFIO_REMAP_USART1);
    afio_cfg_debug_ports(AFIO_DEBUG_FULL_SWJ_NO_NJRST);
    gpio_set_mode(PORT_TXRX_DIRECTION,...
Results 1 to 40 of 500
Page 1 of 13 1 2 3 4