Not quite the mental image I had. I'm guessing from the T-105 caption, that this is a Terminator variant from Terminator 3, which I haven't seen.
Type: Posts; User: Nocturnal; Keyword(s):
Not quite the mental image I had. I'm guessing from the T-105 caption, that this is a Terminator variant from Terminator 3, which I haven't seen.
:) My hand writing is illegible, unless you happen to have a magnifying glass and a lot of patience. My typing is much much better. I can usually knock out a vaguely amusing short story, but fifty...
Still nothing. Good thing I have a week to prepare to kick myself.
A little off topic, is anyone else participating in NaNoWriMo?
I've still got nothing :)
Hmmm.... Bell's are ringing, but they are all unfortunately, video game related bells.
Is it going to be packing a gun? perhaps a bfg?
Happy belated dirtday 4mem8. I've still got no idea what your building. I'm going to be annoyed if it turns out that I have seen the movie.
*Laughs* I'm not giving up, and I was never interested in the prizes.
Congrats Rudolph :)
:) I've already been using google, and wikipedia, and IMDB. I've encountered a variety of robots that I had never heard of before, but none of the would appear to fit with what 4mem8 is building, so...
:-) If I think of a question that you might answer without lying to me, I will be certain to ask. At the moment, I have to admit, I am stumped.
I do not mean to pry, but you don't by any chance happen to have six fingers on your right hand?
You don't seem to be laughing 4mem8.
Don't make me break out the ROUS
No surprise there. You could say Vizzini is famous for three things, believing himself to be much smarter than everyone else, being very wrong and dying while laughing seconds after having declared...
I could give you a spontaneous response, but here's one I prepared earlier.
It should be OBVIOUS to anyone with sufficient intelligence, a character clearly lacking in most people. All one needs...
Ha ha! You use of jigs to cut things to size reveals EVERYTHING!
And you wonder why we don't trust you.
PayPal leaves a trail, do you accept cash? How much for not only the services detailed above, but a list of all the people who have currently paid you for answers?
I envision something similar to...
Seeing Freeman doesn't bother me, now if someone had a picture of G-Man, I'd be a little more concerned. If I recall correctly, it was G-Man who turned out to be ultimately responsible for the events...
Ok, so you've got the ER1 at the back, the two halves off Wall-e on either side of ED-209, and I think that's J5's base, but whats that in front of the screen on the left hand side of the image?
Is that the same camera as you were talking about over in the Wireless Video thread Adrenalynn?
*laughs* Lot of discussion for something that I wasn't actually proposing as a control method, just using as an easy counter example for network-ability.
I bow to your superior experience.
:) I don't think I would go that far, but based off my experiences with them, if anyone nearby is using any device, that also uses the 2.4ghz range, they are in trouble.
:) If this is a route that you think you might want to go down, a bit of thought now, before you get too far along would be a good idea. Since the method of command and control you decide upon will...
That would be very cool, but latency would be a killer. You'd need some automatic assistance.
Thanks for the welcome guys.
Not sure the kernel subsystems maintainers would agree with you, but fortunately I found a few extra buttons hiding behind the mouse buttons, so its all good.
So in other words, you going to lie in the photos as well..... or are you lying to me now.... Great! now I've got a headache.
Only 27 days to go.
Ok, so your going to lie to me, I can deal with that. Just one question (and given that we've already established your a liar, I'm not going to believe your answer), Will the photos intentionally...
$65US, plus $90US shipping to Australia. I'm working on adding linux support for it atm, running into a little trouble with the 39 buttons... the current joystick api doesn't have quite enough.
...
Has anyone seen the Steel Battalion Controller?
The left joystick only moves left and right, but the hat switch is analog, as are the joysticks and pedals. The gear shift and channel knob are...
I'm in.