Search:

Type: Posts; User: nolimit44; Keyword(s):

Search: Search took 0.01 seconds.

  1. Replies
    0
    Views
    3,130

    Project Transformer Decepticon Robot Eyes

    Here is a video of my Decepticon Robotic Eyes created for my transformer themed car show vehicle that will be installed behind my grill. I want to thank Emilio Iglesias for the hardware design and...
  2. Replies
    17
    Views
    8,140

    Re: Help to finish off program

    anything like this ? lol i tried but am prob not even close


    #include <Servo.h> //include the servo libary - a bunch of code for a host of servo instructions you can use and don't have to...
  3. Replies
    17
    Views
    8,140

    Re: Help to finish off program

    ok so am i adding this to what i already have and just getting rid of the delays or am i removing everything i have in the loop function. i ask this because i have all the motion range of servos...
  4. Replies
    17
    Views
    8,140

    Re: Help to finish off program

    ok after testing the robot eyes for a few days, i noticed that the led will not blink or be on on during servo movement.

    basically the led stays on, blinks, the servo moves to new location, and...
  5. Replies
    17
    Views
    8,140

    Re: Help to finish off program

    thank you very much for taking the time to help me, everything worked great. if i have any other questions ill post again
  6. Replies
    17
    Views
    8,140

    Re: Help to finish off program

    ok i compiled the code and uploaded it , however the unit wont even power on at the push of the button anymore
  7. Replies
    17
    Views
    8,140

    Re: Help to finish off program

    like this ? it errored out during compiling saying undefined reference to loop



    #include <Servo.h> //include the servo libary - a bunch of code for a host of servo instructions you can use...
  8. Replies
    17
    Views
    8,140

    Re: Help to finish off program

    can you help me with this function code, im not a coder and this is my first time doing this kinda stuff so i have no clue how to do it, im just trying to finish this thing for an upcoming car show...
  9. Replies
    17
    Views
    8,140

    Re: Help to finish off program

    i have gotten this code to work with the push button, however it will only shut off now when i press the button in between blinks right as the leds turn off, is there a modification in the code i can...
  10. Replies
    17
    Views
    8,140

    Re: Help to finish off program

    hope this makes reading the code easier. basically i made a set of robotic eyes with leds that blink randomly and a servo which controls the motion from left to right at random speeds and times. i...
  11. Replies
    17
    Views
    8,140

    Help to finish off program

    i am in process of completing my robotic eyes program and ran into a lil issue. I have one of the mini push buttons and am trying to use as both an on and off switch to power an led and servo....
  12. Replies
    0
    Views
    2,691

    First Program with arduinno

    hi, i was wondering if someone would be able to help me. my goal in mind is that i am creating a pair of robotic eyes that i would like to have the leds in the eyes blink at random intervals and...
Results 1 to 12 of 13