Search:

Type: Posts; User: lnxfergy; Keyword(s):

Page 1 of 13 1 2 3 4

Search: Search took 0.05 seconds.

  1. Re: Jimmy the robot, Trossen, Intel and Darwin OP, what am I missing?

    Take a look here for some of the stuff -- not sure everything has been posted yet: https://github.com/21stCenturyRobot

    -Fergs
  2. Replies
    10
    Views
    11,708

    Re: Pypose question

    The baud rate has nothing to do with the motors really. The 38400 baud rate works pretty well with XBEE radios -- which is why it is the default. The problem with higher baud rates (115200, etc) is...
  3. Replies
    10
    Views
    11,708

    Re: Pypose question

    I just pushed a fix to revert the unintentional default baud change: https://github.com/vanadiumlabs/pypose/commit/aea2f90fe7453f8b76a115a9da65e070baea33a4

    In the future, even just commenting on...
  4. Re: Just bought Arbotix-M : Is there a newer manual out? Any problems with it from other owners?

    I pulled your branch into the mainline -- it's better than nothing. Feel free to open any future pull requests for updates -- they will be merged!

    -Fergs
  5. Thread: NUKE issues

    by lnxfergy
    Replies
    46
    Views
    29,580

    Re: NUKE issues

    Just cycling through threads -- I've pushed a fix for the val/rads bug to the mainline (https://github.com/vanadiumlabs/pypose/commit/c47f19fda9db434198b86a264864556375f06c1d)

    Also added the...
  6. Re: PyPose, Arbotix-M and Mac - Issue - PyPose will can not read servos: 1, 2, etc

    I believe you've hit https://github.com/vanadiumlabs/pypose/issues/6

    The fact that the 0015 version works is an interesting fact, I'm adding this thread link to the ticket since that might help...
  7. Re: Just bought Arbotix-M : Is there a newer manual out? Any problems with it from other owners?

    While Vanadium Labs did do the original design, the ArbotiX-M is manufactured and sold entirely by Trossen Robotics, hence the documents on the Vanadium site not being up to date. That said, I also...
  8. Replies
    92
    Views
    93,864

    Re: ArbotiX ROS Stack 0.4.0

    The ~ puts the topic in the local namespace of the node. Thus, if the gripper controller runs with the name "gripper_controller" the full action name becomes "gripper_controller/gripper_action" --...
  9. Thread: Simple_Arms

    by lnxfergy
    Replies
    20
    Views
    23,866

    Re: Simple_Arms

    As stated on the README in the source (https://github.com/vanadiumlabs/simple_arms), simple arms was for Fuerte and earlier (arm_navigation). I don't think I ever really tested on Groovy, because by...
  10. Replies
    5
    Views
    6,014

    Question(s) Re: Geometrically stable gait for Nuke/PyPose

    Looking at the repositories I have checked in, I can't find any code for the RIPPLE_GEO. I definitely was working on that at one point with the version of ISSY that had foot sensors, but I don't...
  11. Thread: Neato + ROS!

    by lnxfergy
    Replies
    2
    Views
    5,206

    Re: Neato + ROS!

    My understanding is that all the Neato models have a *similar* interface, but I don't have any spies inside the company who can confirm this! That said, I have heard some reports of newer models...
  12. Replies
    4
    Views
    10,297

    Re: ROS simple_arm_server for dual arm robot

    You don't need to copy the files -- especially the .action files. What you need to do is remap node names and arguments http://wiki.ros.org/Remapping Arguments Normally this is done by creating a...
  13. Replies
    3
    Views
    27,517

    Project Re: New Rover Project Bulit on ER-1 Platform

    One thing to note here: if you want to leverage the ROS navigation stack (the off-the-shelf software that pretty much can handle driving from point to point collision free), you should really read...
  14. Question(s) Re: (newbie) : Arbotix, dynamixel A12, limits of daisy chaining question.

    The fact that things return to working after a reboot suggests to me that it is a code error. I would suggest adding more information about what you are commanding the servos to do, and if possible,...
  15. Replies
    4
    Views
    10,297

    Re: ROS simple_arm_server for dual arm robot

    I'm not sure what "test.py" means, but if you are using the simple_arm_server node originally developed by me, you would need to run 2 instances, one for each arm, with each having a different name....
  16. Re: Is there a fix for the miss-aligned analog ports on the Arbotix-m

    Can you post the code snippet you are using? I think the issue you are seeing is that you are probably using A1/A3 in the analogRead function. Instead, you should use the pin number:



    // Set...
  17. Question(s) Re: DYNAMIXELs, PhantomX and ArbotiX Lots of questions

    Moving slower probably won't help all that much with heating. Both the AX-18A and RX-24F use coreless motors, which is probably the primary reason they heat up faster. When I had 24Fs, I couldn't...
  18. Replies
    16
    Views
    25,173

    Re: Alternate cheap/easy embedded platforms

    I'm a big fan of the STM32F4 (168Mhz Cortex-M4, with FPU). I've mostly rolled my own boards at this point, but I have posted all of my gcc/libstm setup on github:...
  19. Replies
    23
    Views
    18,914

    Discussion Re: ROS for hobby use

    Not a problem, it's a common misconception and that's why I pointed it out. There is a huge crowd out there that thinks rosserial is a replacement for everything, but it's not.

    -Fergs
  20. Replies
    23
    Views
    18,914

    Discussion Re: ROS for hobby use

    That's a generic crimper, right? I have a pair of the Engineer crimpers, which will kinda do most crimps OK, but it's painful to do a lot of them, and the strain relief isn't always great. For any...
  21. Replies
    23
    Views
    18,914

    Discussion Re: ROS for hobby use

    Thoughts:

    1) EtherCAT & hobby robotics... not sure these mix all that well. I suppose you've handled all of the driver/licensing/etc, but I'm still skeptical of EtherCAT in hobby.

    2) Seeing...
  22. Replies
    23
    Views
    18,914

    Discussion Re: ROS for hobby use

    A couple of comments (From someone who has used ROS first in an academic/hobby situation, later in commercial apps, and still in hobby to this day):

    RE: *replacing cd shell command* -- it's not...
  23. Re: Arbotix - Update Hardware Serial to capabilities of Arduino 1.0.5 capabilities.

    Kurt,

    A ticket or pull request on github is the best way to get changes into the code base. Back in the early days of Arduino when we first rolled out the ArbotiX, we needed to create our own...
  24. Replies
    8
    Views
    5,508

    Re: Arbotix-M is available (and a question)

    485 is more reliable -- when properly used -- although at the given distances the TTL performs about as well. Properly used generally means:

    Use of termination resistors to prevent ringing......
  25. Replies
    5
    Views
    9,826

    Re: Trossen Robotics Github! Arm Software!

    .., and find/understand or write the libraries for peripherals and port all your code.

    ... and then figure out why it's hard faulting, cause it is certainly going to happen at least once, and be...
  26. Replies
    1
    Views
    5,627

    Question(s) Re: motion and measurement models for Kinect

    Seeing as the kinect doesn't move on it's own, I have no idea why you would define a kinect-based motion model.

    As for measurement model, it's pretty similar to a stereo camera. These are two...
  27. Re: compiling Phoenix code for Stock Hexap M2 on linux troubleshooting

    Nothing of consequence has changed in the libraries, or the format of the exported header files, since 0013. The .ppr file format has had some updates over the last couple of releases. The only...
  28. Replies
    10
    Views
    12,520

    Re: Anki AI, physical robotic car racing game

    Some real numbers:

    In 2011, about 165,000 industrial robots were sold worldwide. Since 1963 there have been 2.3 million sold (Source: http://www.worldrobotics.org/index.php?id=home&news_id=261)
    ...
  29. Re: Sucessful users of PyPose/NUKE, how is your system configured?

    And I guess I feel compelled to give just a bit of backstory on why this is broken. Sometime around 2010, (after the v0013 release) I started rewriting the backend to make it possible to support...
  30. Re: Sucessful users of PyPose/NUKE, how is your system configured?

    Oh man. Just logged into the forum for the first time in about a week, and found this thread. Nice work on tracking down these bugs. I'll try to get them merged into the repo soon.

    -Fergs
  31. Re: Sucessful users of PyPose/NUKE, how is your system configured?

    So, a couple of things stand out in this log:

    Limits on servo 11, go to 4096? valid ranges are only 0-4095.. odd, not sure about this.

    But then I went back and looked at your previous .ppr...
  32. Replies
    2
    Views
    5,490

    Re: Query on programming with kuka robots

    I would suggest finding a Kuka forum. I doubt you're going to find that (m)any of our users have worked with a Kuka arm.

    -Fergs
  33. Re: Sucessful users of PyPose/NUKE, how is your system configured?

    Unfortunately, I can't replicate any of those failures in the leg# box on my Ubuntu system. I just added a bit more logging into the function that runs when the NUKE editor is first loaded -- if...
  34. Re: Sucessful users of PyPose/NUKE, how is your system configured?

    Are you using the ZIP from github? We did have a problem like this once before, but I think it was fixed. If you run PyPose from the command line, do you get any errors there (and if so, what are...
  35. Re: Sucessful users of PyPose/NUKE, how is your system configured?

    Yeah, I added the MX-stuff for Tyberius a while back -- but I've never had an MX-based walker to actually test on -- so it is very possible that there are kinks to still be worked out.

    -Fergs
  36. Replies
    14
    Views
    10,525

    Re: Attempting to set up Pypose for a Quad

    There was a bug in sign test -- which I believe I just fixed. Please download the latest code at http://github.com/vanadiumlabs/pypose/zipball/master and give it a try.

    Sorry for the problems,...
  37. Re: Sucessful users of PyPose/NUKE, how is your system configured?

    Could you download http://github.com/vanadiumlabs/pypose/zipball/master, which will now be updated with a patch to the config model function. This makes sign test work on my machine (I somehow missed...
  38. Re: Sucessful users of PyPose/NUKE, how is your system configured?

    Also, would you mind uploading your .ppr file? That might help me test it to see if something got garbled in the file.

    -Fergs
  39. Re: Sucessful users of PyPose/NUKE, how is your system configured?

    I guess I posted the wrong link up there also -- that is for arbotix, not pypose, you have downloaded this though right: http://github.com/vanadiumlabs/pypose/zipball/master ?

    I can't reproduce...
  40. Re: Sucessful users of PyPose/NUKE, how is your system configured?

    Where did you install from? Have you tried the auto-generated-zip from github? http://github.com/vanadiumlabs/arbotix/zipball/master

    -Fergs
Results 1 to 40 of 500
Page 1 of 13 1 2 3 4