If I tell you, I'd have to kill you. :tongue:
Nah, I just had to code into my VBScript to disable the DTR output, which kept resetting the Stamp. I also added a signal byte to both programs.
Type: Posts; User: Judge; Keyword(s):
If I tell you, I'd have to kill you. :tongue:
Nah, I just had to code into my VBScript to disable the DTR output, which kept resetting the Stamp. I also added a signal byte to both programs.
I got it! Answer = Top Secret :cool:!
I need to send my BS2px (COM3) a letter, such as "A", from my pc using VBScript. The Stamp is waiting for the input:
SERIN 16, 188, [LETTER]
The code works fine through the Parallax Stamp...
Hello again,
I'd like to know how to use VBScript to communicate through a serial port, say COM1, to move servos connected to an SSC-32 board. I saw that RoboRealm was recommended, but I...
I have recently purchased an Artigo Builder Kit. The included PS2 cable is too short for my application. I wanted to solder a length of extra wire between the PS2 ports and motherboard pin...
So, essentially, you squeeze the coupler to fit/conform to the shaft, correct?
Is it that easy to bend the coupler by hand? And won't that create a "wobbly" wheel?
Also, do you think it is...
I have the 5" x 7/8" Colson Performa wheels: http://www.trossenrobotics.com/store/p/4272-Colson-Wheel-5-x-7-8-.aspx
I have the Wheel Hub, Colson 7/8" Wheel, 6mm:...
Ok, chica. What are your batteries?
Perfect then, now all I need is a battery that can power 4 motors that can in turn carry the battery and an 8lb. bot for 12 hours (not constant use). Any suggestions? Btw, the toy comment was just...
You think 12 hours is impossible?! My electric wheelchair lasts me 15 hour days at Disney (miles of driving). I didn't know this was just a forum for people building toys.
Well, my goals for this robot are mainly accademic. Physically, I want him to drive around on a level surface indoors. It's simply a rover with a brain. However, I don't want him to last for an...
OK, so 4 x BaneBots Motor Controller (45A peak) and 4 x Banebots 64:1, 36mm Planetary Gearmotor, RS-540 Motor. Do you think those motors are overkill for a 20lb robot? I certainly can't spend more...
Thank you for the prompt reply. I intend to use 5" wheels. Here is the website for my battery http://www.batterygeek.net/product_p/spps-12-444_batterygeek.htm. My rover will use BaneBots Motor...
I'm new to this forum and fairly new to the electronics aspect of robotics. The information online is very confusing, maybe someone can help clarify it for me. Will my 400 watt 12 vdc battery be...