Page 13 of 14 FirstFirst ... 391011121314 LastLast
Results 121 to 130 of 131

Thread: The Robotis TurtleBot3

  1. #121

    Re: The Robotis TurtleBot3

    What's your experience with the Nano? Have you compared it to other boards?
    I kind of don't see what Nvidia wants with the Jetson Nano. It's the quad core ARM from the Jetson TX1 with half of the GPU of the TX1. It's an old GPU architecture (Maxwell) and as such not particularly energy efficient for what it does.
    It's three times the price of the Raspberry Pi 3, so it has no way to compete for "cheap linux." It's a quarter or less of the throughput of the TX2, although it does have a smaller form factor.
    Is it actually "the sweet spot"?

  2. #122

    Re: The Robotis TurtleBot3

    Click image for larger version. 

Name:	nano1.jpg 
Views:	120 
Size:	106.0 KB 
ID:	7518Click image for larger version. 

Name:	nano2.jpg 
Views:	130 
Size:	104.1 KB 
ID:	7519

    The fan was overkill as I have never been able to get it hot enough to turn on
    Once booted onto the USB this is a full on speed demon with V2 camera and as far as I can tell a raspberry PI GPIO or
    something unbelievably close to it. Still playing but I have the full melodic desktop working and am pretty happy so far.
    Check out jetsonhacks he is working hard on the board as well.
    "The Nano is roughly twice the cost (you don't need a case to keep it from throttling), roughly twice the performance,
    4x the RAM, and uses the same power as a Pi 3B+. That's a win, in my book!"

    https://syonyk.blogspot.com/2019/04/...el-builds.html

    https://www.jetsonhacks.com/2019/03/25/nvidia-jetson-nano-developer-kit/

    Last edited by LloydF; 05-15-2019 at 07:57 AM.

  3. #123

    Re: The Robotis TurtleBot3

    And a built-in real-time clock chip, so you don't get the wrong time on boot like with the Pi ...
    Worth the price just for that :-)

  4. #124

    Re: The Robotis TurtleBot3

    LOL and unfortunately there is no RTC (Real Time Clock) on this model.

  5. #125

    Re: The Robotis TurtleBot3

    Because saving 25 cents was totally worth the hassle of invalid file system timestamps ...

    Every hat/attachment to any Pi connector should contain an RTC ...

  6. #126

    Re: The Robotis TurtleBot3

    I am now cheering for the PI4. I have the Raspbian Desktop Image up and running but No ROS image and I could not get that ROSberryPI http://wiki.ros.org/ROSberryPi/Insta...Raspberry%20Pi to run so I am still looking.
    Last edited by LloydF; 07-12-2019 at 11:32 AM.

  7. #127

    Re: The Robotis TurtleBot3

    Sounds Good - I just received a 2gb board, have an SD Card, and wall wart power... But don't have right HDMI cable... Should arrive later today or so.

    Trying to decide to try Raspian or Ubuntu.

  8. #128

    Re: The Robotis TurtleBot3

    Also wonder if any of you have tried to run your RPI 3 or 4 using SSD Drives instead of SD Cards?
    Like for example what is described in: https://jamesachambers.com/raspberry...llation-guide/

    Looks like it might be interesting to try...

  9. #129

    Re: The Robotis TurtleBot3

    Yea, once Ubuntu officially supports Buster things will really take off.
    I am not sure when that is.

  10. #130

    Re: The Robotis TurtleBot3

    It looks like Ubiquuity has a image for the rpi4.
    Note (I should note that this is Loaded with ROS Kinect 16.04.)
    For a direct download:

    https://downloads.ubiquityrobotics.com/pi.html
    Last edited by LloydF; 03-01-2020 at 02:59 PM.

Thread Information

Users Browsing this Thread

There are currently 4 users browsing this thread. (0 members and 4 guests)

Similar Threads

  1. Robotis OpenCM9.04 need help.
    By ErikVH in forum Robot Computers
    Replies: 6
    Last Post: 11-19-2014, 10:25 AM
  2. Robotis Task
    By 2fast4-u in forum Software and Programming
    Replies: 0
    Last Post: 08-23-2014, 06:36 PM
  3. Robotis OpenCM9.04 need help.
    By Hari in forum Robot Computers
    Replies: 38
    Last Post: 03-10-2014, 11:21 AM
  4. The New Robotis CM-900 board is now out!!!
    By Gort in forum Arbotix, Microcontrollers, Arduino
    Replies: 7
    Last Post: 07-16-2013, 10:42 AM
  5. Robotis CM-700 Shell ?
    By Ron in forum Arbotix, Microcontrollers, Arduino
    Replies: 7
    Last Post: 11-15-2012, 06:28 PM

Tags for this Thread

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •