Page 12 of 12 FirstFirst ... 289101112
Results 111 to 118 of 118

Thread: The Robotis TurtleBot3

  1. #111

    Re: The Robotis TurtleBot3

    I am having fun with it. Lately been doing more with the underlying board (OpenCR). I will get back to doing main turtle stuff soon.

    You can obviously do it either way. It is sort of nice having a setup that has other users and a set of developers who are able to answer questions.

  2. #112

    Re: The Robotis TurtleBot3

    Just a thought but, getting ROS and a turtlebot up and running with a book that covers you're platform, and written very well, is a
    amazing deal. It's the documentation that I like to read over and over until I get it.
    Last edited by LloydF; 07-04-2018 at 08:17 PM.

  3. #113

    Re: The Robotis TurtleBot3

    Quote Originally Posted by LloydF View Post
    Just a thought but, getting ROS and a turtlebot up and running with a book that covers you're platform, and written very well, is a
    amazing deal. It's the documentation that I like to read over and over until I get it.
    And thought I would mention, they also have created a new online ROS course for beginners:

    https://community.robotsource.org/t/...-handbook/1454
    And also mentioned up at:
    https://discourse.ros.org/t/new-ros-...-beginner/5320

    I will probably soon start playing through this course... Just finished updating their boards SPI and Wire libraries.... Now need to reassemble Turtle... But first work on water system
    Last edited by KurtEck; 07-10-2018 at 08:55 AM.

  4. #114
    Join Date
    Apr 2013
    Location
    Boston, MA
    Posts
    260
    Images
    11
    Rep Power
    25

    Re: The Robotis TurtleBot3

    Ah that's great. I think i'm going to get my hexapod until its "final" configuration, then check this out. Thanks

  5. #115

    Re: The Robotis TurtleBot3

    Looks like ROBOTIS has a new disk image for the TB3 out and, a firmware update to (v1.2.1)

  6. #116

    Re: The Robotis TurtleBot3

    Thought I would mention, that ROBOTIS has been busy with the TB3.

    Right now I am going to try using an RPI3+ as I fried the UP board I had on it... Something about supplying 12v to the Expansion connector pins, it did not like I plugged the power pins into wrong connector on OpenCR3 board... I have another UP board I will probably use again soon.

    But thought I might take this opportunity to try moving over to ROS2, as this appears to be the direction that Robotis is taking, plus the underlying ROS2 communications is setup to use standardized and more secure communications, which will be supported on Linux as well as Windows and MAC.

    There is more information talking about running the Turtlebot3 using ROS2 up at:
    https://discourse.ros.org/t/tb3-intr...tutorials/5959

    And the Turtlebot3 E-Manual has a section on it: http://emanual.robotis.com/docs/en/p...ications/#ros2


    Assuming I actually get comfortable with ROS2, maybe over time it would be fun to make a version of ROS Hexapod code base that uses ROS2, plus uses the OpenCR to control a lot of the functionality, in much the way that it does for the Turtlebot3...
    As I mentioned on the thread: http://forums.trossenrobotics.com/sh...4287#post94287 I have my MK3 PhantomX working with an OpenCR board.

  7. #117

    Re: The Robotis TurtleBot3

    This is my Burger now with voice and vision
    Click image for larger version. 

Name:	latest12212018.jpg 
Views:	51 
Size:	138.8 KB 
ID:	7426
    I found this: RASPIAUDIO.COM Stereo onboard speaker with Sound Card (AUDIO+SPEAKER) for Raspberry Pi Zero/Pi3/PI3B/PI3B+/Pi2/ with Better quality than a USB device, on amazon that really works well as a hat that does not take up much space and works well , yea!
    Merry Christmas all!
    Last edited by LloydF; 12-21-2018 at 11:41 AM.

  8. #118

    Re: The Robotis TurtleBot3

    I am not totally sure why but the raspberry pi web cam node just keep's breaking after running a short while. It may be a case of who is on first base when you have multiple connection to the internet, a case were /etc/hosts might help, but the usb web cam node module from github seems to work without any issues. Point being rpi cam has issues, were a usb camera is much more usable.
    git clone https://github.com/bosch-ros-pkg/usb_cam.git
    Last edited by LloydF; 2 Weeks Ago at 02:18 PM.

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Robotis OpenCM9.04 need help.
    By ErikVH in forum Robot Computers
    Replies: 6
    Last Post: 11-19-2014, 11:25 AM
  2. Robotis Task
    By 2fast4-u in forum Software and Programming
    Replies: 0
    Last Post: 08-23-2014, 07:36 PM
  3. Robotis OpenCM9.04 need help.
    By Hari in forum Robot Computers
    Replies: 38
    Last Post: 03-10-2014, 12:21 PM
  4. The New Robotis CM-900 board is now out!!!
    By Gort in forum Arbotix, Microcontrollers, Arduino
    Replies: 7
    Last Post: 07-16-2013, 11:42 AM
  5. Robotis CM-700 Shell ?
    By Ron in forum Arbotix, Microcontrollers, Arduino
    Replies: 7
    Last Post: 11-15-2012, 07:28 PM

Tags for this Thread

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •