Results 1 to 2 of 2

Thread: Attaching AX-12A to Actobotics Aluminum Channel?

  1. #1
    Join Date
    Jul 2017
    Location
    Seattle, WA
    Posts
    2
    Rep Power
    0

    Question Attaching AX-12A to Actobotics Aluminum Channel?

    I found this web page on attaching an AX-12A to an Actobotics Aluminum Channel

    http://www.raspberryturk.com/details/arm/3dprint.html

    Looks pretty nice.

    Curious, other options available? I've been thinking about getting a FTC Robot Construction kit for prototyping, but would need a method to attach Dynamixel servos. Obvious, the above web page is a method...

  2. #2

    Re: Attaching AX-12A to Actobotics Aluminum Channel?

    For the servo horn: Drill four holes, 2.1mm size, in a circular pattern with diameter 18mm. Screw into servo horn. Attachment done!

    For the servo body itself, you need to cut a cavity for the servo face plate and drill holes (again, 2.1mm) for the mounting hole pattern. That's a little more involved. (You can also 3D print this, with some success, as long as load is not too high.)

    Here's an example of how I mount the AX12A to rectangular tubing:

    Click image for larger version. 

Name:	ax12a-mount.jpg 
Views:	61 
Size:	41.2 KB 
ID:	7065

    If you don't have access to a mill or drill press, your options become slimmer... Using the plastic Bioloid brackets, and drilling through them, might be an option.
    Last edited by jwatte; 07-04-2017 at 11:46 AM.

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Question(s) Attaching hobby servos stops AX-12A from working
    By gmui in forum Arbotix, Microcontrollers, Arduino
    Replies: 13
    Last Post: 04-11-2017, 05:01 PM
  2. Attaching wheels to Hitec 1422 servo
    By gedelen in forum Mechanics / Construction
    Replies: 3
    Last Post: 01-21-2009, 07:34 PM
  3. CrabF on Discovery channel
    By jes1510 in forum Off Topic
    Replies: 9
    Last Post: 12-23-2008, 11:57 AM
  4. Need to find a N-channel MOSFET replacement
    By librab103 in forum Robotics General Discussion
    Replies: 1
    Last Post: 09-08-2008, 01:11 PM
  5. Robocars on the Science Channel
    By TechMech in forum Robotics General Discussion
    Replies: 5
    Last Post: 07-15-2008, 09:27 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •