Trossen Hexapod  Top Banner
+ Reply to Thread
Results 1 to 5 of 5

Thread: Fuel Burner Control System

  1. #1
    Join Date
    Jun 2007
    Location
    Calgary, Canada
    Posts
    9
    Rep Power
    19

    Fuel Burner Control System

    Hi All. I hope some of you find this interesting. I'm not putting this here to win anything because I don't think it will. I think it's fascinating but I'm not sure anyone else will. I hope this isn't too blabby.

    Brief

    What It Is

    • A Controller for a Classified Fuel Burner
    Current Hardware
    • Phidget 4-Servo Controller
    • 2 HiTec HS645 Servos (the most powerful I could use with standard wiring)
    • Banebots 45A DC Motor Controller
    • Measurement Computing USB-TC (USB Temperature Measurement Interface)
    • Omega J Type Thermistor
    • E-Flite Brushless Motor Controller (possibly part of failed experiment)
    • E-Flite 370 Outrunner Brushless Motor (possibly part of failed experiment)
    • Scavenged DC Motor (possibly part of failed experiment)
    Development Environment
    • Microsoft C#
    Current State Of Affairs
    • Version 2 of the software controls the devices but not much more.
    • I'm trying to develop a blower to replace the experimental air supply - a shop vac. I'm pondering the use of a cordless leaf blower.
    • Waiting to see if Burner can be made stable.
    • We're currently finding 1/2 turn fuel valves that can be actuated without adding gears to the servos.
    Background

    A brilliant friend of mine has invented a fuel burner that is a very cool idea. It's so simple and (potentially) effective that I'm sworn to secrecy! Investors are being rounded up and patents are currently being worked on. When I have the freedom to fill everyone in then I'll tell you all about it.

    When I was first told the (especially classified) thing that this burner would do I said it was impossible. When I first saw it - just sitting on the bench and not running - I basically said "I don't get it" and asked "how does this thing work?" When it was explained to me it I was suddenly very excited. In that same conversation I said "I think you'll need a control system and I may be able to make one for you." I was sure I could somehow do it. He said it didn't need one but has since changed his mind.

    It is thought that this burner will be scaled up to a variety of sizes and I'm hoping to build a controller that will work for all of them without tuning.

    Poking Around In the Dark

    I'm a software guy with a lot of experience building all kinds of software - none of it involving AI, though. I've never interfaced with anything in the real world from my software until now.

    "Stepper motor - what's a stepper motor?" "Servo - they use those in R/C airplanes but, really, I have no idea how." "Temperature measurement - can I do that via USB?" "Can I control all this stuff via USB so I can use my laptop?"

    My first crack at things was to buy a stepper motor controller. I hadn't found Trossen yet and bought a controller from a guy in Australia. It arrived but, although it worked fine, the supporting COM object came with hoardes of undocumented methods, the documentation was minimal and the person wasn't even remotely helpful via email. I wasn't happy. I did manage to get a motor out of an old printer and it worked but was way to wimpy to turn a fuel valve. (I should note that the controller was built for a 5-wire motor but I was using a 4-wire motor. A 5-wire can be faked with 4 resistors but this may have sapped a lot of the strength of the motor. I don't really know, though) When I included the gearing from the printer it barely had enough poop to do the job. If it doesn't make every move as directed then I can't use it because there is then no way to reliably know where it currently is.

    I then started looking into servos and managed to find Trossen. As you've probably all experienced, the interface objects are nice, the documentation is great and the people there are responsive and helpful - very nice!

    The Blower Fiasco

    My friend has been using the exhaling part of a shop vac for the blower and built a door over the suction side to control the flow. The shop vac is big, oud and I don't feel that it is accurate. I can (and may have to) use a servo to control the door on the vacuum side but I think I have a better idea - I purchased the Banebots DC motor controller from Trossen with the intent of using it on a blower to control the air.

    I first connected it to a DC motor I scavenged from a printer, bought an R/C prop and put them together. It barely threw enough air to keep one cool on a warm day so that didn't work.

    I then went to an R/C shop and bought a little E-Flite brushless motor/controller combo and an appropriate prop. (no, this doesn't use the Banebots controller) Connected to a couple scavenged 12V UPS batteries in parallel (believe it or not - one battery doesn't supply enough current!) this thing kicks out a LOT of air. For such a teeny little electric motor it's astounding! Having no idea what I'm doing, I built a nice shroud out of furnace duct to direct air from a 9" prop into a 2.5" hose. It didn't work work at all. The air ended up recirculating around the prop because of back pressure. The whisp of air coming out the 2.5" end actually decreased as the prop speed increased!

    Then, I researched ducted fans, cut down the prop and changed my shroud to be much closer to the recommended reductions. It works much better and likely supplies enough air, but, only without back pressure. A little experimenting by putting my hand near the exit showed that this wasn't going to work either.

    Then I researched blowers. It seems that I need something like a centrifugal air pump which supplies less volume but is far more capable of dealing with back pressures. Then it dawned on me - a leafblower. Leaf blowers likely operate fine with some back pressure. I can get an 18v cordless Black and Decker one for about the price of the E-Flite motor/controller combo. I hope that I can replace the NiCad battery pack with power from the Banebots controller and it will serve as a blower - at least on our small experimental burners. We'll see.

    Software Version 1

    My first version of software used the stepper motor and a temperature sensor (not via Trossen - but I hadn't found them yet!). It had the capability to scan or do manual control. It kept a graph of the burner temperature above a horizontal scroll bar showing the device temperature for the fuel setting - clearly showing the sweet spot. I took it to the burner "lab", hooked it up and it worked just dandy.

    I hadn't build any smarts into it yet but maybe that's a good thing. The burner itself works great but it's operation isn't continuous - it isn't "stable". I expected that the ideal fuel setting could be arrived at by any means so the AI portion of my software could poke around to find the sweet spot. To my dismay, the burner required putting in too much fuel and then lowering it to get to the sweet spot. We could not get there by just turning up the fuel. This completely threw my confidence that I could build an application that provided anything more interesting than manual control.

    Software Version 2 - The Current One

    It doesn't do much yet but it can control the 2 servos, the DC motor and hopefully a useful interface. One servo is used for the fuel rate and the DC motor control will eventually (hopefully?) control the air. The other servo is the master fuel valve and is basically a fuel cutoff. The graph is now 2D (air and fuel) and I will have to use color to show the sweet spot. Maybe a blue to red gradient.

    The rest depends on the burner stability. If it can be made stable then I can go for my original idea of some AI to make constant corrections and find the sweet spot. If it can't be made stable then this will be a (relatively boring) programmable controller. If that's the case then we'll end up having to find an ideal startup sequence for each size of burner and the steps will likely be kept in something like an XML config file. Boring but effective. I hope that I end up building it to to do both but I'll only do AI if it seems worthwhile.

    This Is All So Cool!

    I can't say that this project has been a success so-far. It may get there but there are too many things up in the air right now. What I can say is that the journey has been well worth it. The possiblities of things I now see that I can make is endless. There are just so many cool devices to be made with all this stuff. I hope you're all finding this as fun as I am!

  2. #2
    Join Date
    Sep 2006
    Location
    Carol Stream, Illinois
    Posts
    1,695
    Images
    118
    Rep Power
    87

    Re: Fuel Burner Control System

    Thanks for the submission Bill! Sounds like a pretty interesting project

    �In the long history of humankind (and animal kind, too) those who learned to collaborate and improvise most effectively have prevailed�
    - Charles Darwin

  3. Re: Fuel Burner Control System

    Quote Originally Posted by BillW View Post
    I think it's fascinating but I'm not sure anyone else will. I hope this isn't too blabby.
    Haha
    We're engineers, man. If there isn't a nearly incomprehensible amount of detail, we don't want it.

  4. Trossen XBee  Thread  Banner
  5. #4
    Join Date
    Jun 2007
    Location
    Calgary, Canada
    Posts
    9
    Rep Power
    19

    Follow The Instructions, Bill!!

    Thanks for the support, Dave. :-)

    Firstly, I did read the instructions!! (I can't honestly say I always do)

    I bought a B&D 18v Cordless Leaf Blower and I'd say it supplies at least as much air as my buddy's shop vac. I charged the B&D NiCads up and, full of anticipation, didn't bother to check the polarity. (this is the first DC source I've had where it wasn't clearly marked) When I touched the final wire from the BaneBots DC motor controller to the battery it instantly welded the wire to the connector so I quickly yanked it apart. I then jumped to the conclusion (as stupid as it seems now) that the problem was that I didn't have a load connected to the other side of the controller. I connected the blower to the other side of the controller and, again, touched the battery with the wire. One of the copper wire filaments instantly went red-hot so I pulled it off. Then, with a gasp, it dawned on me that the instructions clearly said that I might destroy the controller by connecting the power backwards. Through a bit of experimentation I've proven that I did just that. It seems that if you connect it backwards then it's also a short-circuit!

    The lesson? Don't just read the instructions, follow them.

    I've ordered another controller. The good news is that I now have a blower than I can control. I don't yet know if the controller can handle the load but I guess I'll find out. (I don't have anything to measure that kind of current so I may destroy another one)

  6. Re: Fuel Burner Control System

    Smooth move, Bill! Don't feel bad, though. I've fried a few motor controllers the same way. Those BaneBots controllers can take a hell of a beating when used properly, though. Well, now you know.

    A note about your motor current concerns: That controller can handle 45A for a few seconds, but only 12A continuously. To measure your motor current draw, put a regular DC ammeter between the battery and motor controller (in series, of course). Run the motor for a few seconds and see how high the current gets.

    Have fun!

+ Reply to Thread

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

     

Similar Threads

  1. Contest Entry Quiz Show Scoring System
    By bruf in forum Project Showcase
    Replies: 4
    Last Post: 10-17-2007, 04:03 PM
  2. Kondo web page translated.
    By Droid Works in forum Humanoids, Walkers & Crawlers
    Replies: 4
    Last Post: 10-06-2007, 05:49 PM
  3. Contest Entry Landscape Light Control Project
    By pottsbgstv in forum Project Showcase
    Replies: 7
    Last Post: 08-31-2007, 03:12 PM
  4. Home Security System +
    By SkipFire in forum Project Showcase
    Replies: 3
    Last Post: 08-17-2007, 11:10 AM
  5. Power Control System
    By SkipFire in forum Project Showcase
    Replies: 0
    Last Post: 07-23-2007, 03:50 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts