Results 1 to 6 of 6

Thread: Phidgets 8/8/8 Output problems

  1. Phidgets 8/8/8 Output problems

    For some reason I can't seem to get my outputs on my 8/8/8 to work. I've tested each output with a simple LED (I've tested the LED with a battery and it works fine). I don't have my meter with me tonight, but I suspect it isn't swtiching high. I've used both my code and the sample code....not working. One leg of the LED is wired to G and the other leg to an output.

    The Analog and Digital inputs work fine, but no outputs.

    Am I doing something wrong?

    Josh

  2. #2
    Join Date
    Sep 2006
    Location
    Carol Stream, Illinois
    Posts
    1,695
    Images
    118
    Rep Power
    109

    Re: Phidgets 8/8/8 Output problems

    Hi Josh,

    Are you sure you have the LED connected correctly? The Cathode (shorter lead) needs to be connected to the ground, else it won't work. No worries, I forget about that almost everytime

    If that doesn't work, do happen to have a voltmeter handy?

    �In the long history of humankind (and animal kind, too) those who learned to collaborate and improvise most effectively have prevailed�
    - Charles Darwin

  3. Re: Phidgets 8/8/8 Output problems

    Quote Originally Posted by Alex View Post
    Hi Josh,

    Are you sure you have the LED connected correctly? The Cathode (shorter lead) needs to be connected to the ground, else it won't work. No worries, I forget about that almost everytime

    If that doesn't work, do you happen to have a voltmeter handy?
    I'll try my meter over lunch today. I'm assuming I simply touch the (-) lead to ground and the (+) lead to the output; looking for the output to switch to high (5vdc) when the ouput is on?

    I will say that I wired up a computer fan to the output just like referenced on the phidgets web page, with no luck either. So, if I get no results from the meter, what is the process to diagnose where it is a hardware or software issue?

    Josh

  4. #4
    Join Date
    Sep 2006
    Location
    Carol Stream, Illinois
    Posts
    1,695
    Images
    118
    Rep Power
    109

    Re: Phidgets 8/8/8 Output problems

    Yes, that's exactly how to test the outputs If you are testing the screw heads on the terminal block, be sure that they are screwed in all the way to get a good connection.

    Occasionally a bad board will make it's way through production, so if there is a hardware problem with the digital outputs on your 8/8/8 then we'll replace it no worries. We'll probably have you send the board in so that we can test it in house and replace it if necessary.

    One thing though, you said that you tested the digital and analog inputs though and they worked fine. Did you test them on the same machine that you're testing the digital outputs?

    �In the long history of humankind (and animal kind, too) those who learned to collaborate and improvise most effectively have prevailed�
    - Charles Darwin

  5. 8/8/8 is fine....I am faulty!

    Quote Originally Posted by Alex View Post
    Yes, that's exactly how to test the outputs If you are testing the screw heads on the terminal block, be sure that they are screwed in all the way to get a good connection.

    Occasionally a bad board will make it's way through production, so if there is a hardware problem with the digital outputs on your 8/8/8 then we'll replace it no worries. We'll probably have you send the board in so that we can test it in house and replace it if necessary.

    One thing though, you said that you tested the digital and analog inputs though and they worked fine. Did you test them on the same machine that you're testing the digital outputs?
    I evidently had some bad LED's (or out of range). I went to Radio-Hut over lunch and bought some replacements, and the LED's fire. Sorry for the trouble and thanks for the response,

    Josh

  6. #6
    Join Date
    Sep 2006
    Location
    Carol Stream, Illinois
    Posts
    1,695
    Images
    118
    Rep Power
    109

    Re: 8/8/8 is fine....I am faulty!

    Hey no trouble at all Josh! Glad to hear it was just the LED's.

    In regards to your email you sent to me though: how are you controlling a smoker with the 8/8/8?

    �In the long history of humankind (and animal kind, too) those who learned to collaborate and improvise most effectively have prevailed�
    - Charles Darwin

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. 8/8/8 outputs open on startup
    By Riley in forum Arbotix, Microcontrollers, Arduino
    Replies: 3
    Last Post: 03-29-2007, 03:03 PM
  2. Replies: 29
    Last Post: 03-06-2007, 10:48 AM
  3. Listening for Phidgets 8/8/8 sensors without a GUI to persist thread
    By wmccafferty in forum Arbotix, Microcontrollers, Arduino
    Replies: 3
    Last Post: 02-16-2007, 12:56 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •