Trossen Accelerometer Gyro Top Banner
+ Reply to Thread
Results 1 to 3 of 3

Thread: Entry 1: USB Gun Turret

  1. Entry 1: USB Gun Turret

    vCrib's Automated Gun Turret

    The gun turret is based on a pan tilt servo system, which uses a 4-channel Phidget's USB servo controller to allow PC control. Using its standard security camera the unit doubles as a remote video survelliance device. A servo relay is attached to the electric firing mechanism in the gun. The PC software that controls the unit can be used manually or in autonomous mode with motion tracking.

    Combined with the Virtual Crib home automation software, the gun can be brought online by the house when an alarm is triggered. The turret can be authorized to fire at moving targets. Resident safety is ensured by the automation software instructing the gun to go offline in normal situations and also by overriding the gun by cutting power to it with an appliance module.

    Different types of guns can be mounted as the pan tilt system can control a 6lb load. Testing and safety warrent only the use of an airsoft gun, but water guns, metal BB guns, paintball guns, tazers and small caliber sidearms could be used. Some of these options can be dangerous and/or illegal and much care and research should be done before ever attempting to use any option that could cause damage to property or carbon-based life forms.

    Videos can be seen at:
    v1.0 http://youtube.com/watch?v=Fu0OX7MQL5I
    v1.1 http://youtube.com/watch?v=VCOJA6ps-7s

    The photos are v1.2 which replaced the servo used for firing with a relay and the wiring was cleaned up a little.

    Thanks,
    Vaughn
    Attached Thumbnails Attached Thumbnails Click image for larger version

Name:	Turret1.jpg‎
Views:	374
Size:	86.2 KB
ID:	44   Click image for larger version

Name:	Turret2.jpg‎
Views:	340
Size:	76.2 KB
ID:	45  

  2. #2
    Join Date
    Sep 2006
    Location
    Carol Stream, Illinois
    Posts
    1,695
    Images
    118
    Rep Power
    87

    Re: Entry 1: USB Gun Turret

    Dang that thing looks vicious!

    Thanks for the submission Vaughn

    �In the long history of humankind (and animal kind, too) those who learned to collaborate and improvise most effectively have prevailed�
    - Charles Darwin

  3. Re: Entry 1: USB Gun Turret

    totally awesome. i am a newbee and i would like to try making that. ounce again its out of the park.

+ Reply to Thread

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

     

Similar Threads

  1. wifi robot with fully auto paintball turret
    By seesoe in forum Robotics General Discussion
    Replies: 38
    Last Post: 06-02-2011, 12:34 AM
  2. Contest Entry Entry #3: Home Security/Automation
    By Vaughn in forum Project Showcase
    Replies: 3
    Last Post: 03-02-2010, 06:12 AM
  3. Robotic Gun Turret
    By El Espada in forum Robotics General Discussion
    Replies: 3
    Last Post: 01-11-2008, 10:53 AM
  4. Contest Entry Sentient Turret
    By ekoos7 in forum Project Showcase
    Replies: 18
    Last Post: 12-12-2007, 11:54 AM
  5. Home Automation and Gun turret
    By Vaughn in forum Project Showcase
    Replies: 9
    Last Post: 06-22-2007, 11:35 AM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts