Results 1 to 4 of 4

Thread: Hexabot 6x6 tabletop Robot

  1. Hexabot 6x6 tabletop Robot

    Hello everyone,

    Here is a bot I created for a contest that the Chicago Area Robotics club held last year. The robot is called Hexabot.



    It has 6 motors directly driving 6 wheels. With the exception of the electronics, it is constructed entirely of Tamiya parts:
    Motors: 6 High Speed Gearboxes H.E.
    Tires: 6 Sports Tires
    Main Body: 3 Universal Plates connected with long universal arms
    Underside Support: Long universal arms
    Battery: Tenergy 7.4v 800mAH high output Li-Poly
    Motor Controller: Pololu VNH3SP30 dual h-bridge
    Main Controller: DevBoard-M32
    The contest is listed here - http://www.chibots.org/drupal/?q=node/27


    Here is a video of Hexabot doing a test run:
    http://www.wrighthobbies.net/video/hexabot.wmv

    It's able to complete the course in less than 3 seconds.

    Then, just for fun, I added a Madcatz wireless PS2 controller. The PS2 uses SPI to communicate between the joystick and the game console. I wired the receiver to the DevBoard-M32 and can receive and decode all the buttons and joysticks.



    Here is a video of me running it around my family room:





    My plan is to have it ready to compete in the line following contests at the Fall Chibotica games being held during iHobby Expo.

    Eddy Wright
    Wright Hobbies Robotics
    http://www.wrighthobbies.net
    Last edited by wrighthobbies; 09-19-2007 at 11:14 PM. Reason: Corrected Youtube link

  2. Re: Hexabot 6x6 tabletop Robot

    I have some questions, if you don't mind. Was interfacing the Play Station controller to your dev board is pretty straightforward? Is the command set published somewhere?

    Also, what kind of ISP cable do you use? I've been looking at USB programmers, but they're kind of pricy.

    [edit:] Thanks for submitting your project! It's entered in this month's contest.
    Last edited by Dave; 09-21-2007 at 05:51 PM.

  3. Re: Hexabot 6x6 tabletop Robot

    Hi Dave,

    It took a while to do the research and tweak the timing but once that was done the rest wasn't too hard.

    I have attached the Bascom code I use for Hexabot and the PS2 pinouts. I also show how to make the joysticks non-linear to manage the sensitivity of the small wireless joysticks.

    Communications with the PS2 joystick is handled by the SPI port. Take a look at the Config SPI statement in the code and look at the PS2 subroutine. If you are familiar with SPI, you know that sometimes data is sent and received at the same time. I had to use a combination of SPIOUT (sends a byte) and SPIMOVE (sends a byte and receives a byte simultaneously).

    As for a USB programmer, I haven't seen a lot of affordable choices. Pololu has one for $27, the best price so far. It has a 6-pin header on it but I have 6-pin to 10-pin adapters to make it work with my stuff. If you have a PC, your bet bet may be to add in a Parallel/Serial I/O card and wait on USB. The cost of a USB programmer and a USB to Serial adapter will add up.

    Eddy

  4. #4
    Join Date
    Jan 2007
    Location
    Near Robot Parts In The USA
    Posts
    232
    Rep Power
    47

    Re: Hexabot 6x6 tabletop Robot

    Dave,

    You may be able to use a key mapper (some USB game pads come with the software for it).

    Check out Wal*Mart.

    --Scotty
    Dell Studio XPS Desktop, Windows Vista, 12 GB RAM, 2x 500 GB SATA RAID0 HDD, Intel i7 2.66Ghz Quad Core (4 cores, 8 virtual cores). The power that's needed... plus some!

    RIBO Labs, Springing Robotic Development to a New Level

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Contest Entry The eyeRobot: Robot Blind Aid
    By Shrimpy in forum Project Showcase
    Replies: 16
    Last Post: 02-07-2011, 09:20 AM
  2. [ANNOUNCE] Rat's Life: robot programming contest
    By omichel in forum Robotics General Discussion
    Replies: 4
    Last Post: 09-19-2008, 02:13 PM
  3. Kondo web page translated.
    By Droid Works in forum Humanoids, Walkers & Crawlers
    Replies: 4
    Last Post: 10-06-2007, 05:49 PM
  4. Contest Entry Make a wall avoiding robot! Part 1
    By Brandon121233 in forum Project Showcase
    Replies: 16
    Last Post: 09-12-2007, 04:41 PM
  5. Ping Pong robot
    By stefano.antonelli in forum Arbotix, Microcontrollers, Arduino
    Replies: 7
    Last Post: 08-13-2007, 08:49 AM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •