Results 1 to 2 of 2

Thread: Computer controlled Motor?

  1. #1
    vignetting Guest

    Smile Computer controlled Motor?

    Hello everyone,

    I never made a robot or such thing. So I have no idea about everything, I mean mostly.
    And I'm trying to build a rotating cylinder with some small screens in side. In fact, it is a zoetrope with screens inside.

    Anyway, I had a hard time to find a thing to connect all the wires to the rotational structure from the base. and I found thing called slip ring by the moog or the mercotac company. So one issue is down.

    Another thing is a motor. I don't know what kind I should get. I think it's going to be about 14 inches (diameter) and 8~7 inches(height) probably wood. So it's not that heavy and drive it less than 1000 rpm?

    The major issue is that I want it to control the rpm of motor by computer(usb or serial connection).

    1. What kind of motor do I want?
    2. How can I connect the motor to computer in order to control the rpm?

    It would be great if anyone can recommend specific parts for this.
    Thanks a lot and have a great weekend~

  2. #2
    Join Date
    Sep 2006
    Location
    Chicago Illinois
    Posts
    682
    Images
    174
    Rep Power
    83

    Re: Computer controlled Motor?

    Hello,

    To control a motor from a computer you want to use a Servo controller to output a PWM signal to a DC motor controller. See the graphic and description on this page. There are a whole line of motors from banebots that have many different RPMs. You should be able to find a motor to match your needs there.

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Question(s) fixing Colson wheels on motor shaft
    By stefano.antonelli in forum Mechanics / Construction
    Replies: 6
    Last Post: 02-13-2008, 12:37 AM
  2. Contest Entry Fuel Burner Control System
    By BillW in forum Project Showcase
    Replies: 4
    Last Post: 08-03-2007, 04:54 PM
  3. Fast Spinning DC Motor + Controller
    By BillW in forum DYNAMIXEL & Robot Actuators
    Replies: 3
    Last Post: 06-29-2007, 04:12 PM
  4. Phidget controlled Gun Turret defends home
    By Vaughn in forum Arbotix, Microcontrollers, Arduino
    Replies: 1
    Last Post: 06-15-2007, 05:04 PM
  5. Controlling a MAXI Motor Controller
    By shobley in forum Arbotix, Microcontrollers, Arduino
    Replies: 2
    Last Post: 02-02-2007, 01:59 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •