Results 1 to 3 of 3

Thread: Raspberry Pi 3 + Dynamixel XL-320 + PiCam

  1. #1
    Espen Guest

    Raspberry Pi 3 + Dynamixel XL-320 + PiCam

    I'm thinking about buying some Dynamixel XL-320 servos to a robotarm. Together with the servos I must buy the USB2Dynamixel adapter and the SMPS2Dynamixel adapter. But the main problem I'm having is how to communicate with the servos trough the USB adapter. Do anyone know this? Some explanation and some simple code with this setup just to make the servos run would be very much appreciated!

    Another question; On the robotarm I'm hoping I can mount a PiCamera. With this I hope I can find objects (with OpenCV) and send the coordinates to the servos. How can I do this? Also here is some explanation and some simple code much appreciated!

  2. #2
    Join Date
    Dec 2012
    Location
    Los Angeles, CA
    Posts
    858
    Images
    25
    Rep Power
    88

    Re: Raspberry Pi 3 + Dynamixel XL-320 + PiCam

    Robotis has some sample code on how to use the USB2Dynamixel. Pretty straight forward to read. As far as example of IK code, which is what you will need to do your second question it is best to read up since depending on the degrees of freedom on your arm it will change greatly.

  3. #3

    Re: Raspberry Pi 3 + Dynamixel XL-320 + PiCam

    You can download the Robotis (R+ Manager 2.0) for windows. Then use a ax/mx powered hub from trossen and you will need some x3P convertible maybe X3P cables. Then you can Id and test your servo's. I am using the U2D2 but it should be the same setup.

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Question(s) RX_TIMEOUT error when setting power to Dynamixel Pro - Raspberry Pi
    By jgrosso in forum DYNAMIXEL & Robot Actuators
    Replies: 30
    Last Post: 08-22-2017, 09:36 AM
  2. Raspberry PI 2 vs. Odroid XU3 to use with Dynamixel SDK and usb2ax
    By Snoopy in forum Arbotix, Microcontrollers, Arduino
    Replies: 3
    Last Post: 02-03-2015, 07:19 PM
  3. Question(s) Raspberry Pi
    By Robonaut in forum Robot Computers
    Replies: 20
    Last Post: 07-07-2013, 10:46 AM
  4. About to give up on the Raspberry Pi
    By jwatte in forum Software and Programming
    Replies: 5
    Last Post: 01-14-2013, 10:57 AM
  5. Just For Fun My Raspberry PI
    By rebel in forum Arbotix, Microcontrollers, Arduino
    Replies: 0
    Last Post: 12-31-2012, 05:57 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •