Results 1 to 4 of 4

Thread: Servo won't turn while accepting commands from an Arduino

  1. Thumbs up Servo won't turn while accepting commands from an Arduino

    Hello everyone,


    In my first post, I'm asking for your advice -


    I'm attempting to turn a servo with my Arduino when it gets orders from a serial contribution, for this situation, my console. I have officially done this with engines and it works fine however when I attempt with my servo it doesn't move by any means. (an example from - http://www.powerjackmotion.com/produ...o-motor-range/ ) So far I have this written -


    #include <SoftwareServo.h>
    SoftwareServo myservo;
    int movemotor;
    void setup() {
    Serial.begin(9600);
    myservo.attach (10);
    myservo.write(90);
    }
    void loop() {
    movemotor = Serial.read();
    if (movemotor = 111) {
    for (int pos = 90; pos >=0; pos--) {
    myservo.write(pos);
    delay(15);
    }
    }
    else if (movemotor = 99) {
    for (int pos = 90; pos <= 180; pos++) {
    myservo.write(pos);
    delay(15);
    }
    }
    }

    I'm powering the servo remotely with a 9-volt battery and have made a point to associate its ground to that of the Arduino, however, can't see whatever else I fouled up.
    Any better idea would be greatly appreciated.
    Thanks in advance

  2. #2

    Re: Servo won't turn while accepting commands from an Arduino

    I'm powering the servo remotely with a 9-volt battery
    9-volt batteries are bad for two reasons:

    1) The voltage 9V is way too high for what most RC servos expect. Most servos expect something in the 4.8V-6.0V (4S-5S NiMH) range, and "high voltage" RC servos can expect 6.8V-8.0V (expected to run on 2S LiPo.) There is some chance that hooking up a battery that's too high voltage can destroy the electronics of the servo.

    2) The current available from a 9V battery is very low -- these are not strong batteries. Thus, if the servo is not a "micro" servo, the battery may not be able to source enough current to actually move the servo.

    Another thing I have to ask -- did you hook ground from the Arduino to the black servo wire and the battery - terminal? If not, the servo will not see the voltage differential for the control signal from the Arduino.

  3. Re: Servo won't turn while accepting commands from an Arduino

    Hello Jwatte, Thanks for your reply and helping me.

    So, How many volt batteries I have to use for this.

    No, I didn't hook ground from the Arduino to the black servo wire and the battery terminal.

  4. #4

    Re: Servo won't turn while accepting commands from an Arduino

    So, How many volt batteries I have to use for this.
    I don't know! WHat does your servo need? What servo is it?

    I didn't hook ground from the Arduino to the black servo wire and the battery terminal
    If there is not a shared ground between Arduino, servo, and battery, then the signals from Arduino won't make it to the servo. Electrical signals always need two wires (typically, "signal" and "ground.")

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Question(s) Arduino to Arduino serial servo control
    By cpunk7 in forum Software and Programming
    Replies: 1
    Last Post: 06-30-2015, 01:30 PM
  2. How do I set Dynamixel servo ID using an Arduino?
    By OOrmOnIzArGoR in forum Arbotix, Microcontrollers, Arduino
    Replies: 1
    Last Post: 12-03-2014, 10:33 PM
  3. Dynamixel Servo Control Issues (MX-28 and Arduino Mega)
    By JasonT in forum DYNAMIXEL & Robot Actuators
    Replies: 1
    Last Post: 08-12-2014, 07:12 PM
  4. Question(s) How to control AX-12A Servo motor through arduino with labview interface?
    By Taslim in forum Arbotix, Microcontrollers, Arduino
    Replies: 6
    Last Post: 06-03-2014, 12:12 AM
  5. Arduino bluetooth servo control
    By ArduTank in forum Mech Warfare
    Replies: 6
    Last Post: 07-08-2012, 03:26 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •