Results 1 to 4 of 4

Thread: Kondo KHR-1HV USB Dongle

  1. Kondo KHR-1HV USB Dongle

    I'm using a Mac, and Kondo doesn't have drivers for the SerialUSB Adapter. Their adapter uses an FTDI FT232BL chip, which allows vendors to provide their own Vendor ID and product ID. Kondo has placed such an EPROM on their adapter. As a result, FTDI's drivers won't work.

    My solution? Remove the EPROM. It works great. Tested on OS X, Linux, and Windows (I only have the KHR-1HV working in Windows right now). The EPROM is the 6 pin chip, U1, that's right next to the USB connector on the board (it's on the same side as the FTDI chip).

  2. Re: Kondo KHR-1HV USB Dongle

    Ubuntu has a driver for the FTDI chip, but the brltty causes problems. Removing brltty allows the adapter to show up as /dev/ttyUSB0.

  3. #3
    Join Date
    Sep 2006
    Location
    Carol Stream, Illinois
    Posts
    1,695
    Images
    118
    Rep Power
    109

    Re: Kondo KHR-1HV USB Dongle

    Thanks for the info bdavids1! Within the next month or two tops I hope to get up and running in this community an area where we can all post these nice tips and also have a place where we can upload projects, files, etc.

    �In the long history of humankind (and animal kind, too) those who learned to collaborate and improvise most effectively have prevailed�
    - Charles Darwin

  4. Re: Kondo KHR-1HV USB Dongle

    It turns out there's an easier way of accomplishing the same task, by reprogramming the EEPROM. On Linux, there's a command, ftdi_eeprom, that can be used to reprogram the EEPROM. Create a config file with:

    Code:
    vendor_id=0x165c      # Vendor ID (Replace with the one you found)
    product_id=0x0002     # Product ID (Replace with the one you found)
    then run:
    Code:
    sudo ftdi_eeprom --erase-eeprom eeprom_ftdi.conf

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Kondo web page translated.
    By Droid Works in forum Humanoids, Walkers & Crawlers
    Replies: 4
    Last Post: 10-06-2007, 05:49 PM
  2. Kondo Robots
    By asbrandsson in forum Humanoids, Walkers & Crawlers
    Replies: 2
    Last Post: 02-27-2007, 01:51 PM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •