Results 1 to 4 of 4

Thread: H bridge Design

  1. #1

    H bridge Design

    Being the cheap person i am and needing 10 motor drivers does anybody have a h-bridge design they want to share? I have a lynxmotion ssc driveri want to use.

    12vdc 3a max.

    thanks

  2. #2
    Join Date
    Sep 2006
    Location
    Carol Stream, Illinois
    Posts
    1,695
    Images
    118
    Rep Power
    105

    Re: H bridge Design

    Sorry, I'm not all that savvy in EE stuff, but I looked around and found a couple of sites that might at least give you a good starting point on some areas:

    http://www.mcmanis.com/chuck/Robotic...t-circuit.html

    http://www.robotroom.com/HBridge.html
    http://www.robotroom.com/BipolarHBridge.html


    The RobotRoom has a ton of good content on there. It's just not that easy to find it all.

    Hope some of that info helps

    �In the long history of humankind (and animal kind, too) those who learned to collaborate and improvise most effectively have prevailed�
    - Charles Darwin

  3. #3
    robot maker Guest

    Re: H bridge Design

    lm298 is a very easy circuit and dual 3 amp circuits,looking for a cheap h bridge circuit with all parts solarbotics has one in kits for $19.00 part #, kit#13

  4. #4
    Join Date
    May 2008
    Posts
    2,228
    Images
    155
    Rep Power
    124

    Re: H bridge Design

    12VDC, 3A max, but what is the typical current? The TI SN754410 is about $1.50 a chip, and controls two motors (so 5 chips for your 10 motors). BUT.... it is rated 1amp continuous, 2amp peak (3-36VDC). If I remember correctly, that is without a heatsink. It may be possible with a heat sink to pull 3A, but I'm not sure.... testing would be required. If the SN754410 won't do 3amps without blowing, the L298 is probably the next lowest cost single-chip motor driver (it is 3A rated, but runs about $3 per motor channel).

    As far as using the SSC32 with these motor drivers - that is likely going to increase the cost. You are going to need a circuit to change servo pulses to motor voltage. I know there are few out there on the web, but as far as I remember, each circuit needs about 2-3 different TTL chips, by the time you get done building a 10 channel version you can figure to have 20 TTL chips, and about the same number of resistors and caps. A nightmare to debug....

    What exactly are you building that requires 10 channels?

    -Fergs

    Edit: Wow, just noticed that the original thread was from Nov 07. Guessing this info won't be useful to the original poster (unless his projects progress as slow as mine...)

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. robot foot design
    By sweldon in forum Robotics General Discussion
    Replies: 6
    Last Post: 12-11-2007, 11:59 AM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •