Results 1 to 4 of 4

Thread: Wiimote firefighting robot

  1. Honorablemention Wiimote firefighting robot

    The Wiimote makes a perfect control system for a fire fighting robot. A wiimote can both send and recieve bluetooth commands, making it a low cost bluetooth transciever.


    It also has IR sensors which can detect a candle and a bluetooth transciever to communicate back to a host computer. I used a boebot as the robot platform, an arduino, wiimote and a Linux computer.


    The wiimote uses its IR sensor to find the candle. It transmits the sensor readings back to the host computer over bluetooth . A C program running on the host computer reads the sensor data and sends commands back over bluetooth to the wiimote. The wiimote relays those commands to an arduino board over the wiimote's expansion port.



    The wiimotes expansion port uses the I2C protocol. So normally a nunchuck is reading/sending those I2C commands, but in my case an arduino is reading them. The arduino then controls the servos (the boebot uses rc servos modified for continuous rotation) and a fan. The fan is switched on/off with a ULN8023 chip.


    This fire fighting robot is still very crude. It lacks the number of sensors that you would be need to seriously compete. It is mainly a proof of concept that the wiimote can be used in a fire fighting robot. It basically just circles around until it sees a candle, then turns on the fan and moves toward the candle. The wiimote seems to loose the flame when it gets withing 4 inches. Maybe the candle is overloading the sensors or maybe its just bad programming on my part.
    Arduino code
    C code for host computer
    The C program depends on version .4 of libcwiimote

  2. #2
    Join Date
    Sep 2006
    Location
    Carol Stream, Illinois
    Posts
    1,695
    Images
    118
    Rep Power
    109

    Re: Wiimote firefighting robot

    This is a really cool project tempalte! I had no idea that the wiimote uses I2C. Very interesting.... Now I want to start building Wiimote controlled projects!!

    Do you happen to have any videos of this little bot in action?

    Great work on this I got your project entered in our contest.

    BTW, are you chad on that blog? I dig a lot of those projects.

    �In the long history of humankind (and animal kind, too) those who learned to collaborate and improvise most effectively have prevailed�
    - Charles Darwin

  3. Re: Wiimote firefighting robot

    There are a lot of cool Wiimote hacks out there, but this is the first fire fighting one I've seen. Just shows you how versitile that thing is. I mean, for about 40 bucks you get a 3-axis accelerometer, a bluetooth transiever, and an IR camera, and I2C connectivity. Neato.

    [edit] Also, it would be great if we could see a few more pictures.
    Last edited by Dave; 11-28-2007 at 04:25 PM.

  4. Re: Wiimote firefighting robot

    Quote Originally Posted by Alex View Post
    BTW, are you chad on that blog? I dig a lot of those projects.
    Yep, that is my blog. Hacking the wiimote and nunchuck has given me a lot of project ideas.

    chad

Thread Information

Users Browsing this Thread

There are currently 1 users browsing this thread. (0 members and 1 guests)

Similar Threads

  1. Contest Entry The eyeRobot: Robot Blind Aid
    By Shrimpy in forum Project Showcase
    Replies: 16
    Last Post: 02-07-2011, 09:20 AM
  2. [ANNOUNCE] Rat's Life: robot programming contest
    By omichel in forum Robotics General Discussion
    Replies: 4
    Last Post: 09-19-2008, 02:13 PM
  3. Kondo web page translated.
    By Droid Works in forum Humanoids, Walkers & Crawlers
    Replies: 4
    Last Post: 10-06-2007, 05:49 PM
  4. Contest Entry Firefighting Robonova
    By kemsulli in forum Project Showcase
    Replies: 2
    Last Post: 08-28-2007, 03:44 PM
  5. Ping Pong robot
    By stefano.antonelli in forum Arbotix, Microcontrollers, Arduino
    Replies: 7
    Last Post: 08-13-2007, 08:49 AM

Posting Permissions

  • You may not post new threads
  • You may not post replies
  • You may not post attachments
  • You may not edit your posts
  •